1 Meter of Pi
  • Challenges & Projects
  • Design Challenges
  • 1 Meter of Pi
  • More
  • Cancel
1 Meter of Pi
Blog Envidrawer 6 - Mix of fixes
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
  • Author Author: jduchniewicz
  • Date Created: 1 Jan 2021 5:38 PM Date Created
  • Views 1070 views
  • Likes 5 likes
  • Comments 2 comments
  • 1meterofpi
  • pimoroni
  • envidrawer
  • urban farming
  • climate crisis
  • 1meter of pi
  • rapsberrypi
  • smart farming
Related
Recommended

Envidrawer 6 - Mix of fixes

jduchniewicz
jduchniewicz
1 Jan 2021

Previous blogs

Description

#1 - Introduction, the plan and materials preparationIn this blog post we describe the project's main concept and some initial high-level design of it.
#2 - Materials and casing assembly

Our journey with selecting proper materials, cutting and assembling the drawer and its casing!

#3 - Modelling, cutting, planting!The title says it all: this part describes some modelling we did before cutting some holes in the drawer and finally planted some vegetables!
#4 - Plants, harvests, and fertilisers

First harvest, problems with plants and used fertilisers. All that went off-script for our plants in the artificial environment.

#5 - Piping and pumping - water and liquid fertiliser delivery systemDesign and development of water supply system.




Next blogsDescription
#7 - Ride the lightning - Wiring diagram, pinout and components discussionDiagram of the circuit, pinout for most components, wire choices and their connections
#8 - Pulling the stringsLED and Fan control circuit, overview of BJTs and MOSFETs with a handful of useful general information

#9 - 3D printing

Detailed description of 3D printed components, their presentation and some tips
#10 - Software, architecture and the benefits of good preparationBig explanation of the software and its architecture
#11 - SummaryOur final post before the end of the challenge!

      • Intro
      • Water supply
      • Foil and soil
      • Plants and their fate
      • Lightning changes
      • Summary

Intro

In this blog, we focus on final touches to the lightning and water supply system as well as simple, yet important fixes to soil containment and internal design. We address previous problems met by plants. We improve our design to best create an environment easy to control and adjust to plants' current needs.

 

Water supply

The pipe was buried, sealed and attached to a series of knee connectors. These enter a 1.8 liter box as we decided against using large volume 3D printed one due to material cost and prototype character of our project. The connection is shown on the picture below, with the submersible water pump attached to the bottom of the container using hot glue. All connections were also sealed using hot glue.

imageimage

Picture 1&2: Submersible pump attached inside the 1.8 liter box and the contraption covered with a lid for protection against spillage

 

Water distributes evenly, reaching the furthest drippers and cables, as well as properly dispersing in proximal tubules. It is important to notice that the needle-sized holes were big enough for dripping water and humidifying the soil around them. Pump is sufficient for our needs, and can be further regulated with voltage.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Video 1: Demonstration of water delivery by the furthest from pump 3mm tube buried in soil

 

Foil and soil

To make sure the soil is kept in one container and does not spread to the electronics compartment, the soil is contained within a foil. Temporarily, it was just rolled up and kept as a prototypic environment. When the measurements were taken, and the water supply systems and electric motors were installed, it had to be firmly secured to the bottom of the drawer using wooden planks. We screwed them in to avoid soil spillage into adjacent compartments as well as isolate plants from the electronic compartment.

imageimage

Picture 3&4: The border of the soil bounded by screwed on leftover planks - nothing goes to waste mind you! This is an environmental project!

 

Plants and their fate

As living in a low-light environment, with little airflow is not the ideal conditions for microflora, we decided to consume the rest of the sprouts. They served their purpose, showing that such a project can be practical and can sustain a microenvironment suitable for plant growth.

 

Microgreens are produced with no problem even with very restricted light and nutrient supply. Now as we get closer to an appropriate water delivery system, lightning and airflow, we will diverge towards larger plants. When all the electrical circuitry is ready, the newly purchased plants will be planted and used for final software setup and the microenvironment will be tested.

 

Lightning changes

As our last growth turned out leggy and fragile, we needed to improve the lightning inside the envidrawer. We added 5 m of 5W LEDs, of the same temperature and specifications as before, resulting in a total of 10 m of LED. It should be sufficient to prevent such problems in the future. LEDs were placed in a circular pattern on the top of the drawer. They were cut and joined together for balanced light distribution.

imageimage

Picture 5&6: 2 LED stripes in a circular pattern with separate power line attachment, aluminum foil for reflection of light trapped inside the drawer

 

Summary

Wrapped up, we made a functional water delivery system, improved our lightning and strengthened our overall structure. We showed that it is possible to grow edible (and tasty!) plants under your own bed. Now it is time to finish the hardware and make sure our drawer is as automatic and easy to operate as possible. Best wishes from our fourth team member who found our lightning system a comfortable pillow image

image

Michał & Jakub & Szymon & Brun

 

 

Previous postNext post
#5 - Piping and pumping - water and liquid fertiliser delivery system#7 - Ride the lightning - Wiring diagram, pinout and components discussion
  • Sign in to reply

Top Comments

  • genebren
    genebren over 5 years ago +1
    Good work. Keep moving forwards!
  • DAB
    DAB over 5 years ago +1
    Good update. DAB
Parents
  • genebren
    genebren over 5 years ago

    Good work.  Keep moving forwards!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 5 years ago

    Good work.  Keep moving forwards!