BeagleBone Black Radio Challenge
  • Challenges & Projects
  • Design Challenges
  • BeagleBone Black Radio Challenge
  • More
  • Cancel
BeagleBone Black Radio Challenge
Blog Beaglebone Black Radio Challenge - Part 3: User interface (Work in progress)
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fvan
  • Date Created: 27 Feb 2014 9:41 PM Date Created
  • Views 3222 views
  • Likes 2 likes
  • Comments 8 comments
  • RoadTest
  • wifi
  • lcd
  • Black
  • radio
  • bbb
  • BeagleBone
  • sdr
  • challenge
  • beaglebone_black_radio
Related
Recommended

Beaglebone Black Radio Challenge - Part 3: User interface (Work in progress)

fvan
fvan
27 Feb 2014

All entries in this blog series:

  • Beaglebone Black Radio Challenge - Review
  • Beaglebone Black Radio Challenge - Part 1: Project description
  • Beaglebone Black Radio Challenge - Part 2: Getting the different components to work
  • Beaglebone Black Radio Challenge - Part 3: User interface (Work in progress) (this post)
  • Beaglebone Black Radio Challenge - Part 4: The Build
  • Beaglebone Black Radio Challenge - Part 5: Project Finalisation

 

  • Webserver
    • Installation
    • Disabling default webserver
    • CGI/Perl support
  • User interface
    • Sketches
    • Implementation
  • Testing

 

I don't have a lot of experience programming, I am however familiar with scripting and HTML. This is why I planned to create the interface for the radio in HTML/Perl.

 

Webserver

 

In order to be able to server the web interface of the radio, a webserver is required. While searching, I came across other people using "lighttpd" on the Beaglebone, so I decided to give it a try.

 

Installation

 

The lighttpd package needed to be installed:

 

root@beaglebone:~# opkg install lighttpd

 

The installation also took care of setting up the necessary files to start the webserver automatically:

 

ln -s '/lib/systemd/system/lighttpd.service' '/etc/systemd/system/multi-user.target.wants/lighttpd.service'
Job for lighttpd.service failed. See 'systemctl status lighttpd.service' and 'journalctl -xn' for details.
Adding system startup for /etc/init.d/lighttpd.

 

Once installed, I checked the status of the newly installed webserver:

 

root@beaglebone:~# systemctl status lighttpd.service
lighttpd.service - Lightning Fast Webserver With Light System Requirements
   Loaded: loaded (/lib/systemd/system/lighttpd.service; enabled)
   Active: failed (Result: exit-code) since Sat 2000-01-01 01:36:45 UTC; 18s ago
  Process: 917 ExecStart=/usr/sbin/lighttpd -D -f /etc/lighttpd.conf (code=exited, status=255)
   CGroup: name=systemd:/system/lighttpd.service

Jan 01 01:36:45 beaglebone systemd[1]: Starting Lightning Fast Webserver With Light System Requirements...
Jan 01 01:36:45 beaglebone lighttpd[917]: 2000-01-01 01:36:45: (network.c.379) can't bind to port:  80 Address already in use
Jan 01 01:36:45 beaglebone systemd[1]: lighttpd.service: main process exited, code=exited, status=255/n/a
Jan 01 01:36:45 beaglebone systemd[1]: Failed to start Lightning Fast Webserver With Light System Requirements.
Jan 01 01:36:45 beaglebone systemd[1]: Unit lighttpd.service entered failed state

 

The webserver could not bind to port 80 because it was already in use. This was caused by another webserver already running on the Beaglebone.

 

Disabling default webserver

 

Following commands were used to disable the Beaglebone's default webserver:

 

root@beaglebone:~# systemctl disable bonescript.service
root@beaglebone:~# systemctl disable bonescript-autorun.service
rm '/etc/systemd/system/multi-user.target.wants/bonescript-autorun.service'
root@beaglebone:~# systemctl disable cloud9.service
rm '/etc/systemd/system/multi-user.target.wants/cloud9.service'
root@beaglebone:~# systemctl disable bonescript.socket
rm '/etc/systemd/system/sockets.target.wants/bonescript.socket'

 

Lighttpd was now able to start and bind to port 80 successfully. The default index page was accessible.

 

CGI/Perl support

 

With the webserver installed and running, it was time to activate the cgi modules.

 

In the lighttpd config file, I uncommented the "mod_cgi" module along with other CGI related parameters:

 

root@beaglebone:/www/pages# nano /etc/lighttpd.conf

## modules to load
server.modules              = ( "mod_access",
  "mod_cgi",
  "mod_accesslog" )

#### CGI module
cgi.assign                 = ( ".pl"  => "/usr/bin/perl",
                               ".cgi" => "/usr/bin/perl" )

 

I restarted the webserver to apply the changes:

 

root@beaglebone:/www/pages# /etc/init.d/lighttpd restart
Restarting Lighttpd Web Server: stopped /usr/sbin/lighttpd (pid 125)
2000-01-01 00:42:04: (plugin.c.169) dlopen() failed for: /usr/lib/mod_cgi.so /usr/lib/mod_cgi.so: cannot open shared object file: No such file or directory
2000-01-01 00:42:04: (server.c.676) loading plugins finally failed
lighttpd.

 

Even though I enabled the CGI module in the config file, the webserver refused to start. The module needed to be installed separately:

 

root@beaglebone:/www/pages# opkg install lighttpd-module-cgi
Installing lighttpd-module-cgi (1.4.31-r2.3) to root...
Downloading http://feeds.angstrom-distribution.org/feeds/v2012.12/ipk/eglibc/armv7a-vfp-neon/base/lighttpd-module-cgi_1.4.31-r2.3_armv7a-vfp-neon.ipk.
Configuring lighttpd-module-cgi.

 

With the CGI module now activated and installed, lighttpd was happily starting.

 

root@beaglebone:/www/pages# /etc/init.d/lighttpd restart
Restarting Lighttpd Web Server: no /usr/sbin/lighttpd found; none killed
lighttpd.

 

Testing a sample CGI/Perl page, I could validate the installation:

image

 

User interface

 

I had a pretty clear idea of how I wanted my interface to look like, but before starting the actual implementation, I made some sketches.

 

Sketches

 

For the interface, I had three main menus in mind:

  • Listen: play controls, play mode (FM or Web) and channel selection
  • Manage: managing channels (add, edit, delete)
  • Configure: possibility to configure some settings of the radio

 

Implementation

 

While making the interface, I tried to avoid static values as much as possible. The interface should work on more than this very specific LCD and specific resolution alone.

 

By defining everything in proportions, the interface should look the same (or as much as possible at least) on different devices such as pc, smartphone, tablet, and LCD cape.

 

The code is still unstable, so I'm only providing a small preview here. The full code will be available once the interface is stable and finished.

image

 

Some screenshots/pictures of the interface accessed from different devices:

 

On the LCD cape:

 

image

 

On the smartphone in landscape mode:

 

image

 

And finally, on the laptop:

 

image

 

There is still a lot of work to be done, but I hope to post the final result soon!

 

Testing

 

Below you will find a video of a small test of the interface:

 

The radio is playing in FM mode. I then press on the web icon to switch to internet radio for the same channel.

You can hear a switch, but I'm not sure the difference between FM and internet radio can clearly be heard.

After that I press the pause (should perhaps become a "stop" button) to stop playing any music.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

That's it for this week's post, stay "tuned" for more!

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 12 years ago +2
    Very nice, and good to see soneone not using python for a change
  • shabaz
    shabaz over 12 years ago +1
    Hi Frederick, Great stuff. I also agree, Apache would be way overkill. Good to choose an alternative, and lighttpd is a good one. The project is looking really good!
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    Hi Frederick,

     

    Really nice project, congrats on winning the TI prize, you're a star now !

     

    Do you intend to provide the source code of the perl script ?

    It would be a really great source of inspiration

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 12 years ago

    Hi Frederick,

     

    Really nice project, congrats on winning the TI prize, you're a star now !

     

    Do you intend to provide the source code of the perl script ?

    It would be a really great source of inspiration

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • fvan
    fvan over 12 years ago in reply to e14 Contributor

    Hi Vlad,

     

    thanks! Not sure about the star part, but it's fun making things like this!

    I link to the full source code in part 5: Beaglebone Black Radio Challenge - Part 5: Project Finalisation

    Everything should be on GitHub. Feel free to use, improve, etc ... image

     

    Frederick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to fvan

    I didn't read well enough image

    Thanks Frederick !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 12 years ago in reply to e14 Contributor

    You're welcome!