Experimenting with Extreme Environments
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Extreme Environments
  • More
  • Cancel
Experimenting with Extreme Environments
Blog ComputeCam and PicoPorch - Early Muddling
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Extreme Environments to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 22 Apr 2024 6:54 AM Date Created
  • Views 2339 views
  • Likes 10 likes
  • Comments 17 comments
  • Garden Secrets System
  • dougw
  • PicoPorch
  • compute module 4
  • MIDAS DISPLAYS MC42005A6W-SPTLYI-V2
  • Experimenting with Extreme Environments
  • Hammond Manufacturing
  • ComputeCam
Related
Recommended

ComputeCam and PicoPorch - Early Muddling

dougw
dougw
22 Apr 2024

Intro

This is the second installment of Experimenting With Extreme Environments.

I have been struggling to navigate through a maze of long and twisty rabbit holes in the early stages of this project. Although some progress is being made, it still feels like there are a lot of unknowns to resolve.

This blog includes scattered tidbits of interest  about what I have been up to, just to show some progress, but most of the hard slogging and dead end efforts aren't exciting enough to make it into the blog.

Computers and Cameras

Here are some early descriptions of the computers and cameras that will be used in the project:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Camera Action

Here is a demo of 3 cameras in action:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The PicoPorch Panning System

Here is some preliminary work on the Pi Pico camera panning controller and Midas display:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Of course this needs to work with a Pico W, but the one I ordered has not arrived yet.

Discussion

There is still a lot of work to do to explain what was done to get these results, but there are a lot of aspects that are not finalized yet, so this blog has been more of a series of teasers about what is happening on the project and what is to come.

So far I have ordered a lot of parts, but there are still many that have not arrived. It is tough to design with parts that are not here and have no datasheets. I have designed and 3D printed at least 10 parts, but there are quite a few still not started.

One custom PCB has been received, the other one had to wait until a breadboard circuit was proven, so it is going to be late - hopefully it arrives before the project deadline.

Two Hammond boxes have been modified to house Raspberry Pi Zero 2W computers with Pi cameras. These boxes are handy since these modules get warm and 3D printed housings might sag with the heat. I have made some mods to one of the 3 clear lid Hammond enclosures, and started designing the insert structure, but there is a long way to go on that front.

The next immediate step is to design and build the motorized panning mechanism, even though the Pico W has not arrived.

Links:

  • Garden Secrets System
  • ComputeCam and PicoPorch - Early Muddling
  • PicoPorch and ComputeCam - The Motor System
  • PicoPorch - LCD PCB & Bezel
  • PicoPorch power wiring
  • PicoPorch Motor Controller Demo
  • PicoPorch System Demo
  • PicoPorch Final Touches
  • Deep Dive On Kit Components
  • Backyard Secrets 1
  • MotionEyeOS Tutorial
  • Garden Secrets Project Summary
  • Experimenting with Extreme Environments Design Challenge
  • Pi 4 Compute Module Datasheet
  • Pi 4 Compute Module I/O Board Datasheet
  • Midas Display Datasheet
  • Enclosure Drawing
  • Enclosure Manufacturer Page
  • Antenna Datasheet
  • Connectors Datasheet
    • Sign in to reply

    Top Comments

    • DAB
      DAB over 2 years ago +1
      Great start Douglas.
    Parents
    • javagoza
      javagoza over 2 years ago

      Thanks for sharing your progress and problems encountered. I'm not using the cameras, but I've checked the motionEyeOS image repository and it appears to be a dead project. There have been no updates for two years and it appears that an image for the compute module 4 (CM4) was never built.

      I would try to try the project https://github.com/motioneye-project/motioneye which seems more standard and I think it will work on the CM4 with the Raspberry OS. It's just a proposal, I haven't tried it. Good luck!

      • Cancel
      • Vote Up 0 Vote Down
      • Sign in to reply
      • More
      • Cancel
    • dougw
      dougw over 2 years ago in reply to javagoza

      I will keep plugging away at the CM4 to see if I can figure something out. The standard Raspberry Pi OS has built-in camera support but I can't even get that working. You are right about the motionEyeOS - it doesn't even work with the Pi Zero 2, but I have found a 3rd party build that does work with Pi Zero 2.

      • Cancel
      • Vote Up 0 Vote Down
      • Sign in to reply
      • More
      • Cancel
    • ralphjy
      ralphjy over 2 years ago in reply to dougw

      I used it with the Pi Zero 2 W a couple of years ago /members-area/personalblogs/b/ralph-yamamoto-s-blog/posts/raspberry-pi-zero-2-w---motioneyeos, but the fork I used also does not appear to have been updated since then.  I'll be interested to see if you get it working with the CM4.

      • Cancel
      • Vote Up 0 Vote Down
      • Sign in to reply
      • More
      • Cancel
    • javagoza
      javagoza over 2 years ago in reply to javagoza

      With  Debian Bookworm any code that uses a library added via the pip utility should be added and executed inside a virtual environment.

      You can do the following:

      • Open a terminal window and create a new directory:
      mkdir MyWorkingDirectory
      • Enter the new directory with:
      cd MyWorkingDirectory
      • Create a new virtual environment that inherits all currently installed packages with:
      python -m venv --system-site-packages env
      • Enter the virtual environment with
      source env/bin/activate
      • Your command line prompt should now have a prefix of (env)
      (env) _
      • We can now use pip to install :
      (env) pip install ...
      (env) pip install ...
      ...
      • If you need to exit the virtual environment, execute deactivate from the command line.
      (env) deactivate
      • To reenter the virtual environment simply execute source env/bin/activate again from inside the  MyWorkingDirectory folder.
      source env/bin/activate
      (env) _


      I have had to do this to include the libraries that I am using in my solution, such as the TensorFlow library, to perform the classifications of the recorded audios.

      • Cancel
      • Vote Up 0 Vote Down
      • Sign in to reply
      • More
      • Cancel
    • dougw
      dougw over 2 years ago in reply to ralphjy

      I am thinking CM4 may need to use a different video streaming method all together.

      • Cancel
      • Vote Up 0 Vote Down
      • Sign in to reply
      • More
      • Cancel
    • ralphjy
      ralphjy over 2 years ago in reply to dougw

      Hi dougw ,  I finally got a heatsink for the CM4 so I'm starting to verify that all the RPi4 stuff works.  I wanted to try out the camera to see if I was going to have problems like you have.  My only surprise is that I guess I wasn't paying attention and didn't realize that the CM4 uses a RPi Zero style 22p FFC.  So, I had to swap the cable that I was using with the RPi4.

      It sounds like you are having functional problems getting the camera to work.  The camera is working okay for me.  I am able to run programs using the Picamera2 library and also use the libcamera apps.  I also ran a simple object detection model.  I am using a different camera (Arducam Pi Camera 3) than you, but I also do not autodetect the camera.  I specify it explicitly in /boot/firmware/config.txt.  I thought I might have to edit the file to indicate that I am using cam1, but it wasn't necessary.  Maybe if I add another camera...

      Can you see your camera if you run libcamera-hello --list?  It is interesting that my camera enumerates as 0 even though I'm using the cam1 connector.

      image

      I tried strreamng via TCP to VLC on my Windows computer.  It does work, but I do see occasional tearing in the image.  ffplay doesn't seem to be working on my PC, so I may have to reinstall it.  I did not try streaming the camera on the RPi4 so can't compare.  Maybe I'll try later.

      • Cancel
      • Vote Up 0 Vote Down
      • Sign in to reply
      • More
      • Cancel
    • dougw
      dougw over 2 years ago in reply to ralphjy

      libcamera-hello does not find any cameras. I have tried 3 different Pi cameras and cables, all of which work on other Pi systems...Disappointed

      • Cancel
      • Vote Up 0 Vote Down
      • Sign in to reply
      • More
      • Cancel
    Comment
    • dougw
      dougw over 2 years ago in reply to ralphjy

      libcamera-hello does not find any cameras. I have tried 3 different Pi cameras and cables, all of which work on other Pi systems...Disappointed

      • Cancel
      • Vote Up 0 Vote Down
      • Sign in to reply
      • More
      • Cancel
    Children
    • ralphjy
      ralphjy over 2 years ago in reply to dougw

      Hope that you have been able to resolve your problem.

      Just one final piece of info.  I had a V2 camera attached to a Pi Zero W and I tried it on the Cam0 port (added the jumpers and the config.txt entry).

      And it came right up.  I used two terminal windows to run two rpicam-hello preview windows (resized to 640x480). V3 on the left.

      image

      • Cancel
      • Vote Up 0 Vote Down
      • Sign in to reply
      • More
      • Cancel
    • dougw
      dougw over 2 years ago in reply to ralphjy

      I will try the CAM 0 port with jumper...

      I have the config set for autodetect at the moment.

      • Cancel
      • Vote Up 0 Vote Down
      • Sign in to reply
      • More
      • Cancel
    • ralphjy
      ralphjy over 2 years ago in reply to dougw

      I didn’t use autodetect because apparently it does not detect the Arducam V3 (per the documentation).  I’ve also read that autodetect might not work for cam0.  Of course, who knows what version of the firmware that applies to.  Documentation is confusing because things have been changing over time.