In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Blog [AirCare] InTheAir - Week 13: GP2Y10 BoosterPack
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
  • Author Author: fvan
  • Date Created: 25 Jan 2015 8:08 PM Date Created
  • Views 1958 views
  • Likes 3 likes
  • Comments 7 comments
  • eclipse_iot
  • mqtt
  • openhab
  • beaglebone_black
  • internet_of_things
  • in_the_air
  • texas_instruments
  • iot_sensor_nodes
  • cc3200
  • launchpad
Related
Recommended

[AirCare] InTheAir - Week 13: GP2Y10 BoosterPack

fvan
fvan
25 Jan 2015

Previous posts for this project:

  • [AirCare] InTheAir - Project Description
  • [AirCare] InTheAir - Week 1: Getting a Launchpad to Blink
  • [AirCare] InTheAir - Week 2: Preparing the Beaglebone Black
  • [AirCare] InTheAir - Week 3: Fuel Tank Testing
  • [AirCare] InTheAir - Week 4: Using the CC3200
  • [AirCare] InTheAir - Week 5: openHAB and MQTT
  • [AirCare] InTheAir - Week 6: Accessing Fuel Tank's Data
  • [AirCare] InTheAir - Week 7: Dust sensor
  • [AirCare] InTheAir - Week 8: MSP430FR5969 with Energia14
  • [AirCare] InTheAir - Week 11: CC3200, Energia and analogRead()
  • [AirCare] InTheAir - Week 12: Automatically starting some things

 

  • Introduction
  • Templates
  • Eagle

 

Introduction

 

In the past weeks, I experimented with the GP2Y10 dust sensor from Sharp. Using an Arduino all was well, but I was however running into problems when using it with the CC3200. It's not the only issue I encountered with the CC3200. There was also the fact that the I2C pins of the CC3200 and FuelTank did not match.

 

I've tried to tackle both issues with a custom BoosterPack (my first!).

 

 

Templates

 

To start, I searched for BoosterPack templates. I quickly came across the ones from TI: Build Your Own BoosterPack for TI LaunchPad

 

The BYOB kit from TI contains a variety of files for different tools: Eagle, Fritzing, ... Very nicely done and easy to find!

 

 

Eagle

 

Using Eagle, I created a schematic and board. Now, I don't have much experience with Eagle. I did fiddle a bit with it during the Forget Me Not challenge, but never got to making an actual PCB. Fritzing seems to be more up my alley, but anyway ... let's proceed.

 

I loaded all the required parts in the schematic and started connecting all the dots. There are four parts to this schematic:

  • the opamp circuit as suggested by shabaz in Week 11
  • the circuit required to hook up the dust sensor
  • the launchpad headers
  • an optional I2C connection to overcome the mismatch between FuelTank and CC3200

 

This is the schematic:

image

 

For the board, I laid out the components across the available space and let Eagle do the routing. This is the resulting board:

image

 

Nothing spectacular, but I'll be more than happy if I manage to get it soldered and working image

  • Sign in to reply

Top Comments

  • DAB
    DAB over 11 years ago +3
    I remember hand drawing board layouts and then having the graphics folks lay down the traces with ink before we could do a photo transfer to a board. You guys have it much easier today. DAB
  • Jan Cumps
    Jan Cumps over 11 years ago +2
    fvan , I've also created a FuelTank-to Standard adapter for the Hercules LaunchPad MK I, Mine was just a pin-rerouting - no additional functionality like your boosterpack . Loaded it to OSHPark, and never…
  • shabaz
    shabaz over 11 years ago +1
    Hi Frederick, Great stuff. Looking forward to seeing the assembled board!!
Parents
  • DAB
    DAB over 11 years ago

    I remember hand drawing board layouts and then having the graphics folks lay down the traces with ink before we could do a photo transfer to a board.

     

    You guys have it much easier today.

     

    DAB

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 11 years ago

    I remember hand drawing board layouts and then having the graphics folks lay down the traces with ink before we could do a photo transfer to a board.

     

    You guys have it much easier today.

     

    DAB

    • Cancel
    • Vote Up +3 Vote Down