On the Line
  • Challenges & Projects
  • Design Challenges
  • On the Line
  • More
  • Cancel
On the Line
Forum SolarSense - Part 5 - Making an Live Dashboard using Lab View
  • News
  • Projects
  • Forum
  • DC
  • Leaderboard
  • Files
  • Members
  • More
  • Cancel
  • New
Join On the Line to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 37 subscribers
  • Views 198 views
  • Users 0 members are here
  • design challenge
  • labview
Related

SolarSense - Part 5 - Making an Live Dashboard using Lab View

arvindsa
arvindsa 4 months ago

Recap:

I'm building a smart solar monitoring system that uses three panels with a clean reference to eliminate weather effects and directly measure dust-induced losses in real time. One panel stays pristine as a baseline, and comparing the two under identical sky conditions gives a performance ratio that reveals soiling immediately. The goal is to use environmental sensors and edge AI to predict exactly when cleaning is needed, before efficiency drops enough to impact revenue. This beats fixed-schedule cleaning or waiting for output to degrade.Also this is complementary to my Master's thesis of a minute Shape memory Alloy based solar panel cleaning robot

Previous posts:

  • SolarSense - Part 1 - Introduction, The POC Built and The Plan
  • SolarSense - Part 2 - Can Arduino CAN?
  • SolarSense - Part 3 - PCB Schematics Walkthrough
  • SolarSense - Part 4 - CAN Protocol Deep Dive and Implementation

Hello Lab View, Haven't seen you since my Undergrad

The last time I used Lab View was during my Undergraduate academics in Control Lab, I never was a fan of high level graphical style programming plus all of my work never required Lab View, so I was happy until this challenge came up. On the bright side, I am happy to say that there is Community version available. I don't remember seeing the community when I used it. Without any research of what is the difference between Community vs Professional was, I went to the community version. Obviously to activate the Community version, I had to create an account. It was No mess, No Fuss  Installation.

In this post, the aim will be to create a dashboard to show values published by the Arduino Q via TCP packets. These will include, the Solar panel outputs, The Environmental parameters such as UV, AQI, Humidity and then the system parameters such as battery, Error flags etc. 

Getting A Gauge up and Running

The Python Code

I made a quick code to keep sending values 4 times a second. Apologies for no comments.

import math
import socket
import threading
import time

HOST = "0.0.0.0"
PORT = 9000
UPDATE_INTERVAL = 0.25


def read_value(t: float) -> float:
    return round(50 + 45 * math.sin(t / 3.0), 2)


def handle_client(conn: socket.socket, addr) -> None:
    print(f"[+] client connected: {addr}")
    start = time.monotonic()
    try:
        while True:
            value = read_value(time.monotonic() - start)
            conn.sendall(f"{value}\r\n".encode("ascii"))
            time.sleep(UPDATE_INTERVAL)
    except (ConnectionResetError, BrokenPipeError, OSError):
        pass
    finally:
        conn.close()
        print(f"[-] client disconnected: {addr}")


def main() -> None:
    with socket.socket(socket.AF_INET, socket.SOCK_STREAM) as server:
        server.setsockopt(socket.SOL_SOCKET, socket.SO_REUSEADDR, 1)
        server.bind((HOST, PORT))
        server.listen()
        print(f"Gauge TCP server listening on {HOST}:{PORT}  (Ctrl+C to stop)")
        try:
            while True:
                conn, addr = server.accept()
                threading.Thread(
                    target=handle_client, args=(conn, addr), daemon=True
                ).start()
        except KeyboardInterrupt:
            print("\nShutting down.")


if __name__ == "__main__":
    main()

The Front Panel of Lab View

A Plain Gauge with range 0-100 and a Stop button

image

Block Diagram

When Creating a VI, it opens two window, one is the UI Editor and the other is the Block Diagram Editor. The Block diagram is where is the logic is executed.  I Referred to the YouTube video https://www.youtube.com/watch?v=LMtdLqmRnVU to make the TCP Communication logic. One thing to note is that for all Inputs and Outputs to work in a loop, it has to be in the loop, else only the value of input at the start of first iteration of the Loop will be used. Any changes or presses to the Buttons will not be considered. 

image

The Result

10mins into Lab View, I have a live dashboard. 

image

Building the Actual Panel

To get a full picture of the situation I need to have the following data

Variable Type Unit Range
panel_efficiency[0] DBL % 0–100
panel_efficiency[1] DBL % 0–100
panel_efficiency[2] DBL % 0–100
soiling_ratio DBL % 5.0–29.0
battery DBL % 0–100
tank_level DBL % 0–100
humidity DBL % 10–70
temperature DBL °C 13–37
uv DBL Index 2.0–8.0
aqi INT µg/m³ 20–80
status_ok INT — 0 or 1
error INT — 0 or 1

These data will be sent as a JSON over TCP. For testing, i will be randomizing the values such that they oscillate between minimum and maximum.

{
  "panel_efficiency": [25.5, 24.8, 22.3],
  "soiling_ratio": 15.2,
  "humidity": 65.0,
  "temperature": 28.5,
  "uv": 6.2,
  "aqi": 55,
  "battery": 78.4,
  "status_ok": 1,
  "error": 0,
  "tank_level": 78.4
}

The Front Panel

image

The Block Diagram

www.youtube.com/watch

This is where I started running into trouble. I initially thought the Unflatten from JSON block would simply split the JSON into key–value pairs, but it wasn’t that straightforward. I had to declare the structure of the expected JSON format using a cluster definition—the long vertical box to the left of the while loop. I was able to get this working by referring to a YouTube video https://www.youtube.com/watch?v=kx1E5QnnLy0. However, I ran into another issue when declaring a Boolean. For some reason, I couldn’t find the Boolean type. To save time, I modified the Python code to send the status flags as 0/1 integers instead of Booleans.

I assumed I could use an integer-to-Boolean conversion block while reading the JSON from the server, but I couldn’t find such a block either. As a workaround, I ended up using the “If Not Equal” comparison block instead. I also noticed that the UI started being slow. Not sure why.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

image

The Final Working

image

I have not been able to get the XY Graph to work yet, But to me, It's a stretch goal which i added impromptu Hopefully I should get it working by the deadline.

Final Notes. 

I had some time reminiscing my college days using Lab View, fighting with my classmates to claim the limited number of floating license of Lab VIew, Coordinating with my friends so that They will claim the license the second I surrender mine back into the common pool,  Getting the dashboard to work was probably the easiest part, but I still had fun. The PCB for the data collection has completed fabrication and is on the way, it should be with me in a day or two, I am still using the old POC to keep the data collection alive till then. 

  • Sign in to reply
  • Cancel
  • DAB
    DAB 4 months ago

    Nice update.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • arvindsa
    arvindsa 4 months ago in reply to DAB

    Thank you Slight smile