Path to Programmable 3
  • Challenges & Projects
  • Design Challenges
  • Path to Programmable 3
  • More
  • Cancel
Path to Programmable 3
Blog 5. LED Blink Part-5: Thoughts on all previous LEDs
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Path to Programmable 3 to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: rajivbishwokarma
  • Date Created: 27 Jul 2023 7:06 AM Date Created
  • Views 811 views
  • Likes 5 likes
  • Comments 2 comments
  • fpga
  • Ultra96-V2 Board
  • Path to Programmable 3
  • Training blog
Related
Recommended

5. LED Blink Part-5: Thoughts on all previous LEDs

rajivbishwokarma
rajivbishwokarma
27 Jul 2023

Introduction

I could have done so much more with the Ultra96v2 board, I stuck with the theme of LED blinking through different ways and although it is not too fancy, one thing that I have noticed is that I spend too much time when it comes to creating something new. For example, rather than testing an already verified design in a new environment, what I have found myself doing is that I create new designs and start playing with those and when they don’t work (even if they are fun, that’s bad practice), I spend too much time debugging only to find out that I set something in an incorrect way. That was why I wanted to take this opportunity to actually create a set of tested designs that I can run and verify that new environments that I am working with are actually set correctly.

We have seen four (3 actually) ways we can blink LEDs in Ultra96v2 board, and I find this board to be really interesting and the only (for a board of this kind) complain that I have is the lack of accessibility of the clock directly from the PL (or maybe it’s just me who could not figure out how). I have to admit though that for a board of this size, too much complexity would have driven the cost much higher, so designers had to make some adjustments.

This final blog is more of a thought process and reflection on last four LED blinking blogs. The original plan was a bit different as I had planned to do one custom petalinux based LED blinking but because I did not have enough time to fix the errors that I was getting while building the petalinux based design, I had to leave it at that. But that is okay because if not for that, I would not have thought of actually doing a reflection-based blog post.

If you have followed what I did, then let’s do a bit of reflection on each topic.

  1. 4-bit ARM

    This was supposed to be the second blog but while I was doing the PYNQ numbers blog, I realized that the natural progression would be to initialize the design and then to add an AXI IP and then extend that AXI IP to PYNQ. Therefore, I changed the order just while I was finishing up. I wanted to do something more interesting with this one though: I wanted to create a LED blinking with all the cores in parallel. Because of the limited time, I could only do so much but that is something that I look forward to doing sometimes soon.

    Blog: (+) 1. LED Blinking Part 1: 4-bit ARM - element14 Community

    Demo: https://youtu.be/U13CskNeo-g

  2. FPGA flashes Police Lights

    This was supposed to be the first blog and I only came up with the title after I was done with this project. While I was just doing some of my other works, it just came to me that the LED blinking pattern was somewhat similar to that of a Police car light. Initially, I just wanted to use the FPGA and no PS for this task, but I just could not make it work. I also thought of adding an external LED, but I decided against it for the time being (I might do it in the future).

    Blog: (+) 2. LED Blinking Part 2: FPGA flashes Police Lights - element14 Community

    Demo: https://youtu.be/J5f8HpWGUiw

  3. 256 PYNQ Numbers

    Now, this was a very interesting project. PYNQ offers a lot of flexibility when it comes to doing AI related stuffs, unlike C/C++, Python has a much wider community support. And, being able to instantiate the FPGA IP is something that is precious to save prototyping timing. Although we have to move to C++ for production design, it still has great benefits. Now, back to the project. I had initially created another LED board, spending more time than I thought I would, and it had different colored LEDs (RED, BLUE, GREEN, WHITE, YELLOW). But after finishing it up, I tested it and I only could get the YELLOW and RED to light up. The 1.8V obtained from the low-speed expansion header in the Ultra96v2 is nowhere enough to light those others up. Therefore, I just created a simple RED LED breadboard circuit and then tested the design.

    Blog: (+) 3. LED Blink Part-3: 256 PYNQ Numbers - element14 Community

    Demo: https://youtu.be/T47WlpKiQ8Q

  4. Counting using AI

    This was another exciting project. The tutorial was easy enough but fixing those issues while doing it in another custom board is another topic. I wanted to continue this and do a LED blinking at the end, but I did not have enough time. I will see if I can continue this sometime soon (hopefully).

    Blog: (+) 4. LED Blink Part-4: Counting using AI - element14 Community

Conclusion

This concludes all my blogs for the training. Although I had thought of doing so many things, I was only able to finish this much. Hopefully, the big project is still up, and I will enjoy creating and writing about that. See you in the final blog!

  • Sign in to reply
  • rajivbishwokarma
    rajivbishwokarma over 3 years ago in reply to saadtiwana_int

    Thanks! I did, indeed. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • saadtiwana_int
    saadtiwana_int over 3 years ago

    It's Ok...the main purpose of these programs is for people to learn! And looks like you learnt quite a few new things so I think the objective is achieved!