PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog Hologram Pi-ramid - PCB Design
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
  • Author Author: luislabmo
  • Date Created: 19 May 2019 7:17 PM Date Created
  • Views 3259 views
  • Likes 9 likes
  • Comments 6 comments
  • pla
  • acryllic
  • picasso
  • touch screen
  • diy pcb
  • rpi 3b+
  • addressable led
  • raspberri pi
  • plexiglass
  • rgb
  • luislab
  • acrylic_welding
Related
Recommended

Hologram Pi-ramid - PCB Design

luislabmo
luislabmo
19 May 2019

After a successful Pepper's Ghost test, my next step in the project build is to work with some of the electronics.

 

When I was researching and collecting ideas to include in the design of the Hologram Pi-ramid, I really wanted it to be able to work in a similar fashion to the 2D/3D Holographic Displays commercially available, where the holographic 3D content (visual effects, animations, information) is combined with a physical object placed inside the hologram generator; this is perhaps the main reason why it has room for a few of electronics components explained below:

 

Top RGB lights

2 x WS2812B addressable RGB lights will be mounted on top of the object on a small foot print PCB; 25.4mm x 12.954mm (1in x 0.51in)

{gallery:width=480,height=384,autoplay=false} Top RGB lights

image

Top RGB lights: Hologram Pi-ramid top RGB lights pcb layout

image

Top RGB lights - schematic: Hologram Pi-ramid top lights schematic

image

Top lights location: Location of top RGB lights pcb

 

Front RGB lights

3 x WS2812B addressable RGB lights will be mounted on a small pcb located near the bottom-front of the Acrylic pyramid; 51.181mm x 6.35mm (2.015in x 0.25in)

{gallery:width=480,height=384,autoplay=false} Front RGB lights

image

Front RGB lights: Hologram Pi-ramid - front RGB lights pcb layout

image

Front RGB lights - schematic: Hologram Pi-ramid front lights schematic

image

Front lights location: Location of front RGB lights pcb

 

Bottom Stand Adapter

The Bottom Stand Adapter contains four generic connections to connect basically "anything" inside the pyramid that contains electronics as long as it only requires a maximum of 4 pin connection; lets say power and/or two data signals. It can be an object with complex electronics, I2C communication, another group of WS2812B leds, etc.; 27.673mm x 10.16mm (1.09in x 0.4in)

{gallery:width=480,height=384,autoplay=false} Bottom stand adapter

image

Bottom stand adapter: Hologram Pi-ramid bottom stand adapter pcb layout

image

Bottom stand adapter - schematic: Hologram Pi-ramid bottom stand adapter schematic

image

Bottom stand location: Location of bottom stand adapter pcb

 

Some redesign

On the initial Hologram Pi-ramid design, I had in mind including side RGB lights. These lights may shine right in front of someone looking inside the pyramid from the sides, disturbing the hologram perception so this idea was discarded.
image

Fusion 360 has many awesome features, one of them is that I can suppress features in the history of the design without having do a complex redesign, in this case I can now remove the placement for the side RGB lights from the design like it was never there.

image

Now the feature is suppressed from the design with just one easy step. Awesome!.

image

 

 

Blogs in this series

 

  1. Hologram Pi-ramid - Intro and initial design
  2. Hologram Pi-ramid - 3D CAD/CAM design
  3. Hologram Pi-ramid - 3D printed parts and initial assembly
  4. Hologram Pi-ramid - Plexiglass Pyramid
  5. Hologram Pi-ramid - My name is Automan
  6. Hologram Pi-ramid - PCB Design
  7. Hologram Pi-ramid - Painting the 3D printed parts
  8. Hologram Pi-ramid - Electronic Parts
  9. Hologram Pi-ramid - Displaying Holograms
  10. Hologram Pi-ramid - Project complete!

 

  • My Picasso Design Challenge entries

 

 

image
My name is Automan

image
Painting the 3D printed parts

  • Sign in to reply

Top Comments

  • luislabmo
    luislabmo over 7 years ago in reply to three-phase +2
    Thank you Donald!. I feel amazed every time I put new tips/tricks to use in Fusion 360, it definitely has made my projects easier to accomplish. Luis
  • e14phil
    e14phil over 7 years ago +2
    Nice... even the logo is a nice touch!
  • three-phase
    three-phase over 7 years ago +1
    Neat update to your project and a very useful tip on the use of Fusion 360 that some will find very useful. Keep up the good work. Kind regards.
  • three-phase
    three-phase over 7 years ago

    Neat update to your project and a very useful tip on the use of Fusion 360 that some will find very useful.

     

    Keep up the good work.

     

    Kind regards.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<