Pi Chef Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Pi Chef Design Challenge
  • More
  • Cancel
Pi Chef Design Challenge
Blog KCON - Pi Chef Challenge UnBoxing Blog
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
  • Author Author: jkutzsch
  • Date Created: 28 Jan 2018 1:06 AM Date Created
  • Views 1318 views
  • Likes 8 likes
  • Comments 2 comments
  • pi chef design challenge
  • kitchen
Related
Recommended

KCON - Pi Chef Challenge UnBoxing Blog

jkutzsch
jkutzsch
28 Jan 2018
  1. Intro Blog
  2. Unboxing   <<<---
  3. Setup
  4. Gourmet Install
  5. Load up some Recipes!
  6. Enclosure Planning.
  7. 7inch Touchscreen Time
  8. AIY Build / Google Voice
  9. AIY API & Certs
  10. Succes with Google AIY!

 

Welcome to my second blog where I get to share with you, all of the goodies that UPS finally delivered to my door!

 

image

 

At long last the kit parts have arrived!  Due to Holiday craziness the one item that was expected to be late actually came earlier then the rest of the kit!

 

image

 

Here we have the Raspberry Pi Camera V2.  These had been separated from the other Kit items.  Element 14 was kind enough to express ship this item to all of us to ensure we can proceed with minimal delay.  Thank you Element 14!  It is hard to work the various Holidays into shipping schedules, especially when sometimes it seems there is no impact and other times everything grinds to a halt.

 

image

 

Opening "the box" reveals a nice little Element 14 bag full of goodies!

 

image

 

The first item out of the bag is a Universal Power Supply.  This is nice since it provides a known good power source for this project without me needing to perhaps cannibalize another project.  I may end up needing a custom solution later but this item is perfect for setting up the test bench and beginning the time of fun.

 

image

 

The next item is a very important item indeed.  The Raspberry Pi 3 Model B!  I can't wait to get this powered up with my Universal Power Supply.

 

image

 

The 4DPI-24-Hat, a 2.4" HAT that acts as a Primary Display for the Raspberry Pi. 

 

image

 

The PiFace Digital 2, a nice little addon board for the Raspberry Pi with relays, switches, input, output and even 8 LED indicators.

 

image

 

The Explore-NFC-WW board, an interesting addon to allow Near Field Communication interaction.

 

image

 

The Raspberry Pi SenseHat. an addon that provides a variety of additional data input that was comprehensive enough to warrant it's own Space Project!

 

image

 

32GB MicroSD card preloaded with NOOBS for Raspberry Pi.  This should be more than ample for my project.

 

image

 

Here are all of the Kit items laid out on the Element 14 bag.  Very promising!

 

image

 

Finally, while not provided by Element 14, I thought this project warranted a slightly larger screen option so I am using the Element 14 7" Touchscreen Display for the Raspberry Pi.  I may look for an even larger option in the future such as 10" but I have worked with the 7" in the past and believe it is a solid item to incorporate into this project.

 

Thank you for watching me progress with this Challenge and I look forward to documenting the next steps in getting my base Console up and running.

  • Sign in to reply
Parents
  • three-phase
    three-phase over 8 years ago

    Nice update, good luck with progressing through the project.

     

    Kind regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • three-phase
    three-phase over 8 years ago

    Nice update, good luck with progressing through the project.

     

    Kind regards