Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog PDU #8 - Different Direction [Upcycle It]
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
  • Author Author: jasonwier92
  • Date Created: 15 May 2017 12:03 PM Date Created
  • Views 1663 views
  • Likes 6 likes
  • Comments 7 comments
  • upcycled_pdu
Related
Recommended

PDU #8 - Different Direction [Upcycle It]

jasonwier92
jasonwier92
15 May 2017

Change Never Changes

 

I have lots of ideas, but I need to get this project moving along, so I have started down the final path, but started more fresh than before.  I have decided to use the other Edison and the mini-board since I am putting all of this in a 1U enclosure.  Here are my hardware plans going down the stretch.

 

Outlet Switching

 

I am going to use an eight port version of the relay module posted right below. I have the module, but it is wired up currently for testing as I have just finished testing my circuit I am going to build to control this set of relays.

 

image

 

Now with these Opto-isolated relay modules, the pins need to be floating or tied to 5V to be off and connected to ground to be in a on state.  For this I have wired up a simple inverter circuit that helps me with another problem with the mini and that is 1.8V.

 

image

 

This is one of eight I will use to control the 8 relays on the board for the 8 outlets.  The LEDs will go the front of the unit it display power status to each outlet. I plan on making this control board to plug into the relay circuit to keep the wire count to a minimal.

 

Edison Mini-board

 

I have added a header to the bottom of the Mini-board and that will plug into another board for power and GPIO. That other board will be mounted inside the PDU, so that the Edison is easily removed if need be.

image

 

Only other thing I need to control is the LCD that will be mounted in the PDU. I will use the Adafruit 4-Bit Level Converter for to bring the I2C 1.8V to 5V fro the LCD.

 

image

  • Sign in to reply

Top Comments

  • Workshopshed
    Workshopshed over 9 years ago +3
    The header on the bottom of the mini-board is a brilliant idea!
  • gpolder
    gpolder over 9 years ago +3
    I'm using a Sparkfun level converter, Looks like its circuit is the same as the Adafruit, featuring the BSS138 FETs. Only the color of the board is different. In my case the Sparkfun works like a charm…
  • jasonwier92
    jasonwier92 over 9 years ago in reply to Workshopshed +2
    Thank you! I have seen partial headers and I have seen male headers, but I wanted female so the pins do not get bent on the part I do not want to solder often.
Parents
  • mcb1
    mcb1 over 9 years ago

    I like the header idea.

     

    The relay board has the option of removing the jumper and adding 1.8v.

    You would need to bypass the onboard LED and reduce the resistor, but it might work.

     

    Perhaps I need to try it ....image

     

    It wouldn't give you the LED for the front panel, so your transistor interface is a good compromise.

     

     

    BE AWARE

    While the relays are rated at 10A, often the pcb is NOT.

    You may wish to solder a heavy solid wire to reinforce the current carrying capabilities of the track.

     

    Hopefully your unit has the slot around the common terminal of the contacts as this one does.

    image

     

     

    For this project, everything is inside the unit, but the normal mains safety advice applies to ensure that you don't end up with a mains voltage where it shouldn't be.

    Make sure the ground is tied to chassis to ensure you can't get a shock, and be very careful when the lid is open.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jasonwier92
    jasonwier92 over 9 years ago in reply to mcb1

    My relay module look just like that one.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to jasonwier92

    My relay module look just like that one.

    Great.

    I'd strongly suggest you add a piece of wire (solid is fine) to increase the current carrying capability.

    You can detail that this is required and just show one to demonstrate the process ....

     

    Basically any of the parts should be capable of carrying whatever the input power allows ... something along the cliché of the weakest link...

     

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 9 years ago in reply to jasonwier92

    My relay module look just like that one.

    Great.

    I'd strongly suggest you add a piece of wire (solid is fine) to increase the current carrying capability.

    You can detail that this is required and just show one to demonstrate the process ....

     

    Basically any of the parts should be capable of carrying whatever the input power allows ... something along the cliché of the weakest link...

     

     

    Mark