Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog UpCycle It - R2I - #1 - Introduction
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
  • Author Author: jkutzsch
  • Date Created: 24 Mar 2017 2:24 AM Date Created
  • Views 2976 views
  • Likes 6 likes
  • Comments 16 comments
  • incubator
  • upcycle it design challenge
  • upcycle_it_r2i
Related
Recommended

UpCycle It - R2I - #1 - Introduction

jkutzsch
jkutzsch
24 Mar 2017

UpCycle IT – R2I INDEX:

 

Blog #1_”Introduction”

Blog #2_”Designing”

Blog #3 "The Kit"

Blog #4_"Mother Natures Version"
Blog #5_"Research"
Blog #6_"Competition01"

Blog #7_"Edison Setup"

Blog #8_"Edison 2 Ardunio"
Blog #9_"Grove-ON"
Blog #10_"Hot2Not"

UpCycle It - R2I –Refrigerator 2 Incubator

Refrigerators, everyone loves them, they keep your food cold, extend the life span of meats and dairy and when they stop working, take up a LOT of space.

Here in the U.S. you have to pay a lot of extra charges to have refrigerators properly disposed of.  Undoubtedly one of the reasons you will see them laying in vacant lots and piled outside of buildings in low income areas.  No one wants to deal with them after they can no longer keep items cold.

 

image

I found an online news article that discussed how second hand refrigerators being imported into Ghana from the European Union reached such a critical mass point that on January 1st 2013 they banned the import of all used refrigerators, freezers and air conditioners.

While newer model systems avoid the old issues of chlorofluorocarbons (cfc) which can damage the ozone layer they can still provide quite an impact on land fills and similar disposal options due to their size and quantity.

As such I am taking an old mini-fridge and using it as the main part of my Upcycle project!  Something that later can be expanded to full sized items easily by anyone desiring to do so.  (In fact I also have another plan to take a full size standing freezer with glass door and Upcycle that in the future but I was unable to find a donor freezer and so that will wait for a future blog posting to Element 14.)

 

image

 

Here is the basis of my project getting a much needed cleaning prior to tear down.

 

image

Here is the door removed, inside compartments of door removed and beginning of inside tear down.  The fridge is actually upside down here since I was cleaning up parts to get ready for a professional to remove the compressor and cooling systems.

image

The Fridge ready to start having items added and tested for the R2I project!

image

The rear showing the compressor and various parts removed and a nice open space in the back.

image

Here is Blue Dude showing us the next piece of the project, eggs!

My idea is to take the Challenger Kit comprising of the IntelRegistered Edison Kit for Arduino, IntelRegistered Edison Breakout Board, Arduino Protoshield R3, the Grove Starter Kit for Arduino, an AC/DC power supply and a USB cable.  Add my stripped and cleaned up mini-fridge, a heating element (looking at heating tape), a custom designed egg turning assembly and of course a dozen or more fertilized chicken eggs to have an Incubator.

 

I want to use as many of the Grove Starter Kit pieces as possible in the incubator (such as the mini-servo, led lights, relays, temperature sensor) but believe I will need to add a high quality humidity sensor as well since I am not seeing such an item reflected in the literature on the kit.

image

Here is a general idea with the Heat tape along the back.  The custom egg holder/rotator going from side to side and there being a divider across the center of the fridge to allow heat to be kept at the top side with a possible use of the bottom for holding the kit.

In addition I will cut a viewing window in the door and replace with plexi-glass to allow us to monitor everything without having to open the device and upset the temperature/humidity.

The Intel Edison Kit looks to be a great option for implementing all of my desired features and I look forward to taking this to the next step and blogging as we create this Upcycle Project.  Ultimately to take it through the incubation of chicken eggs to show success!  I see great video opportunities!

  • Sign in to reply

Top Comments

  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago +2
    A tip would be to ensure the plastic of the fridge interior will take the heat from the tape If you are planning on using Mains powered heaters this become more critical as a failure could lead to injury…
  • mcb1
    mcb1 over 9 years ago in reply to jkutzsch +2
    The 3 options seemed to be: Light bulb. Ceramic heater that goes into a light bulb socket. Heat tape . There are two others I can think of 1. was another heat pad that I saw for keeping welding electodes…
  • shabaz
    shabaz over 9 years ago +2
    It's a shame the Edison is power-efficient, otherwise you could have put a few of them inside, and designed it so they perform useful computation until the inside is at the right temperature, and then…
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago

    A tip would be to ensure the plastic of the fridge interior will take the heat from the tape

    If you are planning on using Mains powered heaters this become more critical as a failure could lead to injury or Fire. also in this case, you need to be sure to follow code hen it comes to wiring etc (You may not be the only one sticking your hands in there.

     

    what happens if the controller locks up in the on mode,?... so think safety cutout features etc.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jkutzsch
    jkutzsch over 9 years ago in reply to Robert Peter Oakes

    Robert Peter Oakes Good point, I have seen projects where all they did was place a light bulb in the small enclosed space and then toggle it on and off as the temp sensor was toggled.  I was thinking heat tape similar to what Reptile cages sometimes use would be safer and keep a more steady heat.  I might need to look into a smoke sensor in there as well!  :-)

     

    The 3 options seemed to be:

    Light bulb.

    Ceramic heater that goes into a light bulb socket.

    Heat tape.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to jkutzsch

    The 3 options seemed to be:

    Light bulb.

    Ceramic heater that goes into a light bulb socket.

    Heat tape

    .

    There are two others I can think of

    1. was another heat pad that I saw for keeping welding electodes dry. Not sure how hot it got.

    2. Cat/Dog bed warmer, which tends to be a fully enclosed or maybe ceramic plate arrangement.

     

    I think you'd be surprised how hot a 100w light bulb in a small place gets.

    Maybe Blog 2 could be a trial ??

     

     

    what happens if the controller locks up in the on mode,?... so think safety cutout features etc.

    I think Robert Peter Oakes may be referring to an overtemperature cutout/thermal breaker.

    These are commonly applied as a fail safe.

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 9 years ago in reply to jkutzsch

    The 3 options seemed to be:

    Light bulb.

    Ceramic heater that goes into a light bulb socket.

    Heat tape

    .

    There are two others I can think of

    1. was another heat pad that I saw for keeping welding electodes dry. Not sure how hot it got.

    2. Cat/Dog bed warmer, which tends to be a fully enclosed or maybe ceramic plate arrangement.

     

    I think you'd be surprised how hot a 100w light bulb in a small place gets.

    Maybe Blog 2 could be a trial ??

     

     

    what happens if the controller locks up in the on mode,?... so think safety cutout features etc.

    I think Robert Peter Oakes may be referring to an overtemperature cutout/thermal breaker.

    These are commonly applied as a fail safe.

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jkutzsch
    jkutzsch over 9 years ago in reply to mcb1

    One of the concerns for the light bulb is the fact that by the time the temperature sensor would trigger to shut off the light bulb that it would still be holding a lot of heat and the temp would continue to rise giving a larger fluctuation in heat then I want.  I have read that the ceramic and heat tape are better for keeping heat at a more constant temperature.  But this is all reading.  :-)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to jkutzsch

    by the time the temperature sensor would trigger to shut off the light bulb that it would still be holding a lot of heat

    I think any heat source is likey to have some latent heat.

     

    Depending on your sensor, it may also have latency, so you may be needing to trip it a little earlier than the actual tempaerature.

     

     

    In theory you could map the rise and apply some intelligence, or just err on the lower side. image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jkutzsch
    jkutzsch over 9 years ago in reply to mcb1

    Spoke to my wife about that a little (she is the head supervisor for this since they are her hens), and she said that the fact that hens will get up off the eggs occasionally allows for rise and fall of some temp. 

     

    If I had the kit handy I would test out the temp via light bulb first to get some data...  Might do that first just to do see how it all works anyway.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to jkutzsch

    If I had the kit handy I would test out the temp via light bulb first to get some data

    You can still do it without the kit.

     

    Light bulb on a cord, thermometer.

    Eyeballs, clock/timer and notebook.

     

    It will give you a basic starting point and some data that will get you on the way.

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jkutzsch
    jkutzsch over 9 years ago in reply to mcb1

    I still have more work to do on the physical container as well since I want to add a double pane viewing window.  Tried to find an old wine cooler since those are already glassed but no luck.   I don't have anything currently that would automatically shut off the light as a temperature was reached but eyeballing it would be interesting.  That would still give me a range of time for the heat to dissipate down to where I would want heat turned back on.