Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog UpCycle IT - R2I - Research
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
  • Author Author: jkutzsch
  • Date Created: 23 Apr 2017 5:33 AM Date Created
  • Views 1631 views
  • Likes 4 likes
  • Comments 7 comments
  • farm
  • upcycle it
Related
Recommended

UpCycle IT - R2I - Research

jkutzsch
jkutzsch
23 Apr 2017

UpCycle IT – R2I INDEX:

 

Blog #1_”Introduction”

Blog #2_”Designing”

Blog #3 "The Kit"

Blog #4_"Mother Natures Version"
Blog #5_"Research"
Blog #6_"Competition01"

Blog #7_"Edison Setup"

Blog #8_"Edison 2 Ardunio"
Blog #9_"Grove-ON"
Blog #10_"Hot2Not"

 

Blog #5 - Research

 

image

 

So under Hobbies, I believe Researcher is a very appropriate label for me.  :-)  Especially as I delve in the varied aspects of melding technology and farming.

 

Here is some of the interesting information I came across while researching incubation for chickens.  The distinction of chickens is important since various fowl incubation differ quite a bit from temperature and humidity to time of incubation.

 

Basic Information:

 

Generally there is some basic information shared for incubation of chickens manually:

 

1.  Obtaining fertile eggs.  It is important to obtain fresh fertile eggs.  No you can not use eggs purchased at the local grocery store and found in their refrigerators.  I will obtain mine from our own hens.  I will not know if they are all fertilized though so there is a chance of mixed results.  We believe a hawk recently took out one of our Roosters and this of course is a required item for fertilized eggs!

 

2.  Temperature varies if you are doing a "Still-Air" or "Forced-Air" implementation.  If you not implementing a fan, then you want the temperature to be at 101.5, measured at the top of the egg.  If you are using a fan then a temperature of 99.5 is a good setting.

 

3.  Minimum number.  As I mentioned above I will not know if all of my eggs have been fertilized as such setting at least 6 eggs improves the chances of having some successful chicks hatch and reach maturity.  Another factor is size of incubator, if you get a massive incubator that can hold 250 eggs then they will probably have a minimum number required to meet the temperature and humidity needed/expected.

 

4.  Approximately 21 days for Chicken eggs to hatch.

 

5.  Humidity should be between 40-50% for the first 18 days of incubation.  After you should raise it to 70%.

 

6.  Unlike our Easter Egg pictures, the egg should not be placed with the pointy tip up.  The wide tip (or bottom for most) should be elevated if possible or at the least the small tip should be as low as it can be placed.  image

 

7.  Egg turning, at least 3 times a day.

 

 

Now this is just some basic information that seemingly can be found everywhere from 4H groups to survivalists to hobby farm user groups.  Many of them may make their own incubator from a Styrofoam box and manually roll their eggs themselves 3 times a day with a handy dandy calendar beside the incubator to appropriately mark each turn and milestone.

 

They may even have invested in an incubator that has a rolling mechanism to gently roll them on their sides automatically.

 

What was a little more interesting to me was reading on how commercial incubators operate and the level of studies and experiments that have went on to verify amount of times the egg should be turned and the minimal angles needed.

 

Commercial level Information:

 

There are a lot of educational links (as in College/University) showing that at one time the chicken egg was quite an interesting academic study.  Surprisingly most seem to be non-functioning now. 

 

One of the best solid sources I have found is

Pas Reform Hatchery Technologies

They provide some pretty interesting reasons why things are done a certain way commercially.  Such as why they place the eggs with the point down an why this can be a serious problem when human error mistakenly places them with the point up. 

 

There is a 12-30 percent reduction in the potential hatching of your eggs when the egg is placed point up.  "A hatchery loses 0.2 per cent of sellable chicks for each 1 per cent of fertile eggs placed with the small end up in a setter tray (Bauer et al, 1990)."  

 

 

FlockLarge end upSmall end up
AHatchability (%)97.679.5
Cull (%)0.03.6
Grade-A chicks (%)97.675.9
BHatchability (%)96.971.8
Cull (%)3.04.3
Grade-A chicks (%)93.967.5
CHatchability (%)100.084.0
Cull (%)2.04.0
Grade-A chicks (%)98.080.0

Reference: Bauer F., Tullet SG and Wilson HR (1990). Effects of setting eggs small end up on hatchability and posthatching performance of broilers.

What does this mean?  Approximately 280,800 chicks will be lost per year from a commercial hatchery that does 1 million chicks a week.

 

Commercial hatcheries have large shelves (setting trays) that rotate their eggs the proper 45 degrees while keeping their eggs in a vertical position with the tip down.  After the 18th day the eggs are transferred to a hatcher tray where they will remain on their sides for the last 3 days and humidity is increased.

 

Taking this information into account has heavily influenced my design for my Refrigerator 2 Incubator project.  Please keep following along to see it as it develops!

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 9 years ago +1
    Research is good. Knowing what your objective is and the unexplained rates of failure before you starts is also good. Have you worked out how they rioll their eggs yet.?
  • DAB
    DAB over 9 years ago +1
    I remember my aunt checking the eggs daily, using a light bulb to check for embryo development. She would move the eggs a couple of times everyday. She only raised a new brood about one a year to change…
  • jkutzsch
    jkutzsch over 9 years ago in reply to mcb1 +1
    Originally I had planned for something like the above where I would have 2 geared rotating shafts across the top with 3 additional free sliding shafts to balance the eggs. But as I read more on the emphasis…
Parents
  • DAB
    DAB over 9 years ago

    I remember my aunt checking the eggs daily, using a light bulb to check for embryo development.

     

    She would move the eggs a couple of times everyday.

     

    She only raised a new brood about one a year to change out the hens over time.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jkutzsch
    jkutzsch over 9 years ago in reply to DAB

    Yes depending on your use for chickens, just doing a small brood is a good way to stay in eggs.  :-)  Now if you want meat and eggs, then I think they start doing multiple hatchings since they cycle through birds quicker.  We have been focused on eggs so a small brood is fine for us.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jkutzsch
    jkutzsch over 9 years ago in reply to DAB

    Yes depending on your use for chickens, just doing a small brood is a good way to stay in eggs.  :-)  Now if you want meat and eggs, then I think they start doing multiple hatchings since they cycle through birds quicker.  We have been focused on eggs so a small brood is fine for us.