WorkBench Wednesdays
  • Challenges & Projects
  • element14 presents
  • WorkBench Wednesdays
  • More
  • Cancel
WorkBench Wednesdays
Forum Microcontroller Dev Boards: What features do you like to have (or to add?)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join WorkBench Wednesdays to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 114 subscribers
  • Views 8119 views
  • Users 0 members are here
  • pcb
  • microcontroller
  • arduino
  • pi pico
Related

Microcontroller Dev Boards: What features do you like to have (or to add?)

baldengineer
baldengineer over 3 years ago

image

A couple of weeks ago, I bribed shabaz (with coffee) to send me one of his Pi PIco Eurocards. As the name implies, these are a development board for the Pi Pico / RP2040. In the past, another friend sent me one of his all-in-one microcontroller development boards (pictured above). And I have designed a few boards that had development features on them. Besides those, boards like Adafruit's Feathers or even the iconic Arduino Uno could be considered dev boards. Last, historically, microcontroller manufacturers had elaborate evaluation platforms for their chips.

All of these points made me wonder: what are the features YOU want to see in a microcontroller development board?

image

If we use shabaz's Eurocard, some notable features are:

  • Headers for changing power source (external / Pi Pico / Programmer)
  • Integrated programmer/debugger (RP2040-based Xiao, in this case)
  • Prototype areas for through-hole and surface mount parts
  • SD Card
  • Button
  • LED
  • (and many more)

In addition to features, what tricks or tips have people learned when making a board like this one?

  • Sign in to reply
  • Cancel

Top Replies

  • wolfgangfriedrich
    wolfgangfriedrich over 3 years ago +8
    I just want to point out one feature, which is really nicely done on both of those boards. The markings of connectors and everything else in silkscreen. Pin numbers or signal labels in readable size, also…
  • michaelkellett
    michaelkellett over 3 years ago +7
    Keep it simple. Power supply input, on board regulator and clock. Break out every pin. Serial port, debug programming port. 0.1" headers are good and cheap but sometimesd take up too much room…
  • mayermakes
    mayermakes over 3 years ago +6
    i don't really have requests in stuff that should be on the board, I prefer to have zero clutter or parts that I don't really use in the project present to avoid conflicts and confusion on my part. also…
Parents
  • misaz
    misaz over 3 years ago

    I disntiguish three types of board usualy refered as:

    • Breakout/prototyping boards. Examples: Raspberry Pi Pico, STM32 Blue Pill
    • Development Kit. Examples: STM32 Nucleo, STM32 Discovery, Renesas EK-RA, Cypress PSoC Pioneer boards, SIlicon Labs Explorer Kits, Microchip Curiosity Nano, Maxim FTHR boards, Nordic nRF52, nRF53 and nRF91 devkits
    • Evaluation Kit: STM32 Evaluation Kits

    The first is simple. No necessary connectors, components and so on. Usualy they have exposed all or almost all pins. They are good for low-power applications because except MCU there is nothing else consuming energy.

    Difference between second and thinrd is in the scope of offered feature. The last should allow user to evaluate ALL features of the MCU while the middle option allows using (smartly selected) subset of the feature. Most devkits are in second group. I guess it is because second group offer best price/performance ratio. First category is good for low-pin MCUs but for higher count MCU it became annoying. Second category offsers good onboard peripherals and allows use most of features without heavy external circuits. Third option is used for users who have needs for heavily using the MCU and need to develop firmware before make prototypes of their own huge boards. Third category is the most expensive, but this boards often contains tons of connectors, sensors, large displays, several connectivity options,... In other words evaluation board (like this one) contains everything but are expensive.

    Nowadays almost every board (currently also including many board classified to first category) has onboard JTAG/SWD debugger and we do not need buying expensive external debugger anymore. It is extremely usefull benefit in comparison with boards avalaible 15 years ago.

    My most favourite development kit design is Renesas EK-RA like EK-RA2L1 which I reviewed as part of roadtest: Review of Renesas EK-RA2L1 Development Board

    image

    It has very few onboard peripherals, but has lot of connectors for most commonly used interfaces: Arduino Uno compatible connector, MIkroE socket, Qwiic, Grove, PMOD. Except these connectors all pins are accessible on dedicated connectors. It is very usefull for connecting logic analyzer. I like this design very much. Other very good options is that all devekits in this serie share the same design, so if you ware familiar wiht one kit, you can freelky move to the other one. They are expensive, but Renesas offers free samples Slight smile

    Second boards which I frequently use are STM Discovery and Nucleo boards. Nucleo shares the samilar design pattern as Renesas EK-RA. In case of STM I like discovery boards over Nucleos because disco boards add some interesting peripherals.

    Nowadays many vendors try to standardize even their breakoutable/prototyping boards. For example recently I played with Silicon Labs EFR32BG22. Silicon labs makes their explorer kits which all have the same (small) form factor, onboard debugger, MikroE socket and exposes all other pins. They use this form factor for all their MCUs no matter if they support BLE or not, are 8-bit or 32-bit and so on.

    image

    At last I like boards which has something very unique and advanced but vendor designed to offer them at very competitive price for promoting their products. For example MAX78000FTHR. I basicaly described it in my blog  Received Project14 7-segment Display Competition Reward . It is 30 USD board with advanced dual core MCU with AI accelerator, on-board debugger, camera, audio codec (+ jacks), other MEMS microphone and allows running from battery (has on-board li-pol/li-ion charger). Very few boards are so tiny, so performant, so cheap and allows so much interesting use cases. But it has other disadvantage like hard firmware development.

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • misaz
    misaz over 3 years ago

    I disntiguish three types of board usualy refered as:

    • Breakout/prototyping boards. Examples: Raspberry Pi Pico, STM32 Blue Pill
    • Development Kit. Examples: STM32 Nucleo, STM32 Discovery, Renesas EK-RA, Cypress PSoC Pioneer boards, SIlicon Labs Explorer Kits, Microchip Curiosity Nano, Maxim FTHR boards, Nordic nRF52, nRF53 and nRF91 devkits
    • Evaluation Kit: STM32 Evaluation Kits

    The first is simple. No necessary connectors, components and so on. Usualy they have exposed all or almost all pins. They are good for low-power applications because except MCU there is nothing else consuming energy.

    Difference between second and thinrd is in the scope of offered feature. The last should allow user to evaluate ALL features of the MCU while the middle option allows using (smartly selected) subset of the feature. Most devkits are in second group. I guess it is because second group offer best price/performance ratio. First category is good for low-pin MCUs but for higher count MCU it became annoying. Second category offsers good onboard peripherals and allows use most of features without heavy external circuits. Third option is used for users who have needs for heavily using the MCU and need to develop firmware before make prototypes of their own huge boards. Third category is the most expensive, but this boards often contains tons of connectors, sensors, large displays, several connectivity options,... In other words evaluation board (like this one) contains everything but are expensive.

    Nowadays almost every board (currently also including many board classified to first category) has onboard JTAG/SWD debugger and we do not need buying expensive external debugger anymore. It is extremely usefull benefit in comparison with boards avalaible 15 years ago.

    My most favourite development kit design is Renesas EK-RA like EK-RA2L1 which I reviewed as part of roadtest: Review of Renesas EK-RA2L1 Development Board

    image

    It has very few onboard peripherals, but has lot of connectors for most commonly used interfaces: Arduino Uno compatible connector, MIkroE socket, Qwiic, Grove, PMOD. Except these connectors all pins are accessible on dedicated connectors. It is very usefull for connecting logic analyzer. I like this design very much. Other very good options is that all devekits in this serie share the same design, so if you ware familiar wiht one kit, you can freelky move to the other one. They are expensive, but Renesas offers free samples Slight smile

    Second boards which I frequently use are STM Discovery and Nucleo boards. Nucleo shares the samilar design pattern as Renesas EK-RA. In case of STM I like discovery boards over Nucleos because disco boards add some interesting peripherals.

    Nowadays many vendors try to standardize even their breakoutable/prototyping boards. For example recently I played with Silicon Labs EFR32BG22. Silicon labs makes their explorer kits which all have the same (small) form factor, onboard debugger, MikroE socket and exposes all other pins. They use this form factor for all their MCUs no matter if they support BLE or not, are 8-bit or 32-bit and so on.

    image

    At last I like boards which has something very unique and advanced but vendor designed to offer them at very competitive price for promoting their products. For example MAX78000FTHR. I basicaly described it in my blog  Received Project14 7-segment Display Competition Reward . It is 30 USD board with advanced dual core MCU with AI accelerator, on-board debugger, camera, audio codec (+ jacks), other MEMS microphone and allows running from battery (has on-board li-pol/li-ion charger). Very few boards are so tiny, so performant, so cheap and allows so much interesting use cases. But it has other disadvantage like hard firmware development.

    image

    • Cancel
    • Vote Up +3 Vote Down