Merry Boxes & LEDs
  • Challenges & Projects
  • Project14
  • Merry Boxes & LEDs
  • More
  • Cancel
Merry Boxes & LEDs
Blog Finally! Two Trees Assembled
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Merry Boxes & LEDs to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ntewinkel
  • Date Created: 30 Dec 2018 7:21 AM Date Created
  • Views 4240 views
  • Likes 13 likes
  • Comments 18 comments
  • wifi
  • mqtt
  • merryboxesledsch
  • holidayspecial19ch
  • xmas
  • esp8266
  • arduino
Related
Recommended

Finally! Two Trees Assembled

ntewinkel
ntewinkel
30 Dec 2018
image

Merry Boxes & LEDs

Enter Your Project for a chance to win a Maker Tool Kit, an Oscilloscope Grand Prize for the project that brings the Most Joy to the Heart, and Gift to Gives!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

It seems like there's always another something-or-other that takes precedence over my fun projects; however, this evening I did finally find some time to finish soldering the second xmas tree.

 

For future reference, I ended up trying the green LEDs with a 10k resistor, but then it barely flashed. So I used the supplied 2k resistor for green, 1k for yellow, and 330 for red.

For the very top I used a 680 ohm resistor (instead of the supplied 10k) and put a flashing LED on the peak instead of the supplied red one. I like how it gives the peak a more festive effect image

image

 

The first tree has been on the mantle downstairs looking pretty for the last few days already, powered by one of those little rechargeable battery boxes often used to refill a cell phone on the go. It looks and acts identical to the tree in the gif (which is showing the one I just finished tonight).

 

The soldering marathon tonight had solder fumes causing my eyes to tear up a little, and I poked myself with a sharp resistor end making me bleed a bit. I also worked up a little bit of a sweat while concentrating. Nothing gross of course, just one of those sexly manly kinds of sweat, honest image

My point is though, that I've put blood, sweat, and tears into this project! sorry, that was bad. but it had to be done image

 

So now that I finally have two trees to work with, the real part of the project can begin - where I connect two WeMos D1 Mini ESP-based boards to them and have them talk to each other!

 

I suppose I could have simply used a little string of battery-powered LEDs for this too, and saved me several nights of soldering up these trees image  But hey, this is much cooler.

 

Cheers,

-Nico

 

Previous posts:

Connected Christmas Trees

Assembling the Trees

 

Next Posts:

Two Trees by a Tree

Connecting the Tree to the Internet

Motion Sensor on Wemos

Trees! one with motion sickness...

Motion Sensor Issues, continued

The Connected Trees are Working!

Merry Boxes - A Project Within a Project

Connected Christmas Trees - Finished!

  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 7 years ago +6
    Nice Job! The cheap LEDs has already created Issues for me in past. Depending on the color a different resistor should be needed to get the same light intensity. When we see both the trees? Cheers Enr…
  • ntewinkel
    ntewinkel over 7 years ago in reply to balearicdynamics +4
    Hi Enrico! > The original critic was for the Chinese engineers. Oh yes, I understood it that way too. I only just bought the kits, I didn't design them It's mind boggling how they can do it though - I…
  • DAB
    DAB over 7 years ago +3
    Nice build Nico. How did the cats react to a blinking tree? DAB
  • neilk
    neilk over 7 years ago

    The tree looks fantastic - I'd say it was definitely worth the blood, sweat and tears!!

     

    Neil

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 7 years ago in reply to ntewinkel

    But now you do make me wonder about other ways of doing it

    I've been looking at splitting the LEDs into groups of two in series, and it's possible ...

    My thought was to drive the six 'groups' from a micro.

     

    Both of your ESP devices have enough pins and the new MKR Zero even has a micro SD card for various sounds ...

     

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to ntewinkel

    I

    I can't imagine how nothing this stuff can cost at the source image

     

    In past, I had the possibility to buy a bunch of components from a Chinese customer (resistors, capacitors, LEDs). I ordered for few dollars (in invoice exchange) a couple of hundreds from him with a list. He shipped me 1.000 per piece as it was the minimum quantity that it was the worth for him to count in a package. I am already using these components after years.

     

    Enrico

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 7 years ago in reply to balearicdynamics

    Hi Enrico!

     

    >The original critic was for the Chinese engineers.

    Oh yes, I understood it that way too. I only just bought the kits, I didn't design them image

     

    It's mind boggling how they can do it though - I only spent $3.62 (Canadian) on one of the kits, and that included free shipping!

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to ntewinkel

    Hello Nico!

     

    The point is - IMHO - that if we make a serious price comparison, we will refer to a serious commercial site. I have searched both components on the Farnell site, in Europe. Then it's true that you find the same somewhere in China for less than less, but - always IMHO - this is not a reference. Then my critic was not about you, as you already know by my previous comments, I loved this idea. What I say is that the guys from China, those who made the original design of the chips, at least some more elegant circuit it was possible to do, This is what I see. Then probably using NE555 SMD bought from China, I don't know the price but sure everything was possible to fit on the same tree base. So, add the tree base, no extra PCB, fewer components etc. and it is possible that also for Chinese guys this was cheaper.

     

    And with some astable configuration of the 555, it is possible to do something better. In you case where you have added a considerable value with the extra board, not bat to "program" the 555 just changing some parameters, for example, with a digital potentiometer connected to the IC. But this is just a fly through. The original critic was for the Chinese engineers.

     

    Enrico

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
>