Open Arduino
  • Challenges & Projects
  • Project14
  • Open Arduino
  • More
  • Cancel
Open Arduino
Blog Arduino in Test Instrumentation - Part 3a: LabVIEW Driver Intitialisation Block
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 8 Apr 2018 6:31 PM Date Created
  • Views 3288 views
  • Likes 8 likes
  • Comments 4 comments
  • diytestequipch
  • ardexpert
  • openarduinoch
  • labview
  • project 14
  • scpi
  • arduino_test_instrumentation
Related
Recommended

Arduino in Test Instrumentation - Part 3a: LabVIEW Driver Intitialisation Block

Jan Cumps
Jan Cumps
8 Apr 2018
image

Open Arduino

Enter Your Project for a chance to win a grand prize for the most innovative use of Arduino or a $200 shopping cart! The Birthday Special: Arduino Projects for Arduino Day!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

Arduino in Test Instrumentation

 

To celebrate Project 14's birthday, I'm going to make a programmable switch with an Arduino UNO.

This post describes the first block for the LabVIEW driver: Initialisation

image

 

LabVIEW Driver

 

A LabVIEW driver is a library that allows you to program an instrument in a intuitive way. It's one layer above the instrument's SCPI interface.

There is a convention that's used by many manufactures: you should provide an init and close block, and blocks to allow to control and query your device.

 

I am following those conventions for the LabVIEW driver lib that I'm building for the Arduino SCPI switch.

In the next few posts I'll introduce all blocks and an example LabVIEW flow.

Let's start of with the Initialize module.

 

Initialize

 

image

This block sets up the communication with your Arduino UNO.

You'll see that there are a number of settings that define the behaviour of the data exchange, like serial communication settings, ports, timeouts.

There are also some behavioural settings. You can ask the device to reset at initialisation*, or if you want check the ID of the device you're talking to.

image

All the values that aren't dependent on the firmware are available as parameters.

The communication settings are internal. They have to match the settings that the Arduino sketch uses to initialise serial communications.

image

 

From left to right, the flow is opening the communication channel, then optionally verifying if we're talking to the right device, optionally resetting the device,

and if an error occurs, handling that.

 

The first block opens the communication.

image

The serial settings are predefined. They are firmware dependent and you don't have to edit them.

The "VISA resource name" is the communication port. This is a parameter that you set before invoking this block.

The "deal with Arduino Communication Reset" parameter is there to do what the label says image. An Arduino UNO resets when you initialise serial communication with it.

There are hardware ways to modify the board so that this reset doesn't happen (but that has impact on the functionality of the Arduino IDE Serial Monitor !).

I'm assuming that the code will run on a board that isn't modded. I've added a wait time just after communication starts,  that can be configured.

On my Arduino, 1500 ms isn't long enough. 2000 ms works every time.

I haven't bothered optimising this value, because it only happens once when the instrument is initialised.

Because in a normal flow you have to initialise a number of instruments in parallel at the start of the flow, the 2 seconds are OK, comparable with many other instrument's setup time.

If you know a way to optimise this, please comment on this blog post with your approach.

 

The next part is a case structure.

Depending of the value of ID Quey you pass, it will either ask the device to show its ID and validate that, or it will not perform that step:

This is the flow that's executed when you select to query the device ID:

 

 

image

You can see in this flow that the SCPI interface is used to retrieve the device ID. In the upper left corner we're sending the *IDN? command.

 

This much easier flow is run if you say that the flow doesn't have to validate the device:

image

 

The next block defines what happens after establishing contact. We'll eather reset or not reset the device.

You'll see that both of these options invoke another driver block for the device.

The Reset option will call our driver's "Reset" module. The other option will call the "Default Instrument Setup" block.

I don't know yet if I will blog about those blocks. That depends on the interest.

In any case, I'll provide the LabVIEW driver lib. That 'll allow you to investigate them yourself.

 

This is the flow when you ask for a reset. Hint: It 'll call the *RST SCPI command.

image

This flow is called if you prefer to not ask a reset.

image

Again, this discussion is moot because a standard Arduino UNO will reset anyways.

 

The last block deals with error handling. Once more, there are two paths, depending on success or error.

 

This flow is executed on success:

image

Indeed, it does nothing. A sucessful flow doesn't require error handling.

When an error occured in the block, this process is executed:

image

We're closing the device and sending a non-initialised VISA resource to the next block.

This will prevent that the next block sends commands to our device.

 

 

*big caviat: an Arduino UNO will always hardware reset the micro controller at start of serial communication, unless you modify the PCB.

 

Related Blog
Arduino in Test Instrumentation - Intro: SCPI Programmable Switch
Arduino in Test Instrumentation - Part 1: SCPI Lib
Arduino in Test Instrumentation - Part 2: Firmware
Arduino in Test Instrumentation - Part 3a: LabVIEW Driver Intitialisation Block
Arduino in Test Instrumentation - Part 3b: LabVIEW Driver Switch Control Block
Arduino in Test Instrumentation - Part 3c: LabVIEW Driver Read Status Block
Arduino in Test Instrumentation - Outro: LabVIEW Example
Attachments:
4370.project14.zip
  • Sign in to reply

Top Comments

  • genebren
    genebren over 8 years ago +1
    Very nice addition to your blog series. Very informative and makes me want to to rush off a learn something new (LabVIEW, at least new to me). Gene
  • michaeldchristopher
    michaeldchristopher over 7 years ago +1
    I very much appreciated your work on this. This is very useful to me. I control SCPI instruments all the time, in many ways (including C++, LabVIEW, and python) so this is awesome for me. I needed this…
Parents
  • michaeldchristopher
    michaeldchristopher over 7 years ago

    I very much appreciated your work on this. This is very useful to me.

     

    I control SCPI instruments all the time, in many ways (including C++, LabVIEW, and python) so this is awesome for me. I needed this to make some giveaway instruments for a class we are presenting about how to use our EMC testing software.

     

    We use those instruments to test things inside anechoic chambers.

     

    There are benefits to all languages for different situations of course, and your project is easy to adapt to whatever is best at that moment.

     

    Great project!

     

    Michael Christopher

    Austin Texas USA (home of NI LabVIEW image)

     

    PS. if you are ever in Austin, I will give you a tour or buy you a beer

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to michaeldchristopher

    Thank you Michael!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to michaeldchristopher

    Thank you Michael!