Recycle & Retrofit
  • Challenges & Projects
  • Project14
  • Recycle & Retrofit
  • More
  • Cancel
Recycle & Retrofit
Blog Mr. Machine gets an upgrade - New boards, but not enough time
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Recycle & Retrofit to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: genebren
  • Date Created: 15 Dec 2020 3:11 AM Date Created
  • Views 1877 views
  • Likes 9 likes
  • Comments 4 comments
  • recycleretrofitch
Related
Recommended

Mr. Machine gets an upgrade - New boards, but not enough time

genebren
genebren
15 Dec 2020

In my prior blogs (Mr. Machine gets an upgrade - working on the pieces. , Mr. Machine gets an upgrade - new internals, motors installed and new PCBs and Mr. Machine gets an upgrade - time is running down ) I walked through Mr. Machine's history and some of my updates.  This time I will wrap up what I can as the project14 deadline closes.

 

I was very concerned as time ran down and my boards had not yet arrived.  Late Saturday afternoon (12/12), the boards finally showed up.  I jumped right in, finishing a few design details (schematic and BOM) and moved on to assembly.  Here are some shots of the finished boards:

 

imageimageimage

 

Clockwise from the upper left hand corner, are the Power Pack, Motor Driver and Controller boards.   During the finalization of the schematics and BOM, I noticed a few errors on the controller board.  First, I noticed that I had mapped one of the pins incorrectly.  The Midi player function uses an timer compare output that is available on Pin3, but I somehow connected Pin2 to the low pass filter and on to the audio amplifier.  The other error was due to a bad assumption that I made concerning the hardware support of the I2C port on the ATTINY85.  Device is basically a simple serial port and requires a fair amount of bit banging to actual function as an I2C port.  With the high rate of sampling needed for the four-voice PWM tone generation of the Midi player, it would be very difficult to get any reliable/repeatable timing on the I2C bus.  I decided to isolate the ATTINY85 part from the I2C bus (mainly used to communicate between the three boards.  Instead, I routed the two signals from the ATTINY85 to two unused pins on the ATMEGA328PB (to be used as a start/stop control and a status line.

 

Here is the updated schematics and BOM for each of the boards:

 

First the Controller Board.

imageimage

 

Motor Driver Board.

imageimage

 

Power Pack Board.

 

imageimage

 

The overall connection diagram is as follows:

image

 

I have started writing/porting the firmware from the WalkyII project, but I have not gotten far enough through the process to document the firmware at this time.  I fully intend to complete this project and I will continue to blog on my progress/results.  All in all this was a fun project undertaking.  I learned a valuable lesson from my deadlines issues with the printed circuit board, which is, complete all of your long lead time orders earlier in the project time line.  I spent a huge amount of time designing and printing all of the plastic parts and I left the final electronic design details and ordering towards the end of the project.  This is a mistake I hope not to repeat in the future.

 

Thanks for following along on this journey with me.  I don't know about you, but for me, this has been a lot of fun!

  • Sign in to reply

Top Comments

  • genebren
    genebren over 5 years ago in reply to dubbie +2
    Thanks Dubbie. The PCB making process is really getting a lot easier with many free tool sets (Eagle has a free, limited version) and many online vendors. At the lowest levels it can be very 'lego like…
  • genebren
    genebren over 5 years ago in reply to ralphjy +2
    Thanks Ralph! A labor of love. I am digging in to the firmware now. I have the Midi played running on the new controller board and I am digging into the remaining controller functions. I hope to have this…
  • dubbie
    dubbie over 5 years ago +1
    Gene, The PCBs look really nice. One day I hope to be able to do the same. Maybe I will make it one of my jobs for New Year. I'm also looking forward to seeing the completed robot up and running (or probably…
Parents
  • ralphjy
    ralphjy over 5 years ago

    Gene,

     

    Great project!  Quite a lot of complexity for a Project14 build (or maybe that should be effort).  I think you did a lot in the short timeframe.  Glad that you're having fun with it image.   Can't wait to see it working.

     

    Ralph

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ralphjy
    ralphjy over 5 years ago

    Gene,

     

    Great project!  Quite a lot of complexity for a Project14 build (or maybe that should be effort).  I think you did a lot in the short timeframe.  Glad that you're having fun with it image.   Can't wait to see it working.

     

    Ralph

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • genebren
    genebren over 5 years ago in reply to ralphjy

    Thanks Ralph!  A labor of love.  I am digging in to the firmware now.  I have the Midi played running on the new controller board and I am digging into the remaining controller functions.  I hope to have this all running before my grandchildren visit again.  I will continue to post as I make progress.

     

    Thanks again.