Congratulations to our winners! They used the ON Semiconductor RSL10-SENSE-GEVK with Bluetooth connectivity to monitor their world and design solutions for everyday problems.
This is my final project submission for the Think ON Design Challenge. The name of the project is Smart N' Safe and it is a Smart Home Device
Quick Jump Links
Aim
Methodology
Components Required
Procedure
Atmosphere IoT Platform…
Regularly, most of the electricity at home is consumed by heating and cooling with the caveat that not all the rooms have the same temperature. There are some key factors that may contribute to these temperature differences like how many sources of heat…
Neonatal Mortality Rate (NMR) quantifies the number of new-born deaths (i.e in the first month of life) per thousand live births and is responsible for more than 46% of all child deaths before the age of five (2.5 Million in 2018). Which means 7000 deaths…
Introduction:
Now a day mostly mass produced vegetables and fruits are GMOs, contaminated with dangerous chemical pesticides and traces of chemical fertilizers. And mostly products labeled as organic, are not 100% organic. So the best and most cost…