Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Arduino and Transistors Question - RE: School Musical Production
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 126 replies
  • Answers 2 answers
  • Subscribers 421 subscribers
  • Views 11220 views
  • Users 0 members are here
  • raspberry
  • transistor
  • pi
  • arduino
Related

Arduino and Transistors Question - RE: School Musical Production

wallarug
wallarug over 12 years ago

One of the directors has asked me to create a special backdrop for our college musical. This particular backdrop has a particular design (see below) that includes LED strip lighting to give the feel of a 1920s casino sign – similar to what is seen today in Las Vegas.

I  have done up a detailed design for this sign, based off the rough sketch given to me by the director and the dimensions of the backdrop.  On this diagram, the arrangement of the LED strip lighting can be seen.

image

          

The LED Strip lighting that will be bought for this project will be sourced from Jaycar – “Low Cost 5m Flexible Adhesive LED Strip Light – Warm White” (ZD0577).  According to the specifications off Jaycar’s website, these LED lights need 1.1 Amps per metre @ 12 volts.  This means that the longest segments of lights need 1.1 * 1.5 = 1.65 Amps of power (rounded up by 20% for safety: 2.0 Amps @ 12 volts).

 

This would not be an issue if I was just turning these LED Strips on and off with mains power BUT I want to control these LEDs via an Arduino, so that they can do fancy things like flash and chase.  That means that I would need a circuit to control these lights with an Arduino so that everything remains safe and does not blow up.

I have come up with this circuit (below) using a couple of NPN transistors and two power supplies.  In the diagram below, I am aware that the transistor pinouts are EBC.  The ones I am going to buy have a pinout of BCE.

 

image

 

The only problem with this is that I have very little understanding of transistor circuits.  What this circuit has to be able to do is:

  • Using the smallest amount of current from the Arduino (at 5 volts) or a Raspberry Pi (3v3 volts), turn on the circuit to allow the 12 volts that powers the LED strip lighting to flow.

 

I was thinking of using either TIP41C NPN Transistors (in a darlington Array) or TIP122 NPN transistors.

 

This circuit will be replicated 8 times over to accommodate for the number of LEDs I am controlling.

 

 

Can anyone help me:

  1. Design a circuit that will work 100% and will be safe (ie: low heat)
    1. This includes base resistance
  1. Confirm which transistors I should be using for this project.

 

Any help will be much appreciated.

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago +1
    Sorry the one I suggested wont work, but this one should http://www.jaycar.com.au/productView.asp?ID=ZK8821 10+ current rating and at 0.016ohms it should be good for your needs pdf here http://www.vishay…
  • mcb1
    mcb1 over 12 years ago in reply to jw0752 +1
    John If you are referring to this It means that at a gate voltage of 1.6 typ, a current of 250uA will be flowing in the Drain. If you look here, you can see that from 3 to 3.3v will give you enough to…
  • D_Hersey
    D_Hersey over 12 years ago +1
    Solenoid Whapper:
Parents
  • wallarug
    0 wallarug over 12 years ago

    Hey guys!

     

    I have built one sample circuit on the PCB but I have an issue.


    When the wire coming from the Arduino (pin 9) registers 4.95v when it is NOT connected to the board.  When that same wire is connected to my circuit board, it registers 0.9v (from pin 9).


    Any ideas what is causing this?  When I built the exact (when I say exact I mean EXACTLY THE SAME) same circuit on the breadboard it works perfectly.


    I am missing something?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gihu
    0 gihu over 12 years ago in reply to wallarug

    If you are using the transistor... Maybe you missed the resistor between the arduino output the base of the transistor?

     

    Hope that helps,

    Miguel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 12 years ago in reply to mcb1

    Nice to see your video, the resistor that Mark suggests is a good idea and will protect that transistor's base.

    Once you have done that then you will need to again check for mistakes /soldering or layout. Note that when you turn over the board you have left the legs on the transistors these will bend and may well be shorting out, they should be cut flush so this does not happen.

     

    If this does not cure it then you need to see which transistor is failing ... take the Arduino out of the game  connect the input to ground then 5V does it work . If so check the Arduino!

    If not  disconnect the NPN from the FET then check the circuit again taking the gate to ground, R2 should pull it up automatically so the LED should light at this  point.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 12 years ago in reply to Problemchild

    I'm off to bed but before I do.....

     

    Have you added the 2k2 resistor in series with the Arduino pin to the base of the PN100.?

    The resistor is also there to ensure that any stray current from the Arduino will NOT cause the PN100 to conduct.!

     

    As much as your pictures/videos are great, without an idea of which connector does what we are guessing.

    It appears that the arduino is connected to the blue? lead standing up between the two blue connectors....however that's an educated guess.

     

    Perhaps you could annotate the drawing with which column/row each connection is ...which would help us to help you.

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 12 years ago in reply to wallarug

    It looks like the PN100 emitter on the breadboard is not connected to anything. It looks like the green wire is connected to the base. Is this correct? (if the emitter is not grounded the base could be driven high)

    As MCB points out, the NPN PN100 really should have a resistor connected between the base and the arduino because the voltage between base and emitter can not exceed 1  forward diode drop (1 volt according to the datasheet).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • wallarug
    0 wallarug over 12 years ago in reply to dougw

    just to clarify: the base is NOT connected to anything and the emitter is grounded (as per the schematic posted with the pn100.
    The collector is connect to the resistor (r2 - goes to 5v/12v). On the same line is the gate of the mosfet.

    the two blue screw terminals are the led breaks that can be seen in the schematic. The one furthest from the mosfet is connect straight to the 5v/12v rail. The other half of the blue connector goes into the mosfet drain. The mosfet source goes to ground.

     

    That should be the same in both circuits.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to wallarug

    in the diagram above the base of the transistor is clearly connected to R1 and then the other side of R1 is connected to the Arduino output pin

     

    You need to connect this up for you circuit to work

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 12 years ago in reply to Robert Peter Oakes

    Wallrug

     

    You may also need to pay attention for dry joints in the final part of this (after you add the base resistor)

    These suggest poor contact with the connector.

     

    image

     

     

    Your post is very interesting, as I wasn't aware those types of prototype board exist.

     

    For future reference, if you swap the PN100 down to the 'c' row, and place the FET at 'e' row, you could have room for a heatsink.

    I always prefer to have them with the metal bit away from the electronics (ie rotated 180 deg), because one day you'll be measuring/adding a wire to the connector when the power is on.....

    Then that No5 answer appears   As long as nothing is damaged/destroyed or otherwise had the magic smoke let out.

     

     

    Mark

    edit fixed spelling mistake

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 12 years ago in reply to mcb1

    Yes Mark those PCBs are quite common I even found some in the Farnell catalogue (did come from Adafruit though!!)

     

    http://uk.farnell.com/mcu-mpu-dsc-dsp-fpga-development-kits_accessories/accessory-type/breadboard-pcb-kit/pg/110514094

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 12 years ago in reply to wallarug

    Sorry there I don't to Labour it but really  you need to check over that soldering and clean up all those joins  several have far too much solder and several barely any at all and this may just be the problem any number of bad joints would cause your problem

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 12 years ago in reply to Problemchild

    John

    Thanks for the link .. the small one is for the RPi 'extender' although I used a different type.

     

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • wallarug
    0 wallarug over 12 years ago in reply to Problemchild

    I will let the builder know that his work is not up to standard.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • wallarug
    0 wallarug over 12 years ago in reply to Problemchild

    I will let the builder know that his work is not up to standard.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Problemchild
    0 Problemchild over 12 years ago in reply to wallarug

    Sorry Wallarug wasn't trying to be awful but  bad construction techniques will simply drive you round the twist and if you've copied the breadboard exactly you will be chasing your self until you get past these bits .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 12 years ago in reply to Problemchild

    I assist with helping students put together an electronic Xmas Tree.

    It involves component insertion and soldering some of whom have had some experience, and some none at all.

     

    In each case we try to show them why their solder joint needs rectification, and how to spot a poor joint before firing it up.

    The end result of all this (and yours) is a reliable, working well and useful piece of electronics.

    In many cases it might work until it is heated and cooled a couple of times, then it only works sometimes.

     

    Hence the reason we are pointing out these problematic areas so that you don't have half a display on opening night.image

     

     

    I'm sure you have learnt a lot from this whole discussion, and this is no more than that ... more learning.

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 12 years ago in reply to mcb1

    Good point Mark I was avoiding mentioning the inevitable Christmas tree kit trying not to confuse the matter,  but to be fair it's a great excuse to practice basic soldering skills with out the pressure of designing something as well. I have used these with young Nephews and they do indeed like them and get to correct their work as you said...This is the most important thing.. After all those who make no mistakes haven't made anything !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 12 years ago in reply to Problemchild

    After all those who make no mistakes haven't made anything !

     

    Yep.

    The key is trying to spot your mistakes before others...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 12 years ago in reply to mcb1

    I'll admit a field of stupid mistakes before now but I keep the photos of them down to a minimum image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • wallarug
    0 wallarug over 12 years ago in reply to Problemchild

    Ok guys,

     

    All is working.  I had the multimeter in the wrong position of the circuit.

     

    The work on the PCB is of high quality (according to the individual who built it) and I really any help on this project.

     

    I will get back to you when the board is fully built and tested (correctly image)

     

    Thank you again.  I'll keep you posted.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 12 years ago in reply to wallarug

    wallrug.

     

    Please tell us you now have a resistor in series with the Arduino pin and the base of the PN100.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • wallarug
    0 wallarug over 12 years ago in reply to mcb1

    nope. image

     

    I might investigate how to do this by modifying a few cables with a resistor in them.

     

    I ran out of space on PCB for base resistor.  (30 / 6 = 5 outputs) - an extra resistor would mean an extra hole used.

     

    What did seem like a good idea, suggested by one of you, is that you break the connection on the PCB to allow the resistor to be in the circuit (a bit confusing I know).  The only issue with that is it may crack the whole board. 

     

    Any other ideas to get base transistor on PCB without occupying more space and without damaging PCB too much?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 12 years ago in reply to wallarug

    Here are a couple of suggestions:

    1) Replace the PN100 with an N channel FET - preferably with a logic level threshold...

    2) Program the 2 states of the CPU "output" pin as follows:

    1. Output ON (LED Off) - configure the pin as an input with internal pull-up resistor - this will turn the NPN transistor on without stressing the CPU pin
    2. Output OFF (LED On) - configure the pin as an output that is always set low (a riskier solution is to leave the pin as an input but with no internal pull-up)
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 12 years ago in reply to dougw

    wallrug

    I cannot support the suggestion of making it an input, because you can't drive it.

     

    I would remove the two pin jumper you have and insert one end of the resistor in its place. Cut the wire and attach the cut end to the other end of the resistor.

    The second option is add it underneath and use the unused side of the board ie row f - j.

     

    mark