Welcome to
image
MiniZedTm is a single-core Zynq 7Z007S development board. This board targets entry-level Zynq developers with a low-cost prototyping platform.
image

Technical Specification

The MiniZed provides for an efficient hardware reference design with a Cortex A9 processor core.  It is an inexpensive board that can be used to run workshops and tutorials. Product Brief (Datasheet)

Click on the images to enlarge

Top View
MiniZed Top View
Kit
Kit
Antenna View
Antenna View
USB & Cable
USB & Cable
Block Diagram
Block Diagram

Hardware Specification

Specification Description
On-board connectivity through the Murata "Type 1DX" wireless module provides:
  • Wi-Fi 802.11b/g/n
  • Bluetooth 4.1 plus EDR and BLE (Bluetooth Low Energy)
On-board memory from Micron
  • 512 MB DDR3L
  • 128 Mb QSPI flash
  • 8 GB eMMC
Peripherals can be plugged into
  • Dual Pmod-compatible connectors (16 GPIO)
  • Arduino-compatible shield interface (22 GPIO)
  • USB 2.0 host interface
Physical interface
  • Two bi-element user LED’s
  • User pushbutton
  • Reset pushbutton
  • User switch
The integrated power supply from Dialog generates all on-board voltages.  An auxiliary microUSB supply input can be used to power designs that require additional current.
On-board MEMS sensors from ST Micro
  • LIS2DS12 Motion and temperature sensor
  • MP34DT05 Digital Microphone

Reference Designs

H264 Video Streaming on Avnet MiniZed

SDSoC Baremetal Platform - Xilinx Matrix Multiply Example

Tutorial 01 Build a Zynq Hardware Platform

Tutorial 02 First Application - Hello World

Tutorial 03 Generate and Run Test Applications

Tutorial 04 FSBL and Boot from QSPI

Tutorial 06 PL SPI Controller

Tutorial 01-08 Solutions

MJPEG Video Streaming over Wi-Fi on MiniZed using the TDNext Pmod

Prebuilt Platforms Using Hardware Definition Files (HDFs)

Technical Documents

Getting Started Guide

Restore QSPI and eMMC Factory Images

Errata and Product Change Notices

Board Definition Files

Related Blog Posts
  • [PP-12] Lab 9 - the power of scripting

    In this lab we are use a TCL scripts to prepare and finalize our hardware project. We will use here a lab9.tcl script delivered in Speedway support documents.Please go to the following directory: ZynqHW/2017_4/Support_documents/Lab9/ and type so...
  • [PP-11] Lab 8 - hardware debugging of Zynq designs

    In this lab we will learn how to use a hardware debugging interface to to perform run-time interactions with IP cores. 1. Adding a IP JTAG-AXI core to the designPlease select Add IP and choose JTAG to AXI Master Core from IP catalog. After that ...
  • [PP-10] Lab 7 - Adding a custom IP

    In this lab we will learn how to create a custom IP, add it to the IP catalogue and use it in the design. 1. How to create a new AXI peripheralPlease select from main bar option: Tools->Create and Package IP New IP. There will appear a wizard...