Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Have a question about the Next-Gen BeagleBone? Ask it here!
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 197 replies
  • Subscribers 72 subscribers
  • Views 24284 views
  • Users 0 members are here
  • beagle
  • bbb
  • BeagleBone
  • beagle_bone
  • bb_black
  • beagle_bone_black
Related

Have a question about the Next-Gen BeagleBone? Ask it here!

bluescreen
bluescreen over 13 years ago

There is a lot of excitement about TI's Next-Gen BeagleBone. If you have a specific question about its performance characteristics, tech specs, or anything else, post it as a reply to this thread. We are working closely with TI and will make sure to respond to your questions.  Thanks everyone!  Sagar

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 13 years ago in reply to e14 Contributor +2
    Until we have some space to work in, I might as well add to this thread: I've not had much time to experiment with the board recently, but I had an hour today, and I tried powering the board from a battery…
  • shobhitkukreti
    shobhitkukreti over 13 years ago +1
    I just ordered a Beagle Bone. What will be the difference in the present beagle bone and the next gen beagle bone ?
  • jkridner
    jkridner over 13 years ago in reply to johnbeetem +1
    The demo I've been showing here at ELC is using an Attic Lapdock. The only special hack required is a USB cable that doesn't short power sine the Lapdock sources power through a port that normally should…
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    For anyone else with one of these, see

    https://groups.google.com/forum/#!category-topic/beagleboard/beaglebone-black/G_QjWvBNXvc

     

    you'll probably want to go to http://circuitco.com/support/index.php?title=Updating_The_Software and get the latest software image (2013.05.3 as of now) before trying to do anything with opkg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    you'll probably want to go to http://circuitco.com/support/index.php?title=Updating_The_Software and get the latest software image (2013.05.3 as of now) before trying to do anything with opkg

     

    Something must have been wrong with the build.  Looks like they pulled it.  I can see it in the change history so you're not a liar image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bwelsby
    bwelsby over 13 years ago in reply to mikeconnell

    There are a few pre-built images around but I built my own using the Rober Nelson build instructions the rootfs he provides has apache2 and sshd installed and running,  no X windows so just console but then once it's up and running you can configure whatever else you need.

     

    I boot and run from a 16Gbyte class 10 uSD card not the eMMC. I also have a 1TByte USB HD which I use for development and backup.

     

    .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    On top of this, several packages that I use regularly are not available in opkg list despite being provided in every other distro that I've used,

    I won't argue that angstrom has issues, but as you know from other discussions it's my belief that all distros have issues. That said, a distro having different goals and building on different design decisions shouldn't come as any surprise, the same could be said for arch vs debian vs fedora vs gentoo (and I see there's now a gentoo build for BBB which may please you) vs suse vs slackware, they all have different goals and provide different packages compiled in different ways.

    One of my pet peeves is that in a lot of cases you have something like Raspbian trying to force a full desktop distro into an embedded device that really doesn't have the resources for it, so I quite like that angstrom leaves out a lot of non-essential stuff that I'd be tempted to lump into the 'bloat' category myself.

     

    I also assume that your set of regularly used packages is different from mine and from Brians too, so not sure it's fair to compare that way. What doesn't work for you might be fine for me.

     

    On the angstrom website, I know what you mean. You'll also notice that the angstrom version that appears on the BBB doesn't seem to be very closely related to the website, in fact I suspect you couldn't rebuild the BBB angstrom version yourself if you start at that site. I'm not actually sure you could rebuild it at all as I don't think enough of the pieces are available or well enough documented anywhere.

    But you have to ask yourself if that's better or worse for other distros. We've seen the problems Mike Thomson had duplicating the debian build system in order to start on Raspbian, so I expect it's just a difference in how far off the bottom of the scale they all are.  Gentoo and LFS may be different in that regard, but then so are their goals.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to bwelsby

    Brian Welsby wrote:

     

    spent days / weeks trying to get things working on Angstrom only to find that packages are out of date, built for 3.2 kernel, have bits missing

    All distros have that problem though. Once you reach a certain point, and that might be just 100 or so packages, it starts to become a real challenge to keep up to date with everything and to handle the interdependant forward and backward breaking changes. 

    Generally out of date only matters if there's a security fix or new feature you require that's missing in the old version.

     

    Something being built for an older kernel generally isn't an issue and can often be a good thing. 3.2 really isn't old enough to be a big issue here.  However, if you think having things built for the current kernel is good, then I encourage you to rebuild glibc against the 3.10 kernel (use the --enable-kernel=3.1.0 configure option). When you find a bug in 3.10 that causes you to have to revert to 3.9.x until the bug gets fixed you'll have all sorts of fun when you reboot.

     

    Bits missing is a bigger issue, most often when something's been built without some necessary feature.  Building something from source because there's no package available is usually ok. Building something where a package exists just to enable a feature comes with a much more interesting set of problems.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    I have no doubt that Angstrom's goals are different, and the BBB's version of Angstrom different yet again.  That's not the problem.

     

    The problem is that whatever those goals are, they do not include the distro being maintained in working order by a maintainer.  Instead, it's unmaintained so that problems persist over long periods of time --- monitoring the IRC logs shows the same problems coming up again and again as beginners arrive and report their woes.  Quite often they're even ridiculed.  And no bug tracker means no bug tracking and no responsibility for quality.

     

    Nor do those goals include the distro continually being expanded with more packages so that end users used to other distros have a good likelihood of finding their favorite packages ready to install so that getting work done is just minutes away.  Instead they have to port any missing applications themselves, because the maintainer's principle is "I do nothing, if you want something done then do it yourself."

     

    Such "goals" are, to my mind, not the goals of a distro worth using.  I can fix pretty much any problem after decades in the *nix world.  But why should I have to?

     

    Because of the lack of bug tracking and responsible maintenance, the same problems are being fixed by thousands of users in parallel as they discover them, and then fixed again for each new image that they download and write.  What a total waste of everyone's time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to morgaine

    Every identified problem deserves a proposed solution, so here are my recommendations to Jason Kridner.  Since Angstrom is not just a hobby distro but part of commercial products and the quality of the supplied operating system impacts on Beagleboard.org and TI, do the following:

     

    • Appoint a second maintainer in addition to the existing one.
    • Make the new maintainer's first responsibility to implement a bug tracker.
    • Make the new maintainer's second responsibility to implement an automated continuous build system.
    • Make the new maintainer's ongoing responsibility to raise the quality of the distro by 1) fixing bugs caught by the continuous build system, 2) fixing bugs in order of priority on the tracker, and 3) adding packages identified as missing and/or requested on the tracker.
    • Proactively add items to the bug tracker based on problems reported on the mailing list and on IRC.

     

    I guess it's obvious enough, but sometimes even obvious solutions need stating.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bwelsby
    bwelsby over 13 years ago in reply to e14 Contributor

    I don't disagree with what you are saying, all I want is the basic kernel and the tools to build what I need.

     

    As an example, I was trying to get Qt working...  On the BBB just install the Qt tools and you get Error required kernel 3.2.0 so check the BBB forums and the response there is that as opengl-es isn't yet available for kernel 3.18 you can't have it  so install with --force-depends and most of it will work. Ok so far so good but missing some functionality..  so I thought what about using Qtcreator on desktop and cross compile / develop Qt on desktop as per excellent tutorials on Derek Malloys site (written for BBW) you can download the toolchain etc etc but when you go to the Angstom site to get the toolchain you see the ones with qte were produced in 2011 and are Qt v4.6.1.

    I thought I would see about bringing this up to v4.8.x but first of all try to build the tool chain as is.   I installed all the Angstrom build system, rebuilt the kernel etc all worked so then tried the bitbake recipe to build the qte toolchain. it started the process, got so far then error saying it couldn't find the compiler???  turns out it was looking for a different cross compiler to the one the system had built / installed so that then means getting into all the recipes understanding all the bitbake system etc etc..... just too much. It looks like I was using parts of the system that was created in 2011 with the current build system that has been put together for the 3.18 kernel development so even though the recipes are there they are no longer compatible.

     

    On Debian I just install the Qt4 sdk and "everything" is there including qtcreator, and the demos and examples I installed xorg and fluxbox as the window manager and I had an application up and running within minutes. I downloaded the Qt serial port addon and it compiled installed and tested working. 

     

    I have also installed on my BBB the software for my 3D printer I am building and yet again it just works.

     

    If I want to use Java, Python, Perl, PHP, Ada, Fortran, or whatever I am confident that with Debian I can, with Angstrom I expect many issues.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to bwelsby

    In effect, you're saying that the distro is unmaintained and so its problems are revealed continually by users as they try to get work done, instead of being caught and revealed by an automated continuous build system.

     

    That's a substantially shorter statement of the problem. image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • bwelsby
    bwelsby over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    In effect, you're saying that the distro is unmaintained and so its problems are revealed continually as users try to work with it instead of being revealed by an automated continuous build system.

     

    That's a substantially shorter statement of the problem. image

     

    Yes image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to bwelsby

    Brian Welsby wrote:

     

    Yes image

    I've added it to my list of recommendations as the new maintainer's "second responsibility".

     

    Unfortunately the probability of Jason looking here is rather small, and this being a catch-all thread, all this will soon submerge without trace.  Even if seen, the likelihood of these concerns being shared is unknown and probably low, and the likelihood of change even lower.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Such "goals" are, to my mind, not the goals of a distro worth using.

    I don't disagree, but you can't deny that if those really are their goals then they're doing well at meeting them image

     

    I would disagree with your other post though. Having just one additional maintainer isn't enough, it needs a team of people who are interested and will actively contribute. If the current maintainer is blocking the process then it's probably time to remove the roadblock.  The project as a whole won't survive on the shoulders of just one or two people, a distro is too big for that.

     

    Yes there needs to be a public bug tracker, a mailing list, up to date documentation, and the full build system needs to be in a public git tree somewhere so that if the existing maintainers disappear or become roadblocks then others can fork the whole thing without a ground-up rebuild.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Such "goals" are, to my mind, not the goals of a distro worth using.

    I don't disagree, but you can't deny that if those really are their goals then they're doing well at meeting them image

     

    I would disagree with your other post though. Having just one additional maintainer isn't enough, it needs a team of people who are interested and will actively contribute. If the current maintainer is blocking the process then it's probably time to remove the roadblock.  The project as a whole won't survive on the shoulders of just one or two people, a distro is too big for that.

     

    Yes there needs to be a public bug tracker, a mailing list, up to date documentation, and the full build system needs to be in a public git tree somewhere so that if the existing maintainers disappear or become roadblocks then others can fork the whole thing without a ground-up rebuild.