Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Have a question about the Next-Gen BeagleBone? Ask it here!
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 197 replies
  • Subscribers 72 subscribers
  • Views 24520 views
  • Users 0 members are here
  • beagle
  • bbb
  • BeagleBone
  • beagle_bone
  • bb_black
  • beagle_bone_black
Related

Have a question about the Next-Gen BeagleBone? Ask it here!

bluescreen
bluescreen over 13 years ago

There is a lot of excitement about TI's Next-Gen BeagleBone. If you have a specific question about its performance characteristics, tech specs, or anything else, post it as a reply to this thread. We are working closely with TI and will make sure to respond to your questions.  Thanks everyone!  Sagar

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 13 years ago in reply to e14 Contributor +2
    Until we have some space to work in, I might as well add to this thread: I've not had much time to experiment with the board recently, but I had an hour today, and I tried powering the board from a battery…
  • shobhitkukreti
    shobhitkukreti over 13 years ago +1
    I just ordered a Beagle Bone. What will be the difference in the present beagle bone and the next gen beagle bone ?
  • jkridner
    jkridner over 13 years ago in reply to johnbeetem +1
    The demo I've been showing here at ELC is using an Attic Lapdock. The only special hack required is a USB cable that doesn't short power sine the Lapdock sources power through a port that normally should…
Parents
  • halherta
    halherta over 13 years ago

    My question is about the 2GB emmc. While its possible to install a minimal Ubuntu/Angstom in 2GB, If one needs a install a desktop environment, a bunch of libraries (say QT), a bunch of programs and Apache, one will need more that 2GB. I understand that we can still use SD card but how can one parition the root filesystem between the eMMC and the SD Flash to really maximize loading speeds ? Is this something that TI is looking at providing solutions for? or is it simply hoped that the community will figure it out ?

     

    Because if it will be difficult to use the eMMC along with SD, most people (wanting to run Linux) will default to using only the SD card and the 2GB eMMC will not be used.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to halherta

    I'll try to be diplomatic but this comment is stupid. The BB was designed as an extremely low power, extremely high capacity, embedded controller. I have a BB running a web server and doing industrial control. It's like an Arduino on steriods. The NG BB has a more powerful processor and 8 times the RAM. Complaining that it doesn't have enough storage, well, buy a 1TB usb drive and it will have plenty of storage. The BB and NG BB are not high powered development systems. On the other hand, they are less than $100. The eMMC is there for when the unit is running as an embedded controller. For that, it's more than enough.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • halherta
    halherta over 13 years ago in reply to e14 Contributor

    Bill,

    I already have a beaglebone running Ubuntu 13.04 + LXDE + QT and that combination requires 1.6+GB of flash. On my Raspberry Pi I'm running the slighly less bloated Raspbian (Debian Wheezy) + LXDE requires about 1.2GB.

     

    Sure if you want to toggle some gpios it doesn't matter, but if you want to build embedded GUI applications, run mini-servers or do any serious Linux stuff, 2GB of onboard flash is at the very best the bare minimum. Ofcourse one could always rely solely on the SD card but this means that the emmc will not be used as much (despite its superior performance) and that it would add to the cost of manufacturing the next-gen beaglebone unnecessarily. I would've much liked to see an emmc connector instead that allows users to choose the emmc capacity suited for their applications. Granted the BB & NG BB are very small boards and this may be non-ideal space wise.

     

    The BB and NG BB maynot be powerful  systems, but I'd expect them to do pretty much anything that the RasberryPi can do with its older and underpowered ARM11 core, especially the NG BB, since it will have HDMI and 512 MB of RAM.

     

    Running GUI applications, Minimal Desktop Environments  and servers should not be considered too much for these platforms.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • halherta
    halherta over 13 years ago in reply to e14 Contributor

    Bill,

    I already have a beaglebone running Ubuntu 13.04 + LXDE + QT and that combination requires 1.6+GB of flash. On my Raspberry Pi I'm running the slighly less bloated Raspbian (Debian Wheezy) + LXDE requires about 1.2GB.

     

    Sure if you want to toggle some gpios it doesn't matter, but if you want to build embedded GUI applications, run mini-servers or do any serious Linux stuff, 2GB of onboard flash is at the very best the bare minimum. Ofcourse one could always rely solely on the SD card but this means that the emmc will not be used as much (despite its superior performance) and that it would add to the cost of manufacturing the next-gen beaglebone unnecessarily. I would've much liked to see an emmc connector instead that allows users to choose the emmc capacity suited for their applications. Granted the BB & NG BB are very small boards and this may be non-ideal space wise.

     

    The BB and NG BB maynot be powerful  systems, but I'd expect them to do pretty much anything that the RasberryPi can do with its older and underpowered ARM11 core, especially the NG BB, since it will have HDMI and 512 MB of RAM.

     

    Running GUI applications, Minimal Desktop Environments  and servers should not be considered too much for these platforms.