Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Have a question about the Next-Gen BeagleBone? Ask it here!
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 197 replies
  • Subscribers 72 subscribers
  • Views 24605 views
  • Users 0 members are here
  • beagle
  • bbb
  • BeagleBone
  • beagle_bone
  • bb_black
  • beagle_bone_black
Related

Have a question about the Next-Gen BeagleBone? Ask it here!

bluescreen
bluescreen over 13 years ago

There is a lot of excitement about TI's Next-Gen BeagleBone. If you have a specific question about its performance characteristics, tech specs, or anything else, post it as a reply to this thread. We are working closely with TI and will make sure to respond to your questions.  Thanks everyone!  Sagar

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 13 years ago in reply to e14 Contributor +2
    Until we have some space to work in, I might as well add to this thread: I've not had much time to experiment with the board recently, but I had an hour today, and I tried powering the board from a battery…
  • shobhitkukreti
    shobhitkukreti over 13 years ago +1
    I just ordered a Beagle Bone. What will be the difference in the present beagle bone and the next gen beagle bone ?
  • jkridner
    jkridner over 13 years ago in reply to johnbeetem +1
    The demo I've been showing here at ELC is using an Attic Lapdock. The only special hack required is a USB cable that doesn't short power sine the Lapdock sources power through a port that normally should…
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Hi,

     

    How does the XAM3359AZCZ on the initial run of beaglebone compare to AM3358BZCZ100 which would feature on the final runs ?

    What are the feature differences ? and why is this processor switch being done ?

     

    --

    Kunal

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to e14 Contributor

    Kunal Ghosh wrote:

     

    How does the XAM3359AZCZ on the initial run of beaglebone compare to AM3358BZCZ100 which would feature on the final runs ?

    What are the feature differences ? and why is this processor switch being done ?

    I'm not a TI employee or representative, but I believe the A->B means that the silicon revision has gone from 2.0 to 2.1.  According to TI's Silicon Errata document, the only behavioral change is improved latch-up.  The "100" is the important part -- it's now a 1 GHz part.  The initial "X" means it's an "experimental" part rather than a fully-qualified device, i.e., you get to be a pioneer image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to johnbeetem

    what about the 9->8 in 3359A -> 3358B? 

     

    and what is the DDR3 clock speed?

    I've seen 300MHz, 400MHz, 600MHz, and 800MHz.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to e14 Contributor

    coder27 wrote:

     

    what about the 9->8 in 3359A -> 3358B? 

    The PRUSS can't do EtherCAT, which is a form of pass-through switching between Ethernet ports so you don't have to store and forward complete frames.  Since there's only one Ethernet port on BeagleBone, it's not worth paying extra for EtherCAT.  I don't know any details -- I just looked up EtherCAT myself.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    coder27 wrote:

    and what is the DDR3 clock speed?

    I've seen 300MHz, 400MHz, 600MHz, and 800MHz.

    I'd suggest grabbing a copy of the SRM from

    http://circuitco.com/support/index.php?title=BeagleBoneBlack#LATEST_PRODUCTION_FILES_.28A5A.29

    it lists the DDR3L as running at 606Mhz (303Mhz base clock). Quite why the slightly odd frequency I don't know, but I'm sure there will be a reason.

    The SRM will answer all the basic hardware questions, but you'll probably need individual datasheets for the real details.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to johnbeetem

    Hi John, by PRUSS were you referring to -> http://processors.wiki.ti.com/index.php/Programmable_Realtime_Unit_Subsystem ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to johnbeetem

    Quite an insight ( I am completely new to all of this ) . Does the "X" usually (by most manufacturers) refer to experimental ?

    I went through the BeagleBoneBlack system reference manual, as suggested by selsinork, and it atleast made one thing clear:

    "We do not expect any benefit from moving to this device and there should be no impact seen as a result of making this move."

     

    So, the early adopter wouldn't be at a loss when Circuitco decides to move to the newer chip image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to johnbeetem

    Quite an insight ( I am completely new to all of this ) . Does the "X" usually (by most manufacturers) refer to experimental ?

    I went through the BeagleBoneBlack system reference manual, as suggested by selsinork, and it atleast made one thing clear:

    "We do not expect any benefit from moving to this device and there should be no impact seen as a result of making this move."

     

    So, the early adopter wouldn't be at a loss when Circuitco decides to move to the newer chip image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • johnbeetem
    johnbeetem over 13 years ago in reply to e14 Contributor

    Kunal Ghosh wrote:

     

    Quite an insight ( I am completely new to all of this ) . Does the "X" usually (by most manufacturers) refer to experimental?

    Many manufacturers use a designation like this for "preproduction" chips.  Generally they're functionally correct, but they may not meet all the timing and electrical parameters over the full temperature and voltage range.  Since chips vary between fabrication runs, it takes a while before you really have a full picture of how they're going to perform under all conditions.  The manufacturer may need to tweak the timing specs or tweak the process to make chips that match the data sheets.

     

    The "X" parts let designers get started using actual chips.  We generally are using accurate power supplies and running everything at room temperature, so if the chip doesn't work properly at 85C and 3.0V we're not going to notice during development.  We hope that the fully qualified chip is ready by the time we need it for full temperature range testing and for production.