Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Have a question about the Next-Gen BeagleBone? Ask it here!
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 197 replies
  • Subscribers 72 subscribers
  • Views 24643 views
  • Users 0 members are here
  • beagle
  • bbb
  • BeagleBone
  • beagle_bone
  • bb_black
  • beagle_bone_black
Related

Have a question about the Next-Gen BeagleBone? Ask it here!

bluescreen
bluescreen over 13 years ago

There is a lot of excitement about TI's Next-Gen BeagleBone. If you have a specific question about its performance characteristics, tech specs, or anything else, post it as a reply to this thread. We are working closely with TI and will make sure to respond to your questions.  Thanks everyone!  Sagar

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 13 years ago in reply to e14 Contributor +2
    Until we have some space to work in, I might as well add to this thread: I've not had much time to experiment with the board recently, but I had an hour today, and I tried powering the board from a battery…
  • shobhitkukreti
    shobhitkukreti over 13 years ago +1
    I just ordered a Beagle Bone. What will be the difference in the present beagle bone and the next gen beagle bone ?
  • jkridner
    jkridner over 13 years ago in reply to johnbeetem +1
    The demo I've been showing here at ELC is using an Attic Lapdock. The only special hack required is a USB cable that doesn't short power sine the Lapdock sources power through a port that normally should…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    a post in the google group suggests it's available here http://dominion.thruhere.net/koen/angstrom/beaglebone/?C=M;O=D from the person who builds the images, as a couple of others have posted that it's vanished off the official page. There's a newer image up on that site too.

     

    Teething troubles can only be expected at this stage especially as more people get their hands on them.  Still it would be nice if they'd added a "pulled because of...." message so that people who've installed it already know what to expect.

     

    I'm not a fan of forums at the best of times, but that google groups thing they're using is awful, and the general mixture of beagleboard, beaglebone and beaglebone-black stuff leaves you never quite sure if what you're reading even applies to your board.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    that google groups thing they're using is awful, and the general mixture of beagleboard, beaglebone and beaglebone-black stuff leaves you never quite sure if what you're reading even applies to your board.

     

    Totally agree with both of those points.

     

    It would be easy enough for us to make a dedicated BeagleBone (or even more specific BBB) group here to categorize information more clearly, but I suspect that the upstream info isn't ever going to get any clearer because the BeagleBoard old timers have grown up with their pre-AM3358 gear and probably don't see any issue.

     

    The present single thread isn't helping either --- all this info is going to get submerged and lost very quickly.  The problem is particularly acute for beginners, who are faced with a long thread to navigate and no way to title their own posts to highlight their question.  Nobody is benefiting from this.

     

    We really ought to be capitalizing on Element 14's effective group system for BB[B].  It has worked out very well for Raspberry Pi, and is likely to prove equally useful for managing info and discussions about BBB better than is being done at present.

     

    Morgaine.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    I'm not a fan of forums at the best of times, but that google groups thing they're using is awful, and the general mixture of beagleboard, beaglebone and beaglebone-black stuff leaves you never quite sure if what you're reading even applies to your board.

    I agree - I've been trying to find a fix for a problem I'm having with using HDMI and I keep coming across stuff that doen't apply to the BBB despite putting "BBB" or "BeagleBone Black" into the search terms

     

    I can't find a way to compensate for overscan or to set the resulution manually (unlike the Pi which is actually very good in that regard).

    I posted a question there yesterday.

     

    https://groups.google.com/forum/#!searchin/beagleboard/bbb$20uEnv.txt/beagleboard/xobKNktj6WI/mZsxCRJMwasJ

     

    I haven't had any response as yet but I have a horrible feeling after reading the reply by Robert Nelson in this other thread about HDMI problems that there may be no solution:

     

    https://groups.google.com/forum/#!searchin/beagleboard/bbb$20uEnv.txt/beagleboard/fPBgF7j_WX4/XrI0TUrVsPUJ

     

    I was going to update to the image mentioned above (2013.05.3) that has now been pulled as it apparently defaulted to 1280x720 - maybe I'll try the newer one or maybe I'll wait a while and see what happens next. image

     

    It also strikes me as slightly strange that they didn't fix the "no audio output over HDMI" before doing a production release.

     

    I'm not convinced at the moment that the BBB would be a very good "out of the box" experience for a novice when compared with the Pi in present form.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    The present single thread isn't helping either --- all this info is going to get submerged and lost very quickly.  The problem is particularly acute for beginners, who are faced with a long thread to navigate and no way to title their own posts to highlight their question.  Nobody is benefiting from this.

    Yeah, unfortunately while we only have a BBB discussion area that's buried in the bowels of the knode and therefore hard to find it's difficult to do a lot about it. The title of this thread probably doesn't help either.

     

    Until the Admins decide to create a top level BBB group I think we're stuck.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    dhid wrote:

     

    I agree - I've been trying to find a fix for a problem I'm having with using HDMI and I keep coming across stuff that doen't apply to the BBB despite putting "BBB" or "BeagleBone Black" into the search terms

    I keep finding things where you think you've got a BBB specific page but the link from there takes you to a generic BeagleBoard (not even original beaglebone) page. To the point that I was given a BeagleBoard xM SRM at one stage.

     

    Unseen barriers like this will put off a lot of beginners.

     

    I haven't had any response as yet but I have a horrible feeling after reading the reply by Robert Nelson in this other thread about HDMI problems that there may be no solution:

    hmm.. I see him mention KMS image 

    It also strikes me as slightly strange that they didn't fix the "no audio output over HDMI" before doing a production release.

    I'm sure these things will get fixed in time, but as there's already a DVI with audio cape I agree it's surprising it doesn't work yet

    I'm not convinced at the moment that the BBB would be a very good "out of the box" experience for a novice when compared with the Pi in present form.

    The Pi has had over a year to get it's act together, it had its share of issues in the first few weeks after availability as well. If the tether to your main PC works, and it didn't for me for unknown reasons, I expect the BBB will be a much better starting point. The web based interface, IDE, bonescript stuff etc certainly looks very slick and much better for a beginner than a command prompt and not knowing you need to type startx...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    dhid wrote:

     

    I can't find a way to compensate for overscan or to set the resulution manually (unlike the Pi which is actually very good in that regard).

    I posted a question there yesterday.

    did you try 'nomodeset' to stop KMS being stupid ?

     

    Don't know if it helps or not, but there seems to be a way to override the KMS settings. kernel-parameters.txt has the following:

     

    drm_kms_helper.edid_firmware=[<connector>:]<file>

                            Broken monitors, graphic adapters and KVMs may

                            send no or incorrect EDID data sets. This parameter

                            allows to specify an EDID data set in the

                            /lib/firmware directory that is used instead.

                            Generic built-in EDID data sets are used, if one of

                            edid/1024x768.bin, edid/1280x1024.bin,

                            edid/1680x1050.bin, or edid/1920x1080.bin is given

                            and no file with the same name exists. Details and

                            instructions how to build your own EDID data are

                            available in Documentation/EDID/HOWTO.txt. An EDID

                            data set will only be used for a particular connector,

                            if its name and a colon are prepended to the EDID

                            name.

     

     

    So possibly you can write an EDID that does what you need ?

     

    No way for me to try it - don't have a microHDMI cable yet !

     

    Oh, and the first few lines of that EDID/HOWTO.txt file really says quite a lot about KMS image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    To the point that I was given a BeagleBoard xM SRM at one stage.

    Yes I think I must have clicked on the same link as it wasn't until I started to read it that I realised it was for the wrong board!

     

    hmm.. I see him mention KMS image 

    I'm not a Linux expert at all but does this mean that you have to have a suitable EDID file to force a particular mode?

     

    The Pi has had over a year to get it's act together, it had its share of issues in the first few weeks after availability as well. If the tether to your main PC works, and it didn't for me for unknown reasons, I expect the BBB will be a much better starting point. The web based interface, IDE, bonescript stuff etc certainly looks very slick and much better for a beginner than a command prompt and not knowing you need to type startx...

    Yes that's true and we won't mention the USB problems! I spent may "happy" hours hunting for different keyboards and mice in the early days of Pi, including a late night trip to Asda to buy a keyboard which worked, despite having various ones lying around, none of which did work. Then of course the little design "hiccup" over the power rails........image

     

    Regards tethering - I couldn't get SSH working using the included browser client so I ended up using putty, but I agree the concept is good if they can fine tune it so it works ok on most browser and operating system combinations.

     

    EDIT:

     

    Sorry selsinork I hadn't seen your other reply before posting this.

     

    Thanks I'll have a look at the kernel-parameters.txt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    dhid wrote:

     

    I'm not a Linux expert at all but does this mean that you have to have a suitable EDID file to force a particular mode?

    The EDID is supposed to be supplied by the display, essentially there's an I2C connection between the display and the device. Called DDC - http://en.wikipedia.org/wiki/Display_Data_Channel

    This has been around since the 15pin vga days at least. It allows the display to essentially have a small eeprom containing descriptions of the various modes that it supports. The connected device can read these and set itself up accordingly. In some cases the I2C connection can also be used for software control of the display brightness, contrast etc.

     

    However, historically the display mode in windows, linux etc has been set manually in the driver. So all sorts of displays either don't provide the data at all, don't provide correct data or whatever.  The downside to KMS appears to be that it expects everything to play by the rules and unconditionally believes whatever rubbish it reads out of the EDID - leading to problems when something is not right, and that could be as simple as the necessary connections are missing from the cable.

     

    So at some point they've provided the option to force KMS to use an EDID provided by the user instead of believing the display. That gives you a way out, but is rather different from the older kernel command line options that google will turn up.

    I've not looked in detail, but I suspect it doesn't give you the same level of control as you can get from config.txt on the Pi. For example, as EDID was originally for computer displays I don't know if it'll have a way to specify overscan settings to solve your problem.

    Some details on EDID data format here http://en.wikipedia.org/wiki/Extended_display_identification_data I don't see anything specific for overscan though there may be ways to use horizontal blanking ot border settings to deal with it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Don't reach for the soldering iron just yet.  The heartbeat LED on USER0 is controlled by the kernel, so a soft hammer should provide the desired retinal relief. image

    root@beaglebone:~# cd /boot

    root@beaglebone:/boot# dtc -I dtb -O dts am335x-boneblack.dtb > bb.dts

    root@beaglebone:/boot# patch -p0 < bbb-devicetree.patch

    root@beaglebone:/boot# dtc -I dts -O dtb  bb.dts > bb.dtb

    root@beaglebone:/boot# mv am335x-boneblack.dtb am335x-boneblack.dtb.org

    root@beaglebone:/boot# mv bb.dtb am335x-boneblack.dtb

    root@beaglebone:/boot# reboot

     

    where the bbb-devicetree.patch file contains

     

    --- bb.dts~     2000-01-02 04:37:54.765635166 +0000

    +++ bb.dts  2000-01-02 04:41:04.373057063 +0000

    @@ -839,7 +839,7 @@

                            led0 {

                                    label = "beaglebone:green:usr0";

                                    gpios = <0x9 0x15 0x0>;

    -                               linux,default-trigger = "heartbeat";

    +                               linux,default-trigger = "none";

                                    default-state = "off";

                            };

     

     

    your eyeballs will thank you image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    dhid wrote:

     

    I'm not a Linux expert at all but does this mean that you have to have a suitable EDID file to force a particular mode?

    The EDID is supposed to be supplied by the display, essentially there's an I2C connection between the display and the device. Called DDC - http://en.wikipedia.org/wiki/Display_Data_Channel

    This has been around since the 15pin vga days at least. It allows the display to essentially have a small eeprom containing descriptions of the various modes that it supports. The connected device can read these and set itself up accordingly. In some cases the I2C connection can also be used for software control of the display brightness, contrast etc.

     

    However, historically the display mode in windows, linux etc has been set manually in the driver. So all sorts of displays either don't provide the data at all, don't provide correct data or whatever.  The downside to KMS appears to be that it expects everything to play by the rules and unconditionally believes whatever rubbish it reads out of the EDID - leading to problems when something is not right, and that could be as simple as the necessary connections are missing from the cable.

     

    So at some point they've provided the option to force KMS to use an EDID provided by the user instead of believing the display. That gives you a way out, but is rather different from the older kernel command line options that google will turn up.

    I've not looked in detail, but I suspect it doesn't give you the same level of control as you can get from config.txt on the Pi. For example, as EDID was originally for computer displays I don't know if it'll have a way to specify overscan settings to solve your problem.

    Some details on EDID data format here http://en.wikipedia.org/wiki/Extended_display_identification_data I don't see anything specific for overscan though there may be ways to use horizontal blanking ot border settings to deal with it.

    Thanks selsinork I've never really looked at the EDID stuff much before as I've mostly used Windows and what Unix I used in the past was on terminals with no graphics.

     

    Well I've half solved my problem! image

     

    I noticed that RT1 (Polyswitch type fuse for HDMI) was rather hot when I had the HDMI to VGA Adaptor plugged in! Remembering that the HDMI to VGA converters draw a fair bit of current and as the Polyswitch is only 100mA hold current I hooked it out and connected the HDMI 5V to VDD via meter on 300 mA current range and discovered it draws between 140 and 200 mA and worked when connected like this!

     

    So that explains why I got a display briefly when I connected the HDMI converter having already booted connected to the TV but got nothing when booting with it connected directly - there was a couple of seconds before the Polyswitch started to go to high resistance and drop the voltage below that required for the HDMI converter to function correctly.

     

    I've now put a link in between VDD and the HDMI 5V and the HDMI to VGA converter works OK and with no overscan, unlike the TV. I just need to try to sort out the overscan problem when connected to the TV.

     

    I'll start having a play with creating an EDID file and trying different resolutions and refresh rates and see what happens.

     

    Thanks for your interest and help - much appreciated!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>