Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Have a question about the Next-Gen BeagleBone? Ask it here!
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 197 replies
  • Subscribers 72 subscribers
  • Views 24561 views
  • Users 0 members are here
  • beagle
  • bbb
  • BeagleBone
  • beagle_bone
  • bb_black
  • beagle_bone_black
Related

Have a question about the Next-Gen BeagleBone? Ask it here!

bluescreen
bluescreen over 13 years ago

There is a lot of excitement about TI's Next-Gen BeagleBone. If you have a specific question about its performance characteristics, tech specs, or anything else, post it as a reply to this thread. We are working closely with TI and will make sure to respond to your questions.  Thanks everyone!  Sagar

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 13 years ago in reply to e14 Contributor +2
    Until we have some space to work in, I might as well add to this thread: I've not had much time to experiment with the board recently, but I had an hour today, and I tried powering the board from a battery…
  • shobhitkukreti
    shobhitkukreti over 13 years ago +1
    I just ordered a Beagle Bone. What will be the difference in the present beagle bone and the next gen beagle bone ?
  • jkridner
    jkridner over 13 years ago in reply to johnbeetem +1
    The demo I've been showing here at ELC is using an Attic Lapdock. The only special hack required is a USB cable that doesn't short power sine the Lapdock sources power through a port that normally should…
  • shobhitkukreti
    shobhitkukreti over 13 years ago in reply to vandana

    Hi. The hardware is custom built and it is under prototype production, but the beagle bone platform will definitely be helpful to work on the software side. We need to compile the old hardware libraries on beaglebone.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jkridner
    jkridner over 13 years ago in reply to shobhitkukreti

    The key differences are that you'd need an HDMI cape and Memory cape to have the same base functionality with the current Bone, so the new Bone will save you some space and money there. The RAM and CPU clock speed is faster on the new Bone. With the new Bone, you'd need to use a cable to access the serial port or JTAG, whereas the current Bone has them built-in. I think this is a great tradeoff for people looking to deploy these boards into several projects.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jkridner
    jkridner over 13 years ago in reply to johnbeetem

    The demo I've been showing here at ELC is using an Attic Lapdock. The only special hack required is a USB cable that doesn't short power sine the Lapdock sources power through a port that normally should normally sink it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jkridner
    jkridner over 13 years ago

    Even though TI sponsors the project, it/we doesn't/don't own it. Others sponsor it as well, so it is better to say BeagleBoard.org's BeagleBone using TI's ARM processor.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jkridner
    jkridner over 13 years ago in reply to e14 Contributor

    >Vandana,  Can you tell us anything about the graphics processor?

     

    Same as current Bone.

     

    >Will it decode 1080p video?

     

    Not at 30fps for common codecs. The target isn't video applications, but 720p MPEG4 has been demonstrated using software-only decode. The color space conversion for the display is typically done using the SGX, but other solutions seem possible to eliminate dependencies on binary blobs. Other projects have claimed open source, yet still require binary blobs. I'm not interested in trying to fool you.

     

    >Will it be user programmable?

     

    Only through OpenGL.

     

    >Will it accelerate X11?

     

    It could, but the only integration right now is color space conversion. GUI performance is still pretty good. I suggest checking out GUIs on the current Bone with whatever you are currently using. The fast CPU and NEON compositing functions help a lot. The new Bone will have faster/more RAM to help along with faster CPU clock speed and faster flash storage.

     

    >Will it accelerate image processing libs, like OpenCV?

     

    Not the 3D controller, but NEON does. OpenCV libs ship with the current Bone. Check out http://beagleboard.org/project/stache

     

    >Does it have proprietary binary blobs that

    >prevent Linux mainline integration?

     

    You'd have to follow-up with Imagination Tech for the long-term status.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • vandana
    vandana over 13 years ago in reply to johnbeetem

    The Next-Gen BeagleBone will support multiple HDMI resolutions!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • vandana
    vandana over 13 years ago in reply to jkridner

    This will ship late April.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    Hi,

     

    A couple of questions, most important (to me) first:

     

    Can you confirm the impact (if any) on the 6 onboard UARTs (esp UARTs 1 thru 5)

     

    Most of my projects use them extensively (Yes, including UART3 that doesnt have TX and RX pins brought out, CTS and RTS pins do have their uses), and in fact one or two projects I'm having to find "innovative" solutions as ideally I'd have 5 or 6 fully operational serial ports image [And yes, proper serial ports are needed for a lot of these for various reasons, including timing precision and an "RF Hostile" environment]. The 6 (4 fully operational) serial ports is one of the major reasons I prefer the bone to the Pi.

     

    Will all the pins still all be brought out the way they are on the current Bone ?

     

     

    Is there any audio onboard, Or do we still need the audio cape for that ?

     

    Will the current bone still be avaliable once production of the new bone ramps up ? (This will be important to me depending on the implications of the new bone on the UARTs)

     

    And finally, what is the colour of the board ? I know there's a new "bright" colour coming, but is it going to be avaliable in two colours, or is the new "bright" colour the only option ? I quite like the white of the current bone. The unzipping pic suggests dark green. That would be so...common image , and certainly isnt "bright" [and more seriously probably harder to read the legends on the board]

     

     

    Best Regards

     

    Iain

     

     

    Iain

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    And just one more question.

     

    Is the PRUSS present on the new 'bone ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to jamodio

    you've all already asked most of my questions, so I'll just add...

     

    gerbers ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>