Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Parallella $99 board now open hardware on Github
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 69 replies
  • Subscribers 61 subscribers
  • Views 9575 views
  • Users 0 members are here
  • zynq
  • xilinx
  • parallella
  • epiphany
  • cortex-a9
  • adapteva
  • arm
Related

Parallella $99 board now open hardware on Github

morgaine
morgaine over 13 years ago

It's probably spreading everywhere like wildfire, but I just read on Olimex's blog that Adapteva's Parallella kickstarter board now has almost all of its development materials on Github in Parallela and Adapteva repos, and is officially being launched as open hardware.

 

The 16-core board is priced at US$99 and its host ARM is a dual-core Cortex-A9 (Xilinx Zynq 7010 or 7020).  It comes with 1GB DDR3, host and client USB, native gigabit Ethernet and HDMI, so at that price this would be a fairly interesting board even without its 16-core Epiphany coprocessor.  (There's a 64-core version planned too.)  For more details see the Parallella Reference Manual.

 

This has all the makings of a pretty fun board.  I hope Element 14 has one eye open in that direction. image

 

Morgaine.

 

 

PS. Note the 4 x Parallella Expansion Connectors (PEC) on the bottom of the board, illustrated on page 19 of the manual and documented on page 26.  They look very flexible for projects, providing access to both Zynq and Epiphany resources.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 12 years ago in reply to johnbeetem +2
    I wonder why in these discussions so many people overlook Lattice. Easily the most fun FPGA company and they DO have FPGAs in phones. Their Ultra Low Density approach fits well with John's definition of…
  • e14 Contributor
    e14 Contributor over 13 years ago +1
    Morgaine Dinova wrote: PS. Note the 4 x Parallella Expansion Connectors (PEC) on the bottom of the board, illustrated on page 19 of the manual and documented on page 26. They look very flexible for projects…
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor +1
    selsinork wrote: I've wondered about these for a while.. 16 or 64 cores of a specialised processor that probably can't run linux or other general purpose OS makes it highly niche. If they sell many of…
Parents
  • morgaine
    morgaine over 12 years ago

    Although Adapteva are still fulfilling their Kickstarter committment, their shop is already open for preorders of the 16-core Epiphany board for November delivery.  Three options appear to be available:

     

     

    Board Model
    GPIOXilinx Device
    Price
    Parallella-16No GPIOZynq-7010$99
    Parallella-16With GPIOZynq-7010$119
    Parallella-16With GPIOZynq-7020$199

     

     

    If "No GPIO" means none, zero, zilch, that doesn't appear very enticing, I must say.  If this describes the situation accurately, the range of application of the basic board will be a lot narrower than expected.  And if the Zynq-7020-based Parallella-16 costs $199, then the price of the Parallella-64 is probably going to be very unfriendly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    If "No GPIO" means none, zero, zilch, that doesn't appear very enticing, I must say.  If this describes the situation accurately, the range of application of the basic board will be a lot narrower than expected.  And if the Zynq-7020-based Parallella-16 costs $199, then the price of the Parallella-64 is probably going to be very unfriendly.

    Given there's an 'optional upgrade' for the GPIO connectors it seems likely that the difference is simply down to installing the connectors.  Any volunteers to hand solder four of those ?

     

    In some ways you can see the reasoning, not having them will not prevent you doing software things on the Epiphany processor.  If you really want gpio, and don't care so much about the Epiphany there are probably better boards.

     

    Am I correct in thinking that the only difference between the 7010 and 7020 is more FPGA space ?  If so, what's this board really meant to be, a dev board for parallel processing on the Epiphany, or an FPGA dev board ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem

    John Beetem wrote:

     

    However, since modern wire-speed routers are implemented in hardware, there's no reason you can't do this with a decent FPGA since managing an end-point is a lot easier than routing.

     

    I think you meant the opposite, that routing is a lot easier than managing an endpoint.  Routing in hardware needs to handle only the IP layer and can ignore all higher-level detail, which is just payload data at the IP level --- that's why good routers can route frames back-to-back even on 10gig.  The routing management protocols and ICMP only come into play at exception or change points, so that's typically left to CPUs to handle at their leisure in all but the highest end backbone routers.

     

    At the endpoints, the entire protocol stack comes into play, which is a heavy burden indeed.  TCP offload engines commonly dedicate an embedded CPU to the task rather than hardware, although as we both mentioned, simple functions like CRC are very commonly implemented in hardware, often as a dedicated instruction in the SoC.

     

    That iTOE Verilog for Virtex and Spartan doesn't look like open source to me. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 12 years ago in reply to morgaine

    @Morgaine and John,

     

    I haven't quite got to full TCP/IP in the fpga yet but I'm currently using a Lattice ECP3 to generate multi fragment UDPs sent out at wire speed to GBE, (external Marvell phy and it runs pretty hot  - which answers an other question). I can't see that it would ever make sense to do all of the work in the FPGA  - things like ARP don't need that kind of speed.

    I would love to get my teeth into some TCP acceleration in the FPGA but it is very expensive in terms of development time and we have already hit issues with common GBE network components (like switches) which cant actually handle wire speed data unconditionally - and the conditions are not well specified.

    One of the problems you hit with sharing the network stack between processor and FPGA is that you end up writing the entire stack, parts in C and parts in VHDL or Verilog - that's why so far we've kept our end very simple with support for UDP, IP, ARP and not much else.

    The phy uses more power than the FPGA and the processor (STM32F407).

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to johnbeetem

    John Beetem wrote:

     

    I'm actually quite amused (not ROFL -- more like rocking back and forth holding my knees chuckling) at the idea that US$99 is expensive for a Zynq board in 2013.  Parallella was originally prototyped with a 7020-based ZedBoard, which is still US$395 (US$319 for academics).  [FYI: ZedBoard is now 1 year old and has sold over 3,000 units.]  There's now a 7010-based MicroZed board for US$199.   IMO getting the cost with Epiphany down to US$99 is pretty impressive, even if that's pre-order pricing.

    Digilent has announced a Zynq 7010-based board called ZYBO for US$149.  Much friendlier I/O than Parallella, including bidirectional HDMI, 16 bit/pixel VGA, 10/100/1G Ethernet, 512 MB DDR3, and five Digilent PMOD connectors for various I/O cards.  I don't think it has any high-density GPIO connectors, so if you need a lot of GPIO you're probably better off with a MicroZed.  It is nice to see Zynq boards coming down to a reasonable price range.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem

    I suspect that Zynq will never have a reasonable price, meaning the price of mass-market Chinese SoCs.  Like Intel, Xilinx seems to believe that keeping prices sky-high is intrinsic to its self-respect and/or survival, and so the company is not playing the game described by that famous saying "The natural price of all semiconductors is the price of their packaging."

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    I suspect that Zynq will never have a reasonable price, meaning the price of mass-market Chinese SoCs.  Like Intel, Xilinx seems to believe that keeping prices sky-high is intrinsic to its self-respect and/or survival, and so the company is not playing the game described by that famous saying "The natural price of all semiconductors is the price of their packaging."

    Xilinx prices on Spartan chips are very attractive IMO.  If you want to use the latest and greatest and highest performance Xilinx chips in big packages, prepare to pay big bucks.  I'm definitely not the target demographic for those chips.  If you wait a few years for them to get the kinks out of the process, you can get Spartans for great prices.  But it's hard to get down to the "price of the packaging" because an FPGA is essentially an SRAM array with some gates attached to it, and SRAM is pretty expensive.

     

    I once nearly throttled a salesman who sold Xilinx chips because he said my designs obviously weren't very "sophisticated".  I held off because I realized that by "sophisticated", he meant designs that required fast, expensive Xilinx chips with high sales commissions.  He didn't mean "using every trick in the book and a few adapted from other books" to fit a complex function into a smallish, not particularly fast Spartan to save big bucks image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem

    John Beetem wrote:

     

    Xilinx prices on Spartan chips are very attractive IMO.

     

    The words "reasonable" (used earlier) and "attractive" as you've been using them are different to the way in which I prefer to use them.  What they mean to you appears to be "Less costly than I expected them to be", or perhaps "Less costly than they were before".  It has no bearing on their actual cost relative to the state of technology.

     

    If people have gotten used to the latest iLust gadget costing $500, then with the above semantic a price drop to $300 would probably be described as making them "reasonable" or "attractive", despite the fact that it's still bloody extortionate when similar functionality is available for under $100.  Of course there's room for quibbling over quality, but in the case of digital semiconductors that excuse practically evaporates because digital technology without the required noise margins simply doesn't work.

     

    I accept that Spartans can be purchased for not much more than the price of packaging, 3A's all the way down to single digit unit prices, but my comment was really aimed at Zynq, or should have been.

     

    My argument about Zynq pricing would have been stronger if I could point to a native Chinese ARM+FPGA with similar functionality but a much lower price tag, but alas I can't, and I'm not even sure how to  start looking.  (And the documentation might not be in any language I understand anyway.)  Despite this weakness, my gut feeling is that Xilinx is making no effort to bring this family of devices to the mass market (which is entirely a function of price), despite having had ample time to do so since the concept was sprung on the world ages ago.  I think it likes to give this particular product an air of exclusivity (and charge accordingly), which is why it's so hard to find the device listed, priced and in stock.

     

    Parallella seems to be very much an oddball, a product that democratizes Zynq despite Xilinx's best efforts at keeping it away from the unwashed masses.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    John Beetem wrote:

     

    Xilinx prices on Spartan chips are very attractive IMO.

     

    The words "reasonable" (used earlier) and "attractive" as you've been using them are different to the way in which I prefer to use them.  What they mean to you appears to be "Less costly than I expected them to be", or perhaps "Less costly than they were before".  It has no bearing on their actual cost relative to the state of technology.

     

    If people have gotten used to the latest iLust gadget costing $500, then with the above semantic a price drop to $300 would probably be described as making them "reasonable" or "attractive", despite the fact that it's still bloody extortionate when similar functionality is available for under $100.  Of course there's room for quibbling over quality, but in the case of digital semiconductors that excuse practically evaporates because digital technology without the required noise margins simply doesn't work.

     

    I accept that Spartans can be purchased for not much more than the price of packaging, 3A's all the way down to single digit unit prices, but my comment was really aimed at Zynq, or should have been...

    Well, the first marketing materials for Zynq said "starting at $15" [Xcell Journal 2Q2011] and maybe they'll get down there some day.  As far as comparing to iGewgaws, it's a question of volume.  A technology that sells 10M - 100M/year is going to be a lot cheaper than FPGAs, which rarely get into high-volume devices for the simple reason that if you're going to have high volumes you're better off synthesizing your Verilog/VHDL into a real ASIC.  FPGA proponents talk about "getting an FPGA into a cell phone", but the reality is that the margins aren't there and cell phones don't need the logic flexibility an FPGA offers.  Proponents say "but wait!  the FPGA is reconfigurable!" but IMO it's hard enough to get one design to work in an FPGA, much less a whole slew of them.  This would change if they'd open up the bitstream formats.

     

    I'd be quite happy to get that $15 chip image  Maybe someday.  It takes a long time for Xilinx parts to get cheaper, and usually you don't see much price movement on generation N until generation N+1 comes out.  Most of the stuff I read about Xilinx these days is about 3-D chip construction and other ways to make their chips more expensive.  Well, that's probably where they make their money, and Spartan is there because otherwise a competitor would take over the entry level, and then leverage themselves up.  As long as the Chinese stay away from FPGAs, I don't expect much change, and FPGAs haven't reached enough volume to get the Chinese interested.

     

    Back to Zynq pricing, I guess I'm not sticker-shocked because my then-company looked into Virtex II-Pro a long time ago.  Our products were mostly based on PowerPC, so the idea of having PowerPC integrated with an FPGA seemed pretty good.  Then we saw the price tag, and quickly went with a cheap PowerPC SoC and a cheap  Spartan-IIE, interconnected with PCI.

     

    Where FPGAs really stand out IMO is medium-volume applications where designing an ASIC is too expensive and too risky, but the design is not practical without a custom chip.  If it's a communication product where protocols may be evolving (or you need to add others in the future), the flexibility of an SRAM-based FPGA is an excellent match, since you can ship a new release of the hardware with each software release.  FPGA are also great for communication test equipment, where the protocols needed to be tested evolve and you'd like to minimize the effort of updating your equipment.  But it's a medium volume product, though with enough margin that current FPGA pricing is, well, pretty "attractive".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem

    John Beetem wrote:

     

    But it's a medium volume product, though with enough margin that current FPGA pricing is, well, pretty "attractive".

    Grrrrrr .... image image image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 12 years ago in reply to johnbeetem

    I wonder why in these discussions so many people overlook Lattice. Easily the most fun FPGA company and they DO have FPGAs in phones. Their Ultra Low Density approach fits well with John's definition of sophisticated and is currently delivering a million parts per day at very low (single $ or less) prices.

    (MInor rant over -BTW I have no connection with Lattice other than as a customer).

     

    Even though I don't use any Xilinx parts at the moment I think the cost/pricing issue is more complex than just the cost of the silicon. Xilinx (and I assume Altera) spend more on software development than on hardware development. They also spend huge sums on research which makes the mega parts possible. They have to get that back somehow and whilst both companies make a profit I don't think they do much better overall than, for example, Linear Technolgy and nothing like as well as Intel have done. (That's in term sof margins not size).

    And much as I like Lattice their approach with simple cheap bits hasn't made them as big as X or A.

     

    I think we'll see the FPGA market grow a lot more - the potential for cheap tiny parts is huge - but tiny is more about price and package - the capability is getting better all the time. I'm already able to get 1000 LUTs for £2 in 100s off but, I think, <<£1 for 100k. The next generation (Lattice 'X03) will expand tiny to cover 640 to 22k LUTs and at lower prices. The space for ASICs gets smaller with each advance of FPGAs - I don't play in the meg chip zone but there is a lot of scope with the cheapo parts.

     

    Hmmm - this has got very off topic - sorry.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to michaelkellett

    I agree with Michael there, and I'd much rather see open source support the underdog than the field leader --- it's easier to gain some influence that way, among other things, and the immoveable leader then feels the lack of love and sometimes reacts.  Look at nVidia as an example of that, against all expectations actually sitting up and taking notice when it got the finger of disrepute pointed at it.

     

    Lattice MachXO2 looks nice, and 'XO3 will probably be even nicer, especially when spelled with an 'O'. image

     

    Michael Kellett wrote:

     

    Hmmm - this has got very off topic - sorry.

    Readers would get extremely confused if we ever managed to stay on topic. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 12 years ago in reply to michaelkellett

    I agree with Michael there, and I'd much rather see open source support the underdog than the field leader --- it's easier to gain some influence that way, among other things, and the immoveable leader then feels the lack of love and sometimes reacts.  Look at nVidia as an example of that, against all expectations actually sitting up and taking notice when it got the finger of disrepute pointed at it.

     

    Lattice MachXO2 looks nice, and 'XO3 will probably be even nicer, especially when spelled with an 'O'. image

     

    Michael Kellett wrote:

     

    Hmmm - this has got very off topic - sorry.

    Readers would get extremely confused if we ever managed to stay on topic. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • morgaine
    morgaine over 12 years ago in reply to morgaine

    I earlier gazed into the future and handwaved:

     

    "Lattice MachXO2 looks nice, and 'XO3 will probably be even nicer"

     

    Well then I got around to looking at their MachXO3 page and discovered ...

     

    Lattice writes:

     

    Integrated Support for the Latest Interfaces - Simplify and optimize your system design using MIPI, PCIe, and GbE hard blocks.

    OK, now they really have my attention! image  This is a gigabit IoT device on a chip at CPLD prices.

     

    Due "October" ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • packrat
    packrat over 12 years ago in reply to morgaine

     

    Morgaine Dinova wrote:

    Michael Kellett wrote:

     

    Hmmm - this has got very off topic - sorry.

    Readers would get extremely confused if we ever managed to stay on topic. image

     

    tts the off topic stuff that makes the messages (threads) so interessting. image

     

    Walt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    I earlier gazed into the future and handwaved:

     

    "Lattice MachXO2 looks nice, and 'XO3 will probably be even nicer"

     

    Well then I got around to looking at their MachXO3 page and discovered ...

     

    Lattice writes:

     

    Integrated Support for the Latest Interfaces - Simplify and optimize your system design using MIPI, PCIe, and GbE hard blocks.

    OK, now they really have my attention! image  This is a gigabit IoT device on a chip at CPLD prices.

     

    Due "October" ...

    I'll save my opinion until I find out what's the cheapest MachXO3 that has PCIe and/or GbE.  For example, you can't get Zynq PCIe until you get up to to the Z-7030, or Spartan-6 PCIe until you get to the XC6SLX25T.