EAGLE User Support (English) Wot, still no package land pattern vias?
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
  • Replies 31 replies
  • Subscribers 181 subscribers
  • Views 2959 views
  • Users 0 members are here
Related

Wot, still no package land pattern vias?

Former Member
Former Member over 11 years ago

The one thing I expected to be fixed in v7 was vias in land patterns. Nope, still AWOL, in spite of a glaring need for thermal transfer to ground via the center pad on some parts. What gives? When is this coming?

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 11 years ago +1
    On 9/18/2014 10:58 PM, Ryan Pettigrew wrote: The one thing I expected to be fixed in v7 was vias in land patterns. Nope, still AWOL, in spite of a glaring need for thermal transfer to ground via the center…
Parents
  • autodeskguest
    autodeskguest over 11 years ago

    On 9/18/2014 10:58 PM, Ryan Pettigrew wrote:

    The one thing I expected to be fixed in v7 was vias in land patterns.

    Nope, still AWOL, in spite of a glaring need for thermal transfer to

    ground via the center pad on some parts. What gives? When is this

    coming?

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/126808

     

     

    Hi Ryan,

     

    This is already possible. Here's what you would do:

     

    In the package:

     

    1. Place the thermal transfer through-hole pads(pads and vias are

    physically the same thing, the distinction we make in EAGLE is that pads

    are always associated with components and go through the hole board,

    vias are on the board and generally associated with transitions between

    layers).

     

    2. Draw polygons enclosing these pads on the Top, Bottom, tStop, bStop,

    tCream, and bCream layers. My assumption here is that the thermal pad

    shows up on both sides of the board, this isn't always the case but for

    the sake of generality I've included them here.

     

    3. In the device editor, assign all of those pads to the same pin of

    your symbol, because they're within the boundaries of the polygon the

    polygon is considered an extension of those pads.

     

    That's pretty much all you have to do, and EAGLE will handle it without

    errors. Section 8.14 of the EAGLE manual covers this in greater

    detail.The Help pages for PAD and SMD provide more details

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to autodeskguest

    CadSoft Guest wrote:

     

    That's pretty much all you have to do, and EAGLE will handle it without

    errors. Section 8.14 of the EAGLE manual covers this in greater

    detail.The Help pages for PAD and SMD provide more details

     

    Jorge, the problem is, you can't then assign it to the via layer, with all the other vias, where it belongs, and where it is convenient for the board assembler to find it, and know what it is, and what its purpose is supposed to be.

     

    I reiterate; I am NOT interested in ways of working around this problem; I am interested in this problem being fixed, so no workaround is required. If I wanted help getting around this limitation in the software, I would have posted in the help forum, not here in the suggestion forum.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to Former Member

    "Ryan Pettigrew"  skrev i nyhetsmeldingen:

    841402075.181411429316209.JavaMail.jive@flmspu-csapp-02.premierfarnell.com

    ...

     

    Jorge, the problem is, you can't then assign it to the via layer, with

    all the other vias, where it belongs, and where it is convenient for the

    board assembler to find it, and know what it is, and what its purpose is

    supposed to be.

     

    I do not see the need to differ those vias/pads from other vias/pads. Maybe

    you can explain why they need to know? Full through vias and pads are

    generally manufactured in the same process afaik.

     

    The only valid argument I can see is that sometimes, when working with

    blind/buried/micro-vias, you may want the heat transfer between controlled

    layers, but doing this in a library editor is not straight forward. It could

    be done with some "vitrual via" placement that needs to be placed manually

    in the board design, and would cause a DRC error if not present.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to Former Member

    On 9/22/2014 7:41 PM, Ryan Pettigrew wrote:

     

    Jorge, the problem is, you can't then assign it to the via layer, with

    all the other vias, where it belongs, and where it is convenient for the

    board assembler to find it, and know what it is, and what its purpose is

    supposed to be.

     

     

    Hi Ryan,

     

    I'm afraid I disagree, thermal vias within a package don't need to be on

    the vias layer. The distinction between pads and vias is something

    internal to EAGLE. When we generate gerber output, through-hole pads and

    vias are always included together, so they're indistinguishable to the

    board house. Even visually within EAGLE they're indistinguishable

    because the pads and vias layers use the same color.

     

    Has the assembler given any special instruction or complaint?

     

    hth,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    On 24/09/2014 4:11 a.m., Jorge Garcia wrote:

     

    A few 'not trues' here

     

     

    I'm afraid I disagree, thermal vias within a package don't need to be on

    the vias layer.

     

    They do if you don't want drills all the way through the PCB

     

      The distinction between pads and vias is something

    internal to EAGLE. When we generate gerber output, through-hole pads and

    vias are always included together,  so they're indistinguishable to the

    board house.

     

    True when talking of the copper for a layer but un-true  when talking

    drills for a multi layer board.

     

    There should be additional drill files for the holes that go between

    particular layers.

     

    Even visually within EAGLE they're indistinguishable

    because the pads and vias layers use the same color.

     

    Not when you specify the colour as the background colour. Then the

    layers they go between makes them visually different

     

    Has the assembler given any special instruction or complaint?

     

     

     

    Eagle's age is becoming an issue. I'm not talking of GUI's or WOW tools

    like 3D but rather not having keep up with the demands placed on the

    designer by reducing geometries of components and board size. There are

    a few basics that have been suggested repeatedly. I feel it will be the

    failure to deliver these that will reduce the Eagle market share. Sure

    add new features the marketing people can use but this should be

    balanced by correcting some basic short comings so the product remains

    solid and not let down by these deficiencies.

     

     

    hth,

    Jorge Garcia

     

     

     

    HTH

    Warren

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    On 9/23/2014 3:47 PM, warrenbrayshaw wrote:

    On 24/09/2014 4:11 a.m., Jorge Garcia wrote:

     

    A few 'not trues' here

     

     

    I'm afraid I disagree, thermal vias within a package don't need to be on

    the vias layer.

     

    They do if you don't want drills all the way through the PCB

     

    Hi Warren,

     

         How often does this come up? Is that what the user is doing here?

    Sometimes it can be beneficial to simplify a discussion by only focusing

    on key aspects of an issue not all general cases. Heat dissipation on

    internal layers is nowhere near as good as on the outer layers. In high

    power situations you want to devote as much copper on the surface layers

    to aid in heat transfer.

         With that said, I should blanket my responses with statements

    indicating the simplifications or assumptions I'm making so thanks for

    keeping me honest.

     

      The distinction between pads and vias is something

    internal to EAGLE. When we generate gerber output, through-hole pads and

    vias are always included together,  so they're indistinguishable to the

    board house.

     

    True when talking of the copper for a layer but un-true  when talking

    drills for a multi layer board.

     

    There should be additional drill files for the holes that go between

    particular layers.

     

         See first comment

    Even visually within EAGLE they're indistinguishable

    because the pads and vias layers use the same color.

     

    Not when you specify the colour as the background colour. Then the

    layers they go between makes them visually different

     

         See first comment. Very few users are even aware that you can do this.

    Generally only users that make frequent use of blind and buried vias use

    it. I don't believe that's the case here.

     

    Has the assembler given any special instruction or complaint?

     

     

    Eagle's age is becoming an issue. I'm not talking of GUI's or WOW tools

    like 3D but rather not having keep up with the demands placed on the

    designer by reducing geometries of components and board size. There are

    a few basics that have been suggested repeatedly. I feel it will be the

    failure to deliver these that will reduce the Eagle market share. Sure

    add new features the marketing people can use but this should be

    balanced by correcting some basic short comings so the product remains

    solid and not let down by these deficiencies.

     

         I agree with this statement, there are a lot of little things that have

    added up and need to be corrected. They are reported and documented, not

    just in our forums but internally as well. I'm hoping for the best.

     

    Jorge Garcia

     

    hth,

    Jorge Garcia

     

     

    HTH

    Warren

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to autodeskguest

    Thermal vias in center pads is standard practice. In general, if the manufacturer doesn't specify HOW MANY center pad thermal vias a part needs, and you can't get a decent answer out of the part manufacturer, you should assume it needs at least one, to be safe. We should easily be able to specify a via, fill, over-plating on either or both sides, and tenting on either or both sides, for a via in a Land Pattern. How many examples do you want, to justify implementing the feature?

     

    An extreme DQFN example, featuring thermal as well as regular vias, here: http://i.stack.imgur.com/itCYK.png

     

    itCYK.png

     

    Note that this is different from people putting wide thru-holes in a center pad so the center pad can be reached by a soldering iron through the board itself, to enable hand-soldering of the QFN. I don't want manufacturers confusing a hack like this with the Class 3 IPC Type VII vias I need.

     

    Please take the necessary steps to support this badly needed feature.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to autodeskguest

    Thank you, Warren. This is what I posted for. Hopefully, a few more like you will poke their heads in to emphasize the point.

    CadSoft Guest wrote:

     

    Eagle's age is becoming an issue. I'm not talking of GUI's or WOW tools

    like 3D but rather not having keep up with the demands placed on the

    designer by reducing geometries of components and board size. There are

    a few basics that have been suggested repeatedly. I feel it will be the

    failure to deliver these that will reduce the Eagle market share. Sure

    add new features the marketing people can use but this should be

    balanced by correcting some basic short comings so the product remains

    solid and not let down by these deficiencies.

     

    HTH

    Warren

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to autodeskguest

    CadSoft Guest wrote:

     

    The only valid argument I can see is that sometimes, when working with

    blind/buried/micro-vias, you may want the heat transfer between controlled

    layers, but doing this in a library editor is not straight forward. It could

    be done with some "vitrual via" placement that needs to be placed manually

    in the board design, and would cause a DRC error if not present.

    You don't need to do it in the library. You should be able to change the layers of the via after the Land Pattern is placed in the design, so you can assign it to whichever ground or thermal planes you find convenient. The footprint via should assume to be for a 2 layer board, like a through hole, but with options for fill, over-plating on either or both sides, and tenting on either or both sides, with layer assignment to take place after the component is placed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 11 years ago in reply to autodeskguest

    CadSoft Guest wrote:

     

    The only valid argument I can see is that sometimes, when working with

    blind/buried/micro-vias, you may want the heat transfer between controlled

    layers, but doing this in a library editor is not straight forward. It could

    be done with some "vitrual via" placement that needs to be placed manually

    in the board design, and would cause a DRC error if not present.

    You don't need to do it in the library. You should be able to change the layers of the via after the Land Pattern is placed in the design, so you can assign it to whichever ground or thermal planes you find convenient. The footprint via should assume to be for a 2 layer board, like a through hole, but with options for fill, over-plating on either or both sides, and tenting on either or both sides, with layer assignment to take place after the component is placed.