Welcome to the Amphenol page on element14. Here you can find things such as our latest news, training videos, and product details. Additionally, you can engage with us in our forums.
Featured Video
You don't have permission to edit metadata of this video.
Amphenol is an innovative and leading edge manufacturer of both connectors and interconnect systems for applications within the Mil-Aero, Telecom, and Industrial markets. Amphenol products cover technologies within both fibre optic and copper products. Specific recent solutions incorporate signal conditioning, electro-optic transceivers and line protection units. Cabled systems utilise over moulding and open loom manufacture of both copper and fibre products.
The Energy Challenge
In today’s evolving energy landscape, balancing supply and demand is critical. Energy Storage System or ESS are bridging this gap, enabling a stable and adaptable energy infrastructure. ESS stores surplus ene...
In today's highly connected world, USB connectors are crucial for ensuring seamless communication across a variety of electronic devices. As technology advances, the need for faster data transfer, higher power capacity, and greater durability c...
The global shift towards sustainable and renewable energy sources is transforming every aspect of life. As the saying goes, change starts at home. The growing importance of greener power sources in households is driving a surge in de...
In recent years, the field of robotics has seen remarkable advancements, transforming industries and reshaping the way we live and work. From industrial automation to autonomous drones and collaborative robots, the capabilities of robotic systems ha...
What are the features that define a smart city?
From smart commutation to intelligent buildings and streets, everything we see today is equipped with the most advanced sensors. Zettabytes of data are being transferred in microseconds to establish c...
SV offers a wide range of IP67 and IP68 waterproof cable assemblies designed to withstand rigorous environments and harsh elements. SV's line of waterproof cable assemblies include o-ring sealed connectors to 1 x 10-8 cc/sec, making them ideal fo...
Amphenol SV Microwave’s newest mmWave addition gives you true 40GHz performance for right angle 2.92mm cable connectors. No need to sacrifice performance for space or change in interface. The same tried and true 2.92mm connector design means st...
SV Microwave’s high speed RF/coaxial reduced flange edge launch connectors are ideal for high frequency PCB applications where precision is key. These rugged, durable and reusable connectors are 30% smaller than the standard flange allo...
SV Microwave has been a trusted provider of interconnect solutions for military and aerospace applications for over 50 years. Browse our high-reliability, high-density products below and order COTS at any time. D3...
SV Microwave's newest facility in Mesa, Arizona officially received its AS9100 certification on November 12, 2019. AS9100 certification is granted to companies who develop and/or design products for the space, defense or aviation markets and maintain...
We are excited to announce the launch of our upgraded Cable Builder featuring a new look and new features! Read below for more information.Alternate between connector and cable type at any time when building your assemblyRequest Delay Matching if des...
SV Microwave in Mesa, Arizona has officially launched! Our new location will foster additional machining capabilities and assembly operations in order to facilitate the growing need for our RF products. We can't wait to serve all of our customers in ...
Stop by and see us at this year's IMS show to check out our latest and greatest extreme frequency connectors, adapters, components and cable assemblies! Booth #303
Check out SV's space qualified connectors, cable assemblies and components. SV has over 50 years experience in assembly, inspection, testing and qualification of space products.SV is the only DLA approved supplier of M3933/30 attenuators (32 GH...
It is SV Microwave's pleasure to congratulate Carol Fleming, SV's Distribution Account Manager, who recently received the award for Employee of the Year within the Administrative category at the SFMA, The South Florida Manufacturers Association, Awar...
Have you noticed a change recently? SV Microwave is excited to announce the launch of our new website! Compatible across multiple devices, SV's newly launched site strives to deliver an awesome user experience. See for yourself & start browsi...
SV has just released a new video on assembling & disassembling our Mini-D RF product! View the video below and on our Videos page:www.youtube.com/watch Interested? Order your Mini-D RF collection today: Click Here!
SilverLine TM 18GHzTest Cables are cost effective, durable, high-performance cable assemblies designed for use in a broad range of test and interconnect applications. Fabricated from rugged, solid PTFE dielectric cable with stainless steel connectors…
Description Amphenol introduces the SuperSpeed USB 3.0 connector solution to better serve the new market demand which requires much higher data rates. SuperSpeed USB 3.0 is operating up to 5Gbps , delivering 10X time the data transfer rate compared to…
FAKRA RF FAKRA RF With recent advancements in communications technology and increased consumer demand for a diverse array of on-board telematics serv ices, RF communications systems have become indispensable components of the modern automobile. To keep…
Barracuda Barracuda The Barracuda range of environmental IP68 sealed connectors is specifically designed for harsh applications where water, dust, oil or spray is present. These moulded connectors are interchangeable with the equivalent Bulgin standard…
Amphenol Socapex HDAS range of board level connectors are a competitive and available alternative to Hypertac HPH. Amphenol Socapex reduces pitch and increases contact density with it’s HDAS range of ruggedised PCB connectors. The cost effective HDAS…