Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Blog Pi Pico Eurocard Development Board
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 14 Apr 2022 4:15 AM Date Created
  • Views 13351 views
  • Likes 17 likes
  • Comments 55 comments
Related
Recommended
  • perfboard
  • testtag_ignore
  • rpibeginner
  • pico_eurocard
  • eurocard
  • prototyping
  • pi pico

Pi Pico Eurocard Development Board

shabaz
shabaz
14 Apr 2022


Introduction


This is going to be an ultra-short blog post because the project is really short – it's a super-basic development board for the Pi Pico. I grew tired of having a Pi Pico dangling from the PC USB port with bits of wire hanging off it, just to do a bit of prototyping. Although the Pi Pico can be used as-is, there is some minimal circuitry needed for more effective use, such as a power supply, supply switching circuitry, and a reset button. Some space for assembling a few additional chips or modules would help too! So, that's what this project delivers on. See James' video (demonstrating the Rev 2.0 board) here:  Why You Need a Raspberry Pi Pico Development Board by Shabaz - Workbench Wednesdays 70  

image

Photo of the earlier Rev 1.0 board:

image


What does it do?


This project only does a fraction more than the bare minimum that could be needed to develop projects. There aren't any fancy features on the board; there's nothing to get in the way of the large prototyping area! The image here shows what the board contains.

image



This is the solder side of the board:

image

Building It

The board can be ordered from any PCB manufacturer like JLC PCB or Elecrow. It cost about $10 for five boards, not including postage.


The schematic and bill of materials are on GitHub (the board can be hand-soldered within about 20 minutes I expect). Not all connectors need to be purchased or soldered, since it really depends on how you wish to prototype. I intend to use very thin 30 AWG single-core wire to patch connections, instead of using jumper wires. I may replace the two DIL pin headers that flank the Pico, with two SIL pin headers instead, so that I can solder wires into the empty holes for attaching circuitry, and use the SIL pin headers for testing purposes (for instance attaching a logic analyzer with jumper wires).


Alternatively, the card edge connector pins can be used for attaching test equipment, since all the Pico GPIO pins are exposed there too.

Note: This is the Rev 1.x schematic. Scroll further below for Rev 2.x schematics!

image


Summary


An ultra-simple development board for the Pi Pico was presented. If it proves useful, I might create a second revision of it at some point (edit: there is now a revision 1.1 board on Github). I have yet to build the first revision 1.0 board (I have ordered some boards, and will post photos of it all in a week or two time when the boards arrive).


One thing I would like to improve on is providing space for a heatsink for the 7805 regulator (edit: revision 1.1 now has sufficient space to suit some typical TO-220 heatsinks). If the 7805 gets too hot with the revision 1.0 board, it can be swapped with a pin-compatible DC-DC converter replacement, such as MP-K78L05-1000R3 (on Rev 2.x boards, use these DC-DC converters instead: 5V: R-78E5.0-0.5 and 3.3V: R-78E3.3-0.5 , they will fit properly on the board).


Technically the board violates the Eurocard specification, so another improvement would be to rearrange things so that the Pi Pico is rotated by 90 degrees and brought to the left side so that the board can be slid into Eurocard enclosures. I currently can't see myself using this basic development board in such an enclosure, so for now I took the simpler option of not considering it. I might need a 4-layer board design for a compliant Eurocard because the current cheaper 2-layer design uses the edges of the board to route supply traces, which is no good for metal sliding rails in enclosures. So, all-in-all, for now, I didn't feel too bad that it violates Eurocard, with the benefit that it's a cheaper design as a result.


Thanks for reading!

Notes

See the comments section for improvements made for the Rev 1.1 board (files are at the pico-eurocard GitHub link along with the revision history). In particular, the Rev 1.1 board supports I2C LCD displays, and/or SPI TFT screens, which the earlier Rev 1.0 didn't.

Update: Board Revision 2.x

There is now a new revision 2.x board series. The main differences are:

* No TFT screen header pins. Some TFT screens were subtly different, and I was running out of space, so unfortunately if a TFT screen is needed, it will need to be patched to the appropriate connections manually. Another workaround is to use an I2C character display, there are pins for that on the large 3 x 32-way connector on the right of the board

* Slightly reduced perfboard area

* 5V and 3.3V DC-DC converters are now used instead of the 7805 and heatsink. This saves space, and provides two power supplies instead of one.

* MicroSD card support

* Built-in Picoprobe

* Built-in rotary encoder

 

Rev 2.x Schematic

The 2.x board series has the following schematic (slight differences between 2.0, 2.1 and so on, but the component values and connections reflect all the dot-revisions, and anything significantly changed in any future dot-revision will be documented here). The component reference identifiers (such as J1, J2, and so on) have some differences compared to the silkscreen, but it is easy to identify which component is which. I reduced and simplified the silkscreen compared to the schematic, to get rid of the least-important bits of visual detail on the board.

image

image

image

Pin Assignments

The default pin assignments on the board are shown in the diagram. The assignments can be removed or reassigned for most pins, by using shorting jumpers or jumper cables.

image

This diagram from Jan contains more detail:

image

  • Sign in to reply

Top Comments

  • The_Nick
    The_Nick over 3 years ago in reply to shabaz +1
    Hi Shabaz, I just saw your project featured on Youtube. Just looked at your github repository and thought lets change someting using KiCad. I cannot find a schematic and project file in the zip…
  • Jan Cumps
    Jan Cumps over 3 years ago +1
    a little addition that I find useful: the proto area has the right size to add one of those small breadboards . They come with double-sided tape. You can just stick one on. The white ones cost less than…
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to shabaz

    I have not connected a probe to it to see the waveform

    I have probed it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to shabaz

    Many breakout boards don't have the resistors either. Carl (who wrote the code I'm using for testing - he has a lot of FatFS port creds) - indicates it's not a problem if you have 1 SD card. And confirmed by my test yesterday: it woks very well on the EuroCard.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to Jan Cumps

    Hi Jan,

    That's awesome, glad it worked! Although I had not tested it on the Pico-Eurocard board yet, I'd connected a (full-size) SD card to the Pico in an earlier project (Pico LoRaWAN board), and I had left a pull-up position as those notes mention, however it had worked (for the single SD card anyway) with no pull-up, so I omitted it (I figured if extra stuff is soldered to the same SPI bus, then an external resistor can be soldered at the same time). It's a bit of a luxury having two separate SPI buses on the Pico : ) 

    I didn't add the series resistor so that's a bit naughty (I had it on the LoRaWAN board, screenshot below) I can't recall the reason why I omitted it. Probably no reason, I may have just forgotten. I have not connected a probe to it to see the waveform, I can imagine it's not good, but I hope usable (perhaps with a bus speed decrease if necessary), it will be very awkward to add it as a bodge fix, since the traces are too close to each other near the micro SD card holder.

    EDIT: now I've remembered.. I had wired a microSD card socket manually to an older Pico-Eurocard board (which didn't have the footprint for it), with no resistor, and I had not seen an issue there, so just replicated what I did. With hindsight I still should have added that resistor though. 

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to Jan Cumps

    It works:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago

    I'm going to test the SD Card. According to calk3 , it's best to pull up the SPI lines:

    • The SPI MISO (DO on SD card, SPIx RX on Pico) is open collector (or tristate). It should be pulled up. The Pico internal gpio_pull_up is weak: around 56uA or 60kΩ. It's best to add an external pull up resistor of around 5kΩ to 3.3v. You might get away without one if you only run one SD card and don't push the SPI baud rate too high.
    • The SPI Slave Select (SS), or Chip Select (CS) line enables one SPI slave of possibly multiple slaves on the bus. This is what enables the tristate buffer for Data Out (DO), among other things. It's best to pull CS up so that it doesn't float before the Pico GPIO is initialized. It is imperative to pull it up for any devices on the bus that aren't initialized. For example, if you have two SD cards on one bus but the firmware is aware of only one card (see hw_config); you can't let the CS float on the unused one.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>