Browse By Tags

  • Develop for XIAO RP2040 with the Pi Pico Eurocard Development Board

    The Pi Pico Eurocard is a development board for the Raspberry Pico, designed by shabaz . In this post, I set it up to develop with a Seeed XIAO RP2040 . Functionality: Program and debug it with the (onboard) PicoProbe Reset connected to Eurocard…
  • 4 C projects for the Pi Pico Eurocard Development Board

    The Pi Pico Eurocard is a development board for the Raspberry Pico, designed by shabaz . In this post, I'm presenting four C projects that I've tested with the kit. Three of the examples are not mine. I adapted them (pin assignments), to work with the…
  • Pico Eurocard Rev 2.0 - Free (just pay shipping)

    EDIT : all gone, but it is easy to build your own, using the more recent (currently rev 2.2) files on GitHub. (Hoping it is OK to post this, since it's a not-for-profit thing!). Hi, I have three Pico Eurocard Rev 2.0 (it's a recent version, with…
  • Pi Pico Eurocard Development Board

    Introduction This is going to be an ultra-short blog post because the project is really short – it's a super-basic development board for the Pi Pico. I grew tired of having a Pi Pico dangling from the PC USB port with bits of wire hanging off it, just…
  • Stepper Motor Drive Moludes - PM Series

    For Bi-Polar Hybrid Motors These drive modules are designed for installation in standard 19" Euro-rack units. They are 3U high and have an ultra-slim 34mm (7E) width. Step and Half Step control Chopped constant current power stage for high performance…
  • Eurocard Connectors for computers by TE Connectivity (extended)

    .100 & .200 Centerline DIN 41612 Connectors (Eurocard) Product Line Information .100 & .200 Centerline DIN 41612 Connectors (Eurocard) Product Family Search | Product Feature Selector Eurocard Connectors Product Facts Meets DIN 41612 and IEC 603-2 Two…