Raspberry Pi
  • Products
  • More
Raspberry Pi
Blog Stepper Motor Control with Raspberry Pico PIO and DRV8711 driver- Part 5: a more autonomous PIO
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 6 Apr 2025 2:48 PM Date Created
  • Views 2716 views
  • Likes 6 likes
  • Comments 8 comments
Related
Recommended
  • raspberry
  • pico
  • pico_eurocard
  • PIO
  • stepper-motor

Stepper Motor Control with Raspberry Pico PIO and DRV8711 driver- Part 5: a more autonomous PIO

Jan Cumps
Jan Cumps
6 Apr 2025

The Pico has a set of PIO co-processors. They are real-time controllers that can execute logic with deterministic timing. Ideal to run strict-timed sequences and state machines. And to implement extra peripherals.
In this series, I'm trying to use the PIO to control a TI DRV8711 stepper motor controller.

image

Follow up of  Stepper Motor Control with Raspberry Pico PIO and DRV8711 driver- Part 4: PIO  .

The First 4 posts adapted Hackster project PIO Stepper Motor Control - an example that uses the Allegro A4988 stepper driver - to the DRV8711. It's a great example - almost the simplest PIO code you can find. It has limitations: it doesn't manage the DIR pin, and can do maximum 32 steps in a call.

In this new version, I deal with that. I wrote my own PIO program that can independently do up to 2147483647 steps. And the PIO handles the DIR pin. This means that you can really hand of a number of commands to the PIO FIFO input. And do something else in the meantime...

command structure

The data you send to the PIO is 32 bits.

  • bit 0: direction. The DIR pin will be driven to the value you set in this LSB
  • bit 31:1: steps. The PIO will send a pulse train to the STEP pin, with exactly the same pulses as requested

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

PIO code

.program stepper
.side_set 1
.define public DELAY 15
.wrap_target
start:
    pull block      side 0 ; Pull from FIFO to OSR
    out pins, 1     side 0 ; shift direction out of OSR and output to dir
    mov x, osr      side 0 ; Copy rest of OSR to scratch X
    jmp !x start    side 0
    jmp x-- count   side 0
count:
    ; nop             side 1 [DELAY] ; removed because we don't need a symmetrical pulse for a stepper
    jmp x-- count   side 0 [DELAY]
.wrap

What happens?

Preparation:

line 6 gets the data we passed in our main code (the command) into the output shift register. If no data provided, the state machine waits. It also keeps the step pin low.
on line 7, the DIR bit is shifted out of the shift register, sent to pin. This is the STEP pin of DRV8711. It still keeps the step pin low.
line 8 shifts the remaining 31 bits into scratch register x. This is our counter. It still keeps the step pin low.
line 9 aborts the run if we passed 0 steps. It still keeps the step pin low.
line 10 decreases the counter, and we move to the first pulse to generate. It still keeps the step pin low.

Then the loop:

line 12 finally sets the STEP pin high (rising edge of one pulse). It also delays until half the loop time, to keep frequency manageable
line 13 makes the process loop until the counter is exhausted. It also pulls the STEP pin down again (falling edge of that same pulse). It also delays for the remaining loop time, to keep frequency manageable
If the counter is exhausted, we created the requested amount of pulses, and we go back to line 10.

The delay that I use is the maximum I can get. Each instruction has 5 bits that are shared between delay and side step. Because I use 1 side step pin, I get 4 bits for delay. And that results in a maximum delay of 15.

PIO C helper

This is the setup code that's traditionally kept in the same .pio file. It sets up pins and configures which ones are driven as output, and which one as side step.

% c-sdk {
#include "hardware/clocks.h"
static inline void stepper_program_init(PIO pio, uint sm, uint offset, uint pin, float freq) {
   pio_gpio_init(pio, pin);
   pio_gpio_init(pio, pin+1);
   
   sm_config_set_out_pins(&c, pin, 2);
   pio_sm_set_consecutive_pindirs(pio, sm, pin, 2, true);
   pio_sm_config c = stepper_program_get_default_config(offset);
   sm_config_set_sideset_pins(&c, pin+1);

   float div = clock_get_hz(clk_sys) / (32*freq);
   sm_config_set_clkdiv(&c, div);

   pio_sm_init(pio, sm, offset, &c);
}
%}

The build process will generate a header file based on this info. This command in CMakeFiles.txt does that:

pico_generate_pio_header(${CMAKE_PROJECT_NAME}
    ${CMAKE_CURRENT_SOURCE_DIR}/source/stepper.pio
)

The main program

First a few helper functions:

void init_pio() {
    // todo get free sm
    uint offset = pio_add_program(piostep, &stepper_program);
    printf("Loaded program at %d\n", offset);

    stepper_program_init(piostep, sm, offset, dir, frequency);
    pio_sm_set_enabled(piostep, sm, true);
}

void init_everything() {
    stdio_init_all();
    init_drv8711_gpio_hw();
    init_drv8711_spi_hw();
    init_drv8711_settings();
    init_pio();
}

inline uint32_t step_time(uint32_t steps) {
    return (steps > (UINT32_MAX >> 1)) ? 0 : steps * 1000 / frequency;
}

// Write `steps` to TX FIFO. State machine will copy this into X.
// max steps taken is 2147483647 (highest number that fits in 31 bits)
void pio_stepper_set_steps(PIO pio, uint sm, uint32_t steps, bool reverse) {
    if (steps > (UINT32_MAX >> 1)) {
        printf("%d is more than max steps (%d)\n", steps, UINT32_MAX >> 1);
        return;
    }
    pio_sm_put_blocking(pio, sm, steps << 1 | (reverse ? 0 : 1));
}

The two first ones are initialisation. Then a utility function that calculates how long it 'll take to make a number of steps.
The last function, pio_stepper_set_steps(), is the most interesting. That's the one that combines the number of steps and the direction bit.
If you pass a value that doesn'tt fit in 31 bits, the code does not pass the parameter to the PIO and prints a message.
If the step count is valid, it's shifted 1 bit to the left, and that bit then becomes the direction bit.

in main(), I  just loop and keep sending between 0 and 255 steps to the PIO.

int main() {
    init_everything();

    uint32_t steps = 0U;
    {
        wakeup_drv8711 w;
        while (true) {
            printf("Steps = %d\n", steps);
            pio_stepper_set_steps(piostep, sm, steps, true);
            steps = (steps + 1) % 256;
            sleep_ms(10);
            // break;
        }
    }

    return 0;
}

If you want to learn about line 6, where the DRV8711 sleep mode is managed, check this side blog:  embedded C++: manage a resource with a tiny* object .

With a little bit of extra code, you can create a program, feeding the PIO with commands.

struct command {
    uint32_t steps;
    bool reverse;
};

// ...
    std::array<command, 6> cmd{{{200, true}, {200, false},{200, false},{400, false},{250, true},{350, true}}};

    
    {
        wakeup_drv8711 w;
        for(auto c : cmd) {
            printf("Steps = %d\n", c.steps);
            pio_stepper_set_steps(piostep, sm, c.steps, c.reverse);
            // sleep the time it takes for the steps + 0.5 second
            // for demo purpose
            sleep_ms(step_time(c.steps) + 500); 
        }
        sleep_ms(500); // give enough time to complete the action
    }

Here's how this looks like on a scope. Blue is the direction pin.

image

The video near the start of this blog shows the same sequence, but I added a little pause between the steps for visibility.

Thank you for reading. Next post:  Stepper Motor Control with Raspberry Pico PIO and DRV8711 driver- Part 6: autonomous PIO with speed control 

GitHub drv8711 project repository.
GitHub PIO stepper lib repository.
Here's the project  code: pio_drv8711_stepper_20250406.zip

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 1 year ago +1
    A test to see if the PIO actually generates the amount of steps that I request. In this case: 350. I've used my oscilloscope's pulse counter to do the work for me. It's a match.
  • Jan Cumps
    Jan Cumps over 1 year ago

    The PIO program that I wrote works, but it violates a requirement from the stepper motor driver I use, a TI DRV8711

    image

    There should be a 200 ns time between setting the DIR pin, and taking a step. My code violated that blatantly. It had 4 PIO clock ticks between the two events.

    I don't have a perfect solution yet, that works for all PIO clock speeds. Wat I've done now is configure the highest speed that works for my project.
    Then stretch the clocks used to set the DIR pin:

    .define public DIR_DELAY 4
    # ...
    out pins, 1 side 0 [DIR_DELAY] ; shift direction out of OSR and output to dir. 200 ns before next step

    The [DIR_DELAY] stretches the clock ticks used by the out command from one tick to 5. (the command, and 4 delay ticks)
    It's not perfect. For slower PIO clock speeds (something you set, there will be a (nanosecond order of magnitude) delay. But I bet that you won't notice it.
    This is the scope capture of the time between the events, with the adapted code:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago

    Time taken by the ARM core to load an instruction into the PIO FIFO. I used a GPIO to measure the time, so you 'd have to discount two gpio_put() calls from the 360 ns it takes to pass the instruction from ARM to PIO.

    image

    An instruction can have many steps (millions, if you need - anything that fits in 31 bits. For any process that needs a motor to step for milliseconds or seconds (or longer), this is definitely a resource gain. (although you can't put the Pico to sleep during that time, because then the PIO would stop too)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago

    In this video, a LED shows how much time it takes to send 6 instructions to PIO. In total 1600 steps, including direction changes in between.
    The motor is fast too Slight smile - but that is because I uptimised its speed and torque. Even if each of these 6 instructions would generate 100.000s of steps, the setup time in the ARM controller would be the same.

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    In a classic design, the microcontroller would have to spend clock ticks controlling the motor. Ticks it can't spend on other activities.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 1 year ago in reply to Jan Cumps

    Nice work! I was wondering how it was going to be tested. That's very neat!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago

    Using an old school counter to validate the stepper motor firmware:

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    My oscilloscope can do that too, as long as I can fit the signal on a single screen. A counter doesn't have that limitation.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>