Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Blog Win a Raspberry Pi 5 from the element14 Community!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14phil
  • Date Created: 28 Sep 2023 6:24 AM Date Created
  • Views 25585 views
  • Likes 17 likes
  • Comments 251 comments
Related
Recommended
  • competition
  • raspberry pi 5
  • raspberry pi 5 giveaway
  • win a raspberry pi 5

Win a Raspberry Pi 5 from the element14 Community!

e14phil
e14phil
28 Sep 2023

image

Win a Raspberry Pi 5!

We have just announced the release of the amazing Raspberry Pi 5, with its 2.4GHz quad-core, 64-bit Arm Cortex-A76 CPU, VideoCore VII GPU, LPDDR4X-4267 SDRAM (4GB and 8GB SKUs available at launch), 2.4 GHz and 5.0 GHz 802.11ac Wi-Fi, and Bluetooth 5.0 / Bluetooth Low Energy (BLE).

This Competition is now Closed.

Congratulations JWx our team has selected you as the winner of our Raspberry Pi 5 Give away!
We hope to see your experiments with the PCI-E functionality.  
/products/raspberry-pi/b/blog/posts/win-a-raspberry-pi-5-from-element14-community?CommentId=0f1e6de3-ee46-457b-bc91-71acc33df059 

Check out our Raspberry Pi 5 announcement blog here:

 Introducing The New Raspberry Pi 5 - 3x Faster, 2.4GHz, VideoCore VII GPU, RTC, Gigabit Ethernet, 1GB, 2GB, 4GB, 8GB RAM  

If you would like to win a Raspberry Pi 5, all we want to know is ... "What would you build with a Raspberry Pi 5?"

How to Enter:

Comment on this blog below, answering the question: What ould you build with a Raspberry Pi 5? We will send our favorite commenter a Raspberry Pi 5.

End Date: 30th November 2023 at 23:59 

Click here for Terms & Conditions.

Note: When selecting winners, if we discover that your name and address details are not correct on your Community account profile, we will choose a different winner.

Make sure your profile information is correct and up to date.

  • Sign in to reply

Top Comments

  • misaz
    misaz over 3 years ago +4
    In last years I used most time used Raspberry Pi for some kind of long-term automation. For example, last few months two of my Raspberry Pies was running experiments (one Rpi 4B and one 3B+) to evaluate…
  • ItsZephyrOne
    ItsZephyrOne over 3 years ago +3
    I already have a Raspberry Pi Zero; I tried desktop on it, but Zero doesn't have processing power, which is why I need a Raspberry Pi 5.
  • draq357
    draq357 over 3 years ago +3
    I would probably set this up as a server to receive weather information, and display it on a smart mirror. It would get weather info from the home built station in my backyard.
  • tushgaurav
    tushgaurav over 3 years ago

    I have never tried a Raspberry pi and would make it as a home server.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cwindsor
    cwindsor over 3 years ago

    Lions, Tigers and bears oh my.... Looking to build a CanBus interface to Digital Dashboard. The dashboard would interface the a Holley Terminator Max

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Zakave
    Zakave over 3 years ago

    I am really excited for this. Now that the Raspberry PI shortage is over, I was just thinking about building a home lab cluster; and then the RBPI 5 was released! It is perfect, Dedicated POE connector and PCIE for M.2. Perfect!

    My first project will be attempting to setup a serverless offline cluster!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • misaz
    misaz over 3 years ago

    In last years I used most time used Raspberry Pi for some kind of long-term automation. For example, last few months two of my Raspberry Pies was running experiments (one Rpi 4B and one 3B+) to evaluate supercapacitors as part of Experimenting with Supercapacitors. One of test setup look like this:

    image

    Raspberry Pi runs in the box and checks how my mini solar powered temperature sensor behave and checks if it can run for whole day and night with tested supercapacitor. I described my sensor on Element14 community here:  Mini Solar Powered Wireless Temperature Sensor . Raspberry Pi in this test automation project controls

    • WS2812B led strip which behave like virtual sun for testing solar charging
    • ADC module which measures voltage on the supercapacitor used by my sensor node
    • Relay which connects or disconnects ADC from sensor to prevent parasitic discharging of supercapacitor when the program do not measure voltage by ADC
    • Temperature Sensor module for checking that temperature measured by sensor is correct and also protects form overheating by LEDs
    • Light sensor for checking that LEDs are working properly.
    • Radio gateway connected over USB which checks that sensor properly send encrypted packets.

    Most of this can be implemented using just microcontroller but Raspberry Pi allows running standalone and log lot of data to text files which are easily retrievalbe over network. Additionaly it can very easily handle USB devices in comparison with my microcontrollers, so SBC is more suitable for this kind of test automation, I think. At last, it is easier to develop program in Python than writing microcontroller firmware in C.

    I of course use raspberry Pi for much more projects and tests. For example, at this time, my another Raspberry Pi runs OpenWRT and act as Wi-Fi router for testing Schurter Smart Connector DT31 which I RoadTest this time. But it is not a simple basic Wi-Fi router. Instead it is configured to sniff whole Wi-Fi trafic and even more, it allows me to modify network for trying hacks against the device and see how it behave. I am looking forward to Raspberry Pi 5 because due to exposed PCIe bus it will allow to easily add another (wired or wireless) network interface card to the Raspberry Pi.

    At last I have running some purely software project on Raspberry Pi. My main home Rapsberry Pi for example runs web server (written in PHP) which allows me to send Wake on Lan packet to wake my main working computer remotely when I am not in home. Since Raspberry Pi is powerfull enough it runs VPN which make this application more secure.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • pendragonscode
    pendragonscode over 3 years ago

    Right now i would probably start a home lab integrating home automation and production style kind of builds. At the same time, I would also explore using it as a mobile router and maybe make it become part of a cyber deck that i can bring around.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>