• Products and Partners
    Products and Partners
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
Raspberry Pi
  • Products and Partners
  • More
Raspberry Pi
Blog
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Breathe New Life into that old Raspberry Pi 2

    e14 Contributor
    e14 Contributor
    My Raspberry Pi 2 was mostly disused, running a couple of Seti@Home threads.  It is out of date and the speed was always rather slow compared to the other machines in my home.  Some of it is because 1GB RAM is anemic in 2016 but some of it ...
    • 7 Nov 2016
  • Simulink Student Challenge is now live

    madhugovindarajan
    madhugovindarajan
    Are you a student? Here is how you can win up to 1000 USD -  1) Show off your cool projects in which you used Simulink by creating a video which explains how you used Simulink. 2) Visit this page and use the appropriate hashtag while uploading y...
    • 31 Oct 2016
  • New Keypad HAT for the Raspberry Pi - The CapHat

    thinkengineer
    thinkengineer
    Product development specialists, Think Engineer are set to launch a revolutionary new accessory for the Raspberry Pi hardware. CapHat is a new HAT for all versions of the Raspberry Pi, featuring  an easy to use capacitive keypad that gives creat...
    • 27 Oct 2016
  • Piface Digital with RPI2 & drive 16 lights

    chezdomotix
    chezdomotix
    Hello all,I'm working with an artist to build an animated sculpture with (originally 1 but now) 16 lights driven by RPI 2b because of a king of random algorithm.At first sight, as there was only 1 light, ans 2 input switch, I've bought a Piface Digit...
    • 26 Oct 2016
  • Fedora 25 on Raspberry Pi

    oksbwn
    oksbwn
    www.youtube.com/watch  Fedora /fᵻˈdɒr.ə/ (formerly Fedora Core) is an operating system based on the Linux kernel, developed by the community-supported Fedora Project and sponsored by Red Hat. Fedora contains software distributed under a fre...
    • 26 Oct 2016
  • Raspberry Pi 3 HTML Control Interface Part 3

    e14 Contributor
    e14 Contributor
    This part focusses on controlling the gpio pins of the Pi using a web based user interface. Ive kept everything as simple as possible and also kept the page layout simple too. Step 1 The webserver running on the Pi3 needs permission to acce...
    • 17 Oct 2016
  • Access Raspberry Pi on Smartphone

    oksbwn
    oksbwn
    Remotely accessing Raspberry Pi Graphical Interface using smart phone. For this I have used VNC. Virtual Network Computing (VNC) is a graphical desktop sharing system that uses the Remote Frame Buffer protocol (RFB) to remotely control another comput...
    • 15 Oct 2016
  • Raspberry Pi 3 HTML User Interface part. 2

    e14 Contributor
    e14 Contributor
    This post is a demonstration of controlling an i2c device connected to a raspberry pi from a remote device. How it works:  The Raspberry Pi sends a webpage to a remote device that contains a text field and a button, when the button is press...
    • 11 Oct 2016
  • Raspberry Pi 3 HTML User Interface part.1

    e14 Contributor
    e14 Contributor
    I've always loved the idea of being able to access popular single board computers and their hardware using a HTML browser. Nearly every gadget we own e.g. mobile phones, ipods, tablets, laptops etc.. all have web browser functionality so it stan...
    • 10 Oct 2016
  • Raspberry Pi Visual Theremin

    madhugovindarajan
    madhugovindarajan
    A theremin is an electronic musical instrument that can be played without physical contact. The Raspberry Pi utilizes basic image processing algorithms to generate various tones through its on board audio jack. Check out the video here -  www.yo...
    • 7 Oct 2016
  • Connecting ESP8266 with Raspberry PI | AT Commands

    oksbwn
    oksbwn
                                 Connecting the ESP8266  Wi-Fi module to Raspberry Pi.The ESP8266 is a low-co...
    • 7 Oct 2016
  • Raspberry Pi with Google in MadebyGoogle talk

    cstanton
    cstanton
    Edit: Since writing this item, Linux Kernel 4.8 has official support for the BCM2837 chip on the Raspberry Pi 3 (and now v1.2 of the Pi 2), and the Android kernel also has support for the chip, which has prompted a community build of Nougat for the P...
    • 4 Oct 2016
  • Raspbian Jessie with PIXEL First Look | Raspbian SEP-2016 Release

    oksbwn
    oksbwn
    www.youtube.com/watch Raspbian is a free operating system based on Debian optimized for the Raspberry Pi hardware. An operating system is the set of basic programs and utilities that make your Raspberry Pi run. However, Raspbian provides more th...
    • 1 Oct 2016
  • Use Facebook as a Raspberry Pi terminal

    rados-dp
    rados-dp
    OVERVIEWIn this article we'll show how to control your Raspberry Pi terminal from Facebook. Below is a block diagram illustrating how we set up a web application running on a Raspberry Pi, made available to a Facebook application webhook via dat...
    • 20 Sep 2016
  • Ubuntu Mate Installation for Raspberry Pi 2 and 3

    e14 Contributor
    e14 Contributor
    I found this distribution to be the simplest to install, localize, and set-up networking for (wired or WiFi, static IP or DHCP).  I was impressed enough that it is on all of my computers:RPi2 (ARMv7) SoCPine64+/2GB (64-bit ARMv8, like RPi3) SoCB...
    • 18 Sep 2016
  • Read Analog Signals with Raspberry Pi using MCP3208 and JAVA

    oksbwn
    oksbwn
    www.youtube.com/watch This video is all about connecting MCP3208 with Raspberry Pi and accessing it using JAVA.---------------------------------------------------------------------- Repository : https://goo.gl/7NRe5n Schematic : https://goo.gl/k...
    • 15 Sep 2016
  • Ten of the Best: Raspberry Pi Member Projects

    jlucas
    jlucas
     This week, the Raspberry Pi foundation celebrates another milestone with the announcement that they have sold over 10 million Raspberry Pi's around the world. As a leading distributor and manufacturer of the boards, Premier Farnell has man...
    • 9 Sep 2016
  • Sense HAT in Pi IoT

    jwatson
    jwatson
    • 6 Sep 2016
  • Meet the winners of MATLAB and Simulink Hardware Challenge (shared from Arduino's blog)

    madhugovindarajan
    madhugovindarajan
    MathWorks recently ran a hardware challenge, where in users were asked to submit a project in which they programmed hardware boards using MATLAB or Simulink. The grand prize for this challenge was 1000 USD and we received over 60 submissions for this...
    • 31 Aug 2016
  • SQLite | Interact using JAVA | Raspberry Pi

    oksbwn
    oksbwn
    www.youtube.com/watchThis tutorial is an overview of interacting with SQLite database using JDBC connector running on Raspberry Pi. It's not about learning SQlite. I have tried to show briefly how it can be done.--------------------------------------...
    • 27 Aug 2016
  • Do-It-Yourself Certificate Authority on a Raspberry Pi

    e14 Contributor
    e14 Contributor
    On github, I created a Do-It-Yourself Certificate Authority project (https://github.com/texadactyl/diyca), suitable for unit testing (developer testing) just prior to entering integration system testing with a wider audience: more developers, testing...
    • 26 Aug 2016
  • Stream live videos from your Pi

    rados-dp
    rados-dp
    OVERVIEWIn this article we'll show how to stream live videos from your Pi to a web browser. The technology that we've used to achieve that is an MJPG-streamer application and a Raspberry Pi camera. Below is a preview of the end result.PRE-REQUISITESY...
    • 26 Aug 2016
  • Control Raspberry Pi GPIOs with WebSockets

    rados-dp
    rados-dp
    OverviewThere are four components in this system:Breadboard with LEDs attached to GPIO on a Raspberry PiWeb application on Raspberry PiWebsockets server application on Raspberry PiInternet browser This example uses both HTTP and WebSockets where:HTTP...
    • 16 Aug 2016
  • Simple din rail housing for Pi zero

    hwhardsoft
    hwhardsoft
    Hi, I want to introduce a new enclosure project for the Pi Zero. It's a new din rail housing and protoboard with integrated voltage regulator. Project home page www.youtube.com/watch 
    • 6 Aug 2016
  • raspberry pi project:dog house monitor

    e14 Contributor
    e14 Contributor
    when you leave your house you want to see what your pet is doing, right? My first thought is to buy a home safety camera like a nest camera of a pet cube,but those can be extremely expensive so I will build it with a raspberry pi. list of needs:...
    • 22 Jul 2016
<>