• Products and Partners
    Products and Partners
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
Raspberry Pi
  • Products and Partners
  • More
Raspberry Pi
Blog
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Another day and another design. RPi meets PSOC: What do you think?

    ipv1
    ipv1
    A few months back, I enrolled for a design contest at hackster.io . Needless to say its one of those contest where hundreds(500) of people join but every few complete. Anyway I did my part and here are a few tit-bits I gathered. The implementati...
    • 22 Feb 2017
  • How to assemble and get started using BitScope Blade.

    bitscope
    bitscope
    This is the first in a series we'll post about using BitScope Blade and the obvious place to start is unboxing and assembling it. Blade is a robust industrial deployment solution for Raspberry Pi. How you assemble it and the ways you can power and mo...
    • 21 Feb 2017
  • Heatwave no problem for BitScope Blade and Raspberry Pi !

    bitscope
    bitscope
    Not even a near record breaking heatwave can stop BitScope Blade hosted Raspberry Pi servers as we discovered by accident when our trusty old Dells came to an ignominious end but the 32 BitScope Blade Raspberry Pi in the same overheating room survive...
    • 10 Feb 2017
  • Raspberry Pi Applications built with BitScope Blade.

    bitscope
    bitscope
    Following the recent launch of BitScope Blade and the case studies about the weather station in Nepal and the interactive Theremin exhibit at MAAS we received a lot of questions about which Blade is best for what purpose. Read on to learn why Blade c...
    • 7 Feb 2017
  • Universal Display Shield for Arduino and Raspberry Pi

    hwhardsoft
    hwhardsoft
    Hi, I want to introduce a new small project of me. It's a OLED display shield for Arduino and Raspberry Pi. The shield includes 3 buttons and leds to realize simple menues etc. The communication with the Arduino or RPi works via I2c. You wil...
    • 3 Feb 2017
  • An Interactive Museum Installation built with BitScope and Blade Uno.

    bitscope
    bitscope
    Following our post about the Blade weather station in Nepal, this one describes an interactive exhibit created with BitScope Blade UnoBitScope Blade Uno, BitScope CAP and a Raspberry Pi 3Raspberry Pi 3. The BitScope Blade was used to conveniently pow...
    • 1 Feb 2017
  • 16x2 LCD interfacing with Raspberry Pi using I2C/Pi4J/JAVA

    oksbwn
    oksbwn
    www.youtube.com/watch  Interfacing 16x2 LCD by using  MCp23017 16 Bit input/output Port Expander IC with Raspberry Pi by using I2C Interface. To interact with the IC here we have used Pi4J and JAVA.  MCP23017 Features:  ...
    • 31 Jan 2017
  • BitScope Blade Uno Raspberry Pi Weather Station Project in Nepal

    bitscope
    bitscope
    We launched the new BitScope Blade product range exclusively with element14 last week. To help explain how BitScope Blade works and what you can use it for, we'll be publishing a series of posts, of which this is the first, describing some example ap...
    • 30 Jan 2017
  • I2C Communication on Raspberry Pi using JAVA

    oksbwn
    oksbwn
    www.youtube.com/watch Connecting MCp23017 16 Bit input/output Port Expander IC with Raspberry Pi by using I2C Interface. To interact with the IC here we have used Pi4J and JAVA. MCP23017 Features:   16-bit input/output port expander wi...
    • 27 Jan 2017
  • My homemade beowulf cluster underway

    nschreiber0813
    nschreiber0813
    Dear: Element 14 Community I am letting you guys know I am building a raspberry pi cluster based off of a laser cut frame I designed and cut on a laser cutter and designed with librecad. Let me just explain first of all my experiences as an...
    • 26 Jan 2017
  • Raspberry SUPER Pi - Turning the Pi into a games console

    cstanton
    cstanton
    This's a pretty clever design, and I thought to myself "it wouldn't take much to make these into actual cartridges, if the Pi Compute was used as an edge connector". Still, the images speak for themselves, and the creator used ...
    • 26 Jan 2017
  • Raspberry Pi Sense Hat - Enabling The Joystick

    e14 Contributor
    e14 Contributor
    Having had some fun playing with the display on the Sense Hat I moved on to trying to utilise the Joystick. However copying the examples set out in the Sense Hat API results in the following error AttributeError: 'SenseHat' object has no...
    • 23 Jan 2017
  • Show messages on 16x2 LCD | Pi4J | JAVA | Raspberry Pi

    oksbwn
    oksbwn
    www.youtube.com/watch Showing messages on 16X2 LCD display by interfacing with Raspberry Pi using JAVA and Pi4J library.Intro visual Source: http://pi4j.com-----------------------------------------------------------------------------------------...
    • 23 Jan 2017
  • Raspberry Pi 3 Block Diagram

    shabaz
    shabaz
    This is just a High Level Diagram approximation of what the Pi 3 consists of.It is based on various bits of information on the Internet, and could be incorrect in places.If you have any corrections, or additional bits of information/suggested tweaks,...
    • 16 Jan 2017
  • Your Thoughts on the Raspberry Pi Compute Module 3

    spannerspencer
    spannerspencer
    So, I don't know if you've seen, but there's a brand new Raspberry Pi Compute module launching today! As you guys know, having been around the Raspberry Pi block quite a few times, the Compute module isn't really aimed at the mak...
    • 16 Jan 2017
  • Raspberry Pi OS on old PCs

    Catwell
    Catwell
    (LEFT) Boot Screen of Rasbian for PC operating sytems. (RIGHT) This is Raspbian running on a PC. (via Raspberrypi.org) The Raspberry Pi Foundation has created a version of the Raspbian OS for MAC and x86(Windows) personal computers. Raspbian is...
    • 4 Jan 2017
  • New Raspbian version "Pixel"

    balearicdynamics
    balearicdynamics
    I decided to write this post due a silly trap that to be honest I think should be avoided in next updated of the raspbian pixel version. The last official downloadable version at the date is the 2016-11-25-raspbian-jessie.img Here and there ther...
    • 4 Jan 2017
  • Lungs Compliance Meter Raspberry Pi Project

    _vishaladitya
    _vishaladitya
    A simple automated device to demonstrate the measure of volume/pressure change in lungs using compliance curve.www.youtube.com/watchIt is working model for teaching Dynamic Airway Compression. The concept of lung compliance is generally considered to...
    • 29 Dec 2016
  • Raspberry Pi Robot- ADDY: A Hybrid Robot with humanoid and autonomous features

    _vishaladitya
    _vishaladitya
    www.youtube.com/watchI started my robotics project with its name ADDY it’s a hybrid robot, combination of autonomous and humanoid features.ADDY is capable of doing small to complex tasks: -•          ...
    • 29 Dec 2016
  • EEG Game Simulator using BCI and RaspberryPi

    _vishaladitya
    _vishaladitya
     The objective of this project is to enhance gaming experience at cheap costs and the primary focus is to develop an open source dedicated device that can sense alpha/beta brain waves possibly and further the data can be utilized to simulate win...
    • 29 Dec 2016
  • H.O.D.O.R | Home/Office Automation | Raspberry Pi Project | Wireless Smartphone Control

    _vishaladitya
    _vishaladitya
      H.O.D.O.R is a Home/Office Automation project using Raspberry Pi single-board computer. The name H.O.D.O.R has been taken into consideration after us being the die hard fans of Game of Thrones. The name H.O.D.O.R is taken from that famous...
    • 29 Dec 2016
  • Hand Gesture Game Simulator

    _vishaladitya
    _vishaladitya
    A simple automation project with Raspberry Pi using ADXL345 accelerometer to simulate better gaming experience. Supports All Windows Games, currently functioning over Ethernet & WiFi. Best experience with Racing games! www.youtube.com/watchV...
    • 29 Dec 2016
  • Upcoming webinar using Raspberry Pi in an internet of things project

    madhugovindarajan
    madhugovindarajan
    Here is a link to the webinar - Cloud-based traffic analyzer using the Raspberry Pi and Simulink by MathWorks  This webinar will show you how Simulink was used to deploy a car counter algorithm to a Raspberry Pi. The Pi sends the traffic data to...
    • 6 Dec 2016
  • How To Identify Which Model Of The Raspberry Pi You Have

    CharlesGantt
    CharlesGantt
     When the first Raspberry Pi was released in February 2012 it revolutionized the way makers around the world made things, and it completely changed the landscape of the development board world, and continues to do so even today. As of November 2...
    • 21 Nov 2016
  • Building a Thermal Imaging System with the Raspberry Pi 3, Sense HAT and Panasonic Grid-EYE

    shabaz
    shabaz
    IntroductionSometimes it is great to be able to see if things are hot or cold with a thermometer or other device. Multiply it by 64 and it is possible to get a graphical image of hot spots or detect humans for instance.A thermopile array can be used ...
    • 9 Nov 2016
<>