Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Seneca breaks silence on Fedora Remix
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 84 replies
  • Subscribers 709 subscribers
  • Views 10108 views
  • Users 0 members are here
  • raspberry
  • help
  • helpme
  • raspberry_pi
  • raspberrypi
Related

Seneca breaks silence on Fedora Remix

e14 Contributor
e14 Contributor over 14 years ago

After a puzzling two months of silence from Seneca with regard to

plans for fixing the withdrawn Fedora Remix, there is a blog post

indicating that work is starting with the beginning of summer,

including fixing the problem with attempting to change the timezone.

 

http://roottothehead.blogspot.com/2012/05/summer-at-seneca.html

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Chris Tyler posted an update today.

    Estimated release date is 20th, but lots of work to do.

     

    http://lists.fedoraproject.org/pipermail/arm/2012-July/003631.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    That's a very interesting read.

    Lots of problems that appear directly related to trying to force options suited to todays desktops onto the comparatively resource light Pi.

    You have to wonder what PCI devices they expect to see on the Pi.

     

    Wanting to enable SELinux seems particularly strange. If there's any educational goal left, surely we want to get kids interested and hooked on doing stuff before we teach them to hate SELinux ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 14 years ago in reply to e14 Contributor

    From what I read here he actually says

     

    1) I want it to actually scan for the PCI devices ...yes the RPi doesn't have a PCI expansion  but it's quite possible for a
    SOC or any other part to have an internal PCI bus that the peripherals are attached to and also not all may be enabled since that GPU device does some configuring before hand so you can't just guess the config.

     

    2) X performance is poor......Yes it is!.... better than it was at day 0 though! ....I think theat X is very useful since most people don't want tto be thrown into a command line these days if they don't have UNIX experience

     

    3) Re SELinux he's actually saying the SELINUX configuration is TOO memory expensive not that he wants to put it in regardless just that the memory burn is a total PITA.

     

    BTW I saw some where that some bunch had got a generic openGL implementation going using the GPU how do we get this back to these guys rather than moaning !!!

     

    Thanks for the Update BTW Coder27

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to Problemchild

    I see that needing a different SD card for each different image is going to be a major pain in the backside.  Pi really needs a network image boot, so that we can store umpteen different images externally and the SD card can remain fixed --- let the VideoCore boot just a network-aware bootstrap, not a Linux kernel.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 14 years ago in reply to morgaine

    AMEN !!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 14 years ago in reply to jamodio

    I'm wondering if a  network aware minikernel would be good for this then ?!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to jamodio

    If they really want the Pi to get into schools then network boot is pretty much mandatory.  The horrors of administering classroms full of devices each with local storage don't bear thinking about.  You have to have central administration or teachers will be jumping off bridges.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to Problemchild

    1) I want it to actually scan for the PCI devices ...yes the RPi doesn't have a PCI expansion

    ok, so why bother ?

    but it's quite possible for a
    SOC or any other part to have an internal PCI bus that the peripherals are attached to and also not all may be enabled since that GPU device does some configuring before hand so you can't just guess the config.

    Certainly true that it's possible, however ARM devices tend to use AMBA for anything on the SoC. We know the RPi uses AMBA and that it doesn't have PCI, so why waste space on any PCI options ?

     

    He says "I don't want to turn off SELinux", then implies that he will because it's too memory expensive. Not sure how to read that any other way, not wanting to turn it off seems to me a strong hint that you want to turn it on.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to Problemchild

    1) I want it to actually scan for the PCI devices ...yes the RPi doesn't have a PCI expansion

    ok, so why bother ?

    but it's quite possible for a
    SOC or any other part to have an internal PCI bus that the peripherals are attached to and also not all may be enabled since that GPU device does some configuring before hand so you can't just guess the config.

    Certainly true that it's possible, however ARM devices tend to use AMBA for anything on the SoC. We know the RPi uses AMBA and that it doesn't have PCI, so why waste space on any PCI options ?

     

    He says "I don't want to turn off SELinux", then implies that he will because it's too memory expensive. Not sure how to read that any other way, not wanting to turn it off seems to me a strong hint that you want to turn it on.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Problemchild
    Problemchild over 14 years ago in reply to e14 Contributor

    True but also you need to maintain as much of the distro consistancy as posible  unless you want to be the maintainer of 1000's of mods.

     

    "He says "I don't want to turn off SELinux", then implies that he will because it's too memory expensive. Not sure how to read that any other way, not wanting to turn it off seems to me a strong hint that you want to turn it on."

     

    Sounds more likely he wanted to me consistant with the Distro but he feels that the memory hit is TOO big and will leave it off to me quite the oposite.

     

    Personally it's better with it off anyway 'cos it has little relevance to a toy computer and not that much to a real one eitehr most of the time ...GRR bloody SELINUX

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to Problemchild

    .GRR bloody SELINUX

    image that's my feeling too. 

     

    I can understand wanting to be consistent with the distro, but for the educational goal I'd be wanting to remove the barriers to getting kids interested.

     

    OTOH, carrying all the mods is the whole purpose of the remix isn't it ?  If you didn't need the mods you could just use whatever the upstream project provided ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 14 years ago in reply to Problemchild

    "

    The kernel and firmware have been updated to the Raspi upstream. The

    config we're using is (raspi SOC options + usb devices - non-USB devices

    (PCI etc) "

     

     

    Reading it again I would say that the Reference to "PCI" was more of a general sweep of the hand statement for "insert non USB devices/buses  here" rather than PCI  specificaly and exclusively.

     

     

    Bored now!!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to Problemchild

    Dennis Gilmore of RedHat explains why the Fedora Remix isn't planning

    to take advantage of the RPi's floating-point hardware.  He says it's

    "not likely to be a long term sustainable port."

     

    http://lists.fedoraproject.org/pipermail/arm/2012-July/003669.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    Unfortunately Dennis' comment doesn't really make much sense, and "long term sustainable port" is pure market-speak. image

     

    Open source doesn't focus on market share nor on product life nor on some market-inspired concept of sustainability, but on community interest, and it requires a pretty low level of interest before someone makes an appropriate distribution to cater for it.  If both Pi and Via APC (and hacked Roku 2 as well in due course) would benefit from armhf, and that means hundreds of thousands or even millions of users, then hardhf will come.  It's sustainable if there is interest.

     

    What Dennis really means is that he doesn't want to support it himself, which is totally fair  -- it's his own hard work after all.  But someone else will do so in due course, you can bet on it.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    I think Dennis is probably referring to the technical obsolescence of

    the armv6 architecture, particularly for the education market and other

    desktop applications.  Either the RPi will get upgraded soon,

    or it will become irrelevant. So there isn't much point in making

    a major investment in armv6 support.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    I don't think Dennis meant that, since ARM9 is even more obsolete commercially than ARM11 and yet is still deemed worthy of FOSS support.  There is no concept of device obsolescence in that commercial sense in FOSS, everything is supported no matter how old if there is community interest.  And community interest in ARM11 is of course growing rather than shrinking because of the recent influx of cheap boards with ARM11 cores.  ARM is different to Intel in that respect, older cores are often used in embedded devices where leading edge computing is not the requirement.

     

    It was just a personal judgement by Dennis, which he should have phrased as "Maintaining that additional architecture doesn't scratch my personal itch so I won't", which is how FOSS works, and he's probably not getting paid to do more than just scratch his personal itch.  It doesn't go more deeply than that.  Either someone else will step in and maintain an ARMv6 hardfp distro for ARM11 because they personally feel it would be useful, or it won't get done.  How modern a core is doesn't come into it.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 14 years ago in reply to morgaine

    I agree with the itch scratching concept. Also if their emulation is good enough I'm sure that it doesn't form a problem in terms of numbers of bugs whic is the issue for them especially since they have plenty elsewhere!!!

     

    Does any one know the potential improvement in real terms of getting HardFP working ...Surely over the whole OS this isn't more than say 5%...probably not worth the hassle?!?!

     

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to Problemchild

    Morgaine wrote:

    >ARM9 is even more obsolete commercially than ARM11 and yet is still deemed worthy of FOSS support.

     

    but there is an important difference.   Fedora considers ARM9 worthy of continued maintenance, presumably

    because not much work is required.  They are also willing to provide continued maintenance for ARM11

    because it piggybacks on their ARM v5 distro without much additional work.  They draw the line at building

    out a whole distro specifically for ARM V6, which is very costly.  Not only does it require more build-farm

    resources than they have available, but the C compiler has never before been used in ARM 11 mode, which Dennis notes has unique floating-point support, so there are an unknown number of compiler bugs to fix

    or work around.

     

    >There is no concept of device obsolescence in that commercial sense in FOSS, everything is supported no matter how old if there is community interest.

     

    I think there is a cost/benefit ratio involved.  If an older device is difficult to maintain and there is insufficient

    community interest, it will get dropped.  GCC for example drops support for a number of architectures in

    every major release.  Ubuntu has already dropped support for ARM 11 and older.  Fedora may follow suit

    before too long.

     

    John writes:

    >Does any one know the potential improvement in real terms of getting HardFP working ...Surely over the whole OS this isn't more than say 5%...probably not worth the hassle?!?!

     

    See the RPF front-page story on switching to Raspbian because of the perceived (but not quantified) benefits.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Not only does it require more build-farm

    resources than they have available, but the C compiler has never before been used in ARM 11 mode, which Dennis notes has unique floating-point support, so there are an unknown number of compiler bugs to fix

    or work around.

    Not sure I buy that argument, Raspbian seem to be doing OK. 

    If they're simply not interested, for whatever reason, they should just say so and move on instead of inventing arguments.  If Raspbian didn't exist then the argument may hold more weight, but you can't use something like that when a one or two man outfit has already proved it can work.