Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum HDMI resolution problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 705 subscribers
  • Views 3510 views
  • Users 0 members are here
  • hdmi
  • raspberry_pi
Related

HDMI resolution problem

e14 Contributor
e14 Contributor over 14 years ago

Hi, I've just taken delivery of my Raspberry Pi. I loaded up Debian, hooked it up to my TV via the HDMI connection but the edge of the screen overlaps the screen size. I cannot see the task bar or menu buttons. How can I fix this?

Thanks

  • Sign in to reply
  • Cancel
  • wallarug
    wallarug over 14 years ago

    Refer to my posts on Element14 Forums: http://www.element14.com/community/thread/18205?tstart=0

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago

    Have you tried the help wiki?

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=5&t=5851

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago

    Instuctions for others who may be experiencing the same issue with a TV and the Raspberry Pi:

    1. Install a fresh image

    2. start-up the Raspberry Pi and let it set itself up (normal set-up)

    3. After you have gone through normal set-up:

    a. Log-in as a normal user (debian image: pi)

    b. Type the command: "sudo nano /boot/config.txt "

    c. Press enter

    d. Type in: "hdmi_drive=2 " [exactly as it is here]

    e. Then press crtl + o

    f. Press Enter

    g. then press crtl + x

    4. Restart using the command: " sudo shutdown -r now "

     

    That gets the Raspberry Pi to register the TV as a HDMI device. You now have sound! For different resolution:

    5. After you have gone through normal set-up:

    a. Log-in as a normal user (debian image: pi)

    b. Type the command: "sudo nano /boot/config.txt "

    c. Press enter

    d. Type in: "hdmi_group=1 " [exactly as it is here]

    Press Enter

    Type : "hdmi_mode=x " where x = corresponding number of resolution mode. See: http://www.raspberrypi.org/phpBB3/viewtopic.php?f=26&t=5851

    e. Then press crtl + o

    f. Press Enter

    g. then press crtl + x

    6. Restart using the command: " sudo shutdown -r now "

     

    Now you have desired resolution and Sound!!!

     

    Happy Raspberry Pi...ing

     

    I hope this solves your problems

     

    Fergus

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to wallarug

    Hi Fergus

    Thanks for posting on how to set up the hdmi screen. It worked first time for this (very) old man. Now I can see text on the screen, it was to small before your post!

    Best regards

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to wallarug

    Hi,

     

    I've just tried this. I set hdmi_group=1 and hdmi_mode=19 but that had no effect. I then tried hdmi_goup=2 and hdmi_mode=0x8 but that killed it and I had to start again with a new image.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Maybe I could change the settings on the TV but there are no options that I can find to do so. Does anyone know anything about Panasonic Viera's?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    I ran into the same problem. Changed to 4:3 on the picture size using the TV remote. It was like magic . . .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    Kev,

     

    Also: Can you tell us if your TV is registred as a DVI device or HDMI device?  If yes, then follow the instuctions I posted above.  If no, then you might not be putting in the right commands or putting them in wrong.  All commands DO NOT have spaces.

     

    Then:

     

    You have to check whether or not your TV supports that resoultion.

     

    See this link on how to do that:

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=5&t=5851

    1. Run “tvservice –m CEA” to give a list of CEA supported modes.

     

    To do this, you must first change your directory to: /opt/vc/bin  (to do this enter command in terminal: "cd /opt/vc/bin")

    then type: "tvservice –m CEA" (or ./tvservice –m CEA if it doesn't work)

    then the Raspberry Pi will show a list of supported formats.  Use http://www.raspberrypi.org/phpBB3/viewtopic.php?f=5&t=5851 to get the commands of the supported format. Once you find the supported formats,

     

     

     

    Fergus

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to wallarug

    Thanks for the reply Fergus. I followed your instructions and found that mode 19 is supported (at least I think it is, the left of the screen is not visible so all I can see is:

     

              mode 1: 640x480 @60Hz, progressive

              mode 2: 720x480 @60Hz, progressive

              mode 3: 640x480 @60Hz, progressive

    ative)  mode 4: 1280x720 @60Hz, progressive

              mode 5: 1920x1080 @60Hz, progressive

              mode 6: 720x480 @60Hz, progressive

              mode 7: 720x480 @60Hz, progressive

              mode 17: 720x576 @50Hz, progressive

              mode 18: 720x576 @50Hz, progressive

    ative)  mode 19: 1280x720 @50Hz, progressive

              mode 20: 1920x1080 @60Hz, progressive

              mode 21: 720x576 @50Hz, progressive

              mode 22: 720x576 @50Hz, progressive

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks Peg, but when I do that the image is still cropped

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>