Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Rugged RPi Camera case
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 33 replies
  • Subscribers 710 subscribers
  • Views 6350 views
  • Users 0 members are here
  • raspberry
  • rpi_camera
  • raspi
  • pi
  • demolition
  • raspberry_pi
  • raspberrypi
  • rpi
  • camera
Related

Rugged RPi Camera case

e14 Contributor
e14 Contributor over 13 years ago

I've been working on a mount and a fairly rugged case for my RPi camera recently, some photos here

https://picasaweb.google.com/selsinork/RPiCamera

 

The end goal being to do some timelapse and video where the camera would need to be outside in a rather hostile environment

 

This was the result from earlier today

 

the little camera did well image

 

Edit: does the embedded video work ?  I don't see it, so here's the link http://www.dailymotion.com/video/x1255yy_sandiefield-road-demolition_webcam

  • Sign in to reply
  • Cancel
Parents
  • morgaine
    morgaine over 13 years ago

    Wow, what a test subject!

     

    I too had to use the dailymotion link, as the embedding here doesn't work for me either.

     

    Was it deliberately shot with the camera on its side?  I watched it with the sky on the left of the frame.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Was it deliberately shot with the camera on its side?  I watched it with the sky on the left of the frame.

    Yep, distance vs the field of view of the standard lens meant it was the only way.  That's widescreen for you too, I'd probably have got about a third of the block being demolished and most of an empty street the other way.  It's also a bit odd.. take a 1920x1080 still image with it and the field of view is different from 1920x1080 video

     

    When I was building the case I gave myself the option to mount the camera either horizontally or vertically anyway, so not a huge problem for other uses

     

    No surprise though that when you look in the camera section of the RPF forum there's lots of people with creative mods to get different / better lenses.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to e14 Contributor

    Selsinork

     

    Great video.

    The building looks better than half the ones they knocked down in Christchurch, inc a few that they are removing because they don't fit the current plan.

     

    I like your case and mounting, as my project is to shove it up on the skifield, which obviously has all sorts of unpleasant weather,

    Luckily its mainly stills we want to send back over wireless.

     

    I do need to add a controller to control the solar and start it up and shut it down at the end of the day.

     

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    http://gizmodo.com/5915888/an-important-psa-on-why-you-should-never-shoot-videos-vertically

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to e14 Contributor

    I thought the trashy mirror photo article was good.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mcb1
    mcb1 over 13 years ago in reply to e14 Contributor

    I thought the trashy mirror photo article was good.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to mcb1

    Reminds me of these:

    http://www.element14.com/community/blogs/pdp7/2013/05/31/boring-commute-my-favorite-engineering-open-source-podcasts

    http://www.element14.com/community/blogs/pdp7/2013/05/24/my-t-shirt-for-this-tgif-spacewar

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to e14 Contributor

    thankfully he doesn't have the same cleavage.

     

    Because they are a photo, he's allowed the portrait mode.....

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 13 years ago in reply to e14 Contributor

    Mine are much less trashy as I'm holding Linux

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to fustini

    Drew

    So we replace the white low cut TShirt with one that features Linux ...?

     

    Selsinork

    It was suggested to me that a standard outdoor floodlamp makes an ideal rugged holder.

    image

    Nice thin glass on the front, a bracket arrangement to mount it, inc adjustment, and fully waterproof to boot.

    They come in at least three sizes (150w, 500w and 1000w), with the 150 and 500w being throw away cheap.

     

    You'll need to mount the camera, Pi and anything else, as the front glass folds down.

     

    I'm in two minds for my project due to the cold soak of the metal, which generally attracts more ice than anything else.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to mcb1

    Would getting one with a PIR be usefull as you coud use the relay/ Scr drive the PIR uses to switch the lighting on the cheap  or even use the PIR as an additional sensor into the PI.

     

    Only other thing I can think of is that the heat from the Halogen may cook the PI even behind the reflector

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to Problemchild

    Thinking about it I'm not sure most  lights are as sealed as they could be they often have spiders and all sorts making home in there .. might be best to house the PI inside an inner case or at least keep it stood off the outer shell of the lamp.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to Problemchild

    Is that an Otter box or some such?

    It appears to have a nice gasket seal on the rim!

     

    Also did you drill into the case for the camera or merely stick the whole board on the back with out recessing the lens I'm sure you really wouldnt want to compromise the seal unless you needed to image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to Problemchild

    I'm busy trying out some waterproofing solutions for My PI and Cam if this gives waterproofing to a meter or two then this would be great here's the kind of thing I was trying to get more of.

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to Problemchild

    John Alexander wrote:

     

    Is that an Otter box or some such?

    It's made by Bernstein  10163561016356  and is IP65, so won't do for submersion. I also got 13253981325398 which is IP67 and I believe that gets you down to 1m

     

    Also did you drill into the case for the camera or merely stick the whole board on the back with out recessing the lens I'm sure you really wouldnt want to compromise the seal unless you needed to image

    The only hole I put in the case is the one at the bottom for the cable gland. The camera is mounted on some bits of ABS offcuts that are bonded to the inside of the lid with epoxy. The mounting holes on the back are provided for you and are outside the seal.

    It's just a standard Skintop cable gland I'm using, no idea if it'd handle submersion, but I suppose you could seal it up with epoxy to be sure.

     

    I think I'd probably just put the cable in and then submerge it for a while without the Pi or camera to see if it leaked image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to mcb1

    Mark Beckett wrote:

     

    It was suggested to me that a standard outdoor floodlamp makes an ideal rugged holder.

    That's an interesting thought, although I suspect mounting stuff inside one of those could be a bit more challenging.  I may try it next time though..