Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Rugged RPi Camera case
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 33 replies
  • Subscribers 710 subscribers
  • Views 6349 views
  • Users 0 members are here
  • raspberry
  • rpi_camera
  • raspi
  • pi
  • demolition
  • raspberry_pi
  • raspberrypi
  • rpi
  • camera
Related

Rugged RPi Camera case

e14 Contributor
e14 Contributor over 13 years ago

I've been working on a mount and a fairly rugged case for my RPi camera recently, some photos here

https://picasaweb.google.com/selsinork/RPiCamera

 

The end goal being to do some timelapse and video where the camera would need to be outside in a rather hostile environment

 

This was the result from earlier today

 

the little camera did well image

 

Edit: does the embedded video work ?  I don't see it, so here's the link http://www.dailymotion.com/video/x1255yy_sandiefield-road-demolition_webcam

  • Sign in to reply
  • Cancel
  • shabaz
    shabaz over 13 years ago

    Amazing video. I can see why you wanted it protected and ruggedized!

    I couldn't see the video embedded just yet (I believe it may take a while to process, especially with a high-res format), so I used the dailymotion link.

    Was it battery-powered, and was it strapped to a lamp-post or something, to log to SD card?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz

    It's setup as passive PoE, 12v ish down the two unused pairs and a local switching regulator to provide 5v to the Pi.

     

    video saved over nfs to a 2TB drive.  unfortunately the raspivid app seems to have some problems running under screen, when you exited the parent terminal screen was started from the Pi would reboot. Even just running raspivid in the background with '&' is unreliable so I really wasn't sure I'd caught it.  I have several bits of video that ended early and even just a loop in a shell script to keep restarting it appeared to cause the Pi to reset at some point.

     

    Not a lamp post, but a bracket bolted to the outside of my window..  As you can guess, that was well inside the evacuation zone. So me sat much further back trying to stop it rebooting while using a 3G connection was somewhat frustrating.  Thankfully it was rebooting rather than locking up, if it had locked up there would have been nothing I could do.

    I cropped a few mins off the start of the video, but where it ends is due to another reboot. I thing something like 20-25mins was the max I got without a reboot. Still, worth it in the end image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago

    Wow, what a test subject!

     

    I too had to use the dailymotion link, as the embedding here doesn't work for me either.

     

    Was it deliberately shot with the camera on its side?  I watched it with the sky on the left of the frame.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Was it deliberately shot with the camera on its side?  I watched it with the sky on the left of the frame.

    Yep, distance vs the field of view of the standard lens meant it was the only way.  That's widescreen for you too, I'd probably have got about a third of the block being demolished and most of an empty street the other way.  It's also a bit odd.. take a 1920x1080 still image with it and the field of view is different from 1920x1080 video

     

    When I was building the case I gave myself the option to mount the camera either horizontally or vertically anyway, so not a huge problem for other uses

     

    No surprise though that when you look in the camera section of the RPF forum there's lots of people with creative mods to get different / better lenses.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to e14 Contributor

    Selsinork

     

    Great video.

    The building looks better than half the ones they knocked down in Christchurch, inc a few that they are removing because they don't fit the current plan.

     

    I like your case and mounting, as my project is to shove it up on the skifield, which obviously has all sorts of unpleasant weather,

    Luckily its mainly stills we want to send back over wireless.

     

    I do need to add a controller to control the solar and start it up and shut it down at the end of the day.

     

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    http://gizmodo.com/5915888/an-important-psa-on-why-you-should-never-shoot-videos-vertically

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to e14 Contributor

    I thought the trashy mirror photo article was good.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to mcb1

    Reminds me of these:

    http://www.element14.com/community/blogs/pdp7/2013/05/31/boring-commute-my-favorite-engineering-open-source-podcasts

    http://www.element14.com/community/blogs/pdp7/2013/05/24/my-t-shirt-for-this-tgif-spacewar

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to e14 Contributor

    thankfully he doesn't have the same cleavage.

     

    Because they are a photo, he's allowed the portrait mode.....

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    coder27 wrote:

     

    http://gizmodo.com/5915888/an-important-psa-on-why-you-should-never-shoot-videos-vertically

    While I don't disagree on the annoying part, a lot of the rest of that is just nonesense.

     

    Anyway, here's a composite of approximately the same position, one horizontally, one vertically.

     

    image

    So how would you solve that problem ? 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
>