Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Rugged RPi Camera case
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 33 replies
  • Subscribers 710 subscribers
  • Views 6221 views
  • Users 0 members are here
  • raspberry
  • rpi_camera
  • raspi
  • pi
  • demolition
  • raspberry_pi
  • raspberrypi
  • rpi
  • camera
Related

Rugged RPi Camera case

e14 Contributor
e14 Contributor over 13 years ago

I've been working on a mount and a fairly rugged case for my RPi camera recently, some photos here

https://picasaweb.google.com/selsinork/RPiCamera

 

The end goal being to do some timelapse and video where the camera would need to be outside in a rather hostile environment

 

This was the result from earlier today

 

the little camera did well image

 

Edit: does the embedded video work ?  I don't see it, so here's the link http://www.dailymotion.com/video/x1255yy_sandiefield-road-demolition_webcam

  • Sign in to reply
  • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to Problemchild

    Is that an Otter box or some such?

    It appears to have a nice gasket seal on the rim!

     

    Also did you drill into the case for the camera or merely stick the whole board on the back with out recessing the lens I'm sure you really wouldnt want to compromise the seal unless you needed to image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to Problemchild

    I'm busy trying out some waterproofing solutions for My PI and Cam if this gives waterproofing to a meter or two then this would be great here's the kind of thing I was trying to get more of.

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to Problemchild

    John Alexander wrote:

     

    Is that an Otter box or some such?

    It's made by Bernstein  10163561016356  and is IP65, so won't do for submersion. I also got 13253981325398 which is IP67 and I believe that gets you down to 1m

     

    Also did you drill into the case for the camera or merely stick the whole board on the back with out recessing the lens I'm sure you really wouldnt want to compromise the seal unless you needed to image

    The only hole I put in the case is the one at the bottom for the cable gland. The camera is mounted on some bits of ABS offcuts that are bonded to the inside of the lid with epoxy. The mounting holes on the back are provided for you and are outside the seal.

    It's just a standard Skintop cable gland I'm using, no idea if it'd handle submersion, but I suppose you could seal it up with epoxy to be sure.

     

    I think I'd probably just put the cable in and then submerge it for a while without the Pi or camera to see if it leaked image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to mcb1

    Mark Beckett wrote:

     

    Its a cheaper version than a GoPro, so I expect to see more of these appearing now you've started a trend.

    It's kind of what I expect to see, there's things you can do with a Pi camera that you'd think twice about risking an expensive camera on. While you can get some really cheap 10Mpxiel point and shoot type cameras, you mostly lose the capabilities to script the control of what it does, so the Pi + Camera can be quite an interesting combination.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to mcb1

    Mark Beckett wrote:

     

    It was suggested to me that a standard outdoor floodlamp makes an ideal rugged holder.

    That's an interesting thought, although I suspect mounting stuff inside one of those could be a bit more challenging.  I may try it next time though..

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    there's things you can do with a Pi camera that you'd think twice about risking an expensive camera on.

     

    Very true, and it's true for all components, whether they be ARM boards or cameras or absolutely anything else.  The price point makes all the difference in the world when it comes to speculative experimentation.  It's not only that more people can afford it, but also as you noted, that when it's pocket change then you don't feel too bad destroying the item accidentally or putting it at risk by modifying it deliberately for a project.

     

    This is why I'm such a fan of what we've been loosely calling "the Pi niche" of pricing, and why it's so important that other manufacturers are coming onstream to extend the possibilities available to us.

     

    One use for the Pi camera that appeals to me is an HD computerized microscope, as I already have a 14X-60X binocular scope and lots of related optical bits and pieces, and computerizing it would add greatly to its abilities.  Last month there was a nice project described on the Element 14 Pi Blog about linking a Pi camera to a Lensman microscope, and it shows how nice (and useful!) the results can be.

     

    Morgaine.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to morgaine

    Indeed I have a nice inspection microscope I could do the same just need to cut a square bit of acrylic to mount the cam to then a sequence of round ones with holes for the lens to adapt to the eyepiece.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to e14 Contributor

    I was going to use a Lion battery pack and a regulator so we kept the whole thing sealed. Obviously that limits the total endurance but for many things I'm sure it will be great.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to Problemchild

    Only other thing I can think of is that the heat from the Halogen may cook the PI even behind the reflector

    yep it would.

     

    I wasn't thinking of leaving the Pi lamp or any of the reflector in their ... just using the housing.

     

    There is a sinlge mount point that holds the reflector and the lamp bracket available .

    yes there is some work to holding it, but then the excellent plastic box also had some mounting considerations as well.

     

     

    Mark

     

    31/7/13 edit to remove the wrong word .... what was I thinking.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to mcb1

    Mark Beckett wrote:

     

    31/7/13 edit to remove the wrong word .... what was I thinking.

     

    Dither is used in audio to improve overall perceived sound quality.  You're just extending the domain of this engineering technique. image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<>