Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Rugged RPi Camera case
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 33 replies
  • Subscribers 710 subscribers
  • Views 6219 views
  • Users 0 members are here
  • raspberry
  • rpi_camera
  • raspi
  • pi
  • demolition
  • raspberry_pi
  • raspberrypi
  • rpi
  • camera
Related

Rugged RPi Camera case

e14 Contributor
e14 Contributor over 13 years ago

I've been working on a mount and a fairly rugged case for my RPi camera recently, some photos here

https://picasaweb.google.com/selsinork/RPiCamera

 

The end goal being to do some timelapse and video where the camera would need to be outside in a rather hostile environment

 

This was the result from earlier today

 

the little camera did well image

 

Edit: does the embedded video work ?  I don't see it, so here's the link http://www.dailymotion.com/video/x1255yy_sandiefield-road-demolition_webcam

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to mcb1

    Mark Beckett wrote:

     

    The building looks better than half the ones they knocked down in Christchurch, inc a few that they are removing because they don't fit the current plan.

    Those weren't in the current plan either, but regardless of how they look, they were plagued with damp due to poor construction. So they skipped the queue and were demolished early.

     

    I like your case and mounting, as my project is to shove it up on the skifield, which obviously has all sorts of unpleasant weather,

    Luckily its mainly stills we want to send back over wireless.

    It's a challenge to get something that's properly resistant to the elements while at the same time not messing up the images. That case is made of 3mm polycarbonate, and depending on the lighting conditions it becomes more or less obvious that there are distortions.  There's obviously other choices depending on conditions and how good you need the images to be. It was suggested to use a thin glass filter bonded to the outside with a hole cut for the camera, but I simply didn't have a clue what to expect here, so went for the more robust method.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    Love this project, have you thought about removing the IR filter on the camera and using the project for night time photography?

     

    There looks like there is plenty of space in the case to include motion sensors and IR emitters.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    image

     

    You've just invented the ideal format.  It'll take the world by storm !!!! image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    shhh... you don't want to go giving them any more silly ideas image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Joseph Kirk wrote:

     

    Love this project, have you thought about removing the IR filter on the camera and using the project for night time photography?

    Not really, but since the camera is quite cheap and they appear to be reasonably easily available now then there's a chance I might try it.

     

    There looks like there is plenty of space in the case to include motion sensors and IR emitters.

    There's a fair bit of space left, you're limited by sizes of cases with clear lids that a Pi will fit in though.  One idea is a simple ambient light sensor on i2c which would let you change settings for day/night or whatever.  I do have some sensors, but just didn't have time to put one in there this time.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 13 years ago in reply to e14 Contributor

    Mine are much less trashy as I'm holding Linux

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to fustini

    Drew

    So we replace the white low cut TShirt with one that features Linux ...?

     

    Selsinork

    It was suggested to me that a standard outdoor floodlamp makes an ideal rugged holder.

    image

    Nice thin glass on the front, a bracket arrangement to mount it, inc adjustment, and fully waterproof to boot.

    They come in at least three sizes (150w, 500w and 1000w), with the 150 and 500w being throw away cheap.

     

    You'll need to mount the camera, Pi and anything else, as the front glass folds down.

     

    I'm in two minds for my project due to the cold soak of the metal, which generally attracts more ice than anything else.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to e14 Contributor

    So how would you solve that problem ?

     

    There is nothing worse than chopping the top or bottom of the image off.

    Fixed lens, fixed location ... you get what you can.

     

    Your vertical approach was right for the intended use, and fully captured the subject matter.

     

    We can all lay on our sides and watch, or download and rotate it.

     

    Its a cheaper version than a GoPro, so I expect to see more of these appearing now you've started a trend.

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to mcb1

    Would getting one with a PIR be usefull as you coud use the relay/ Scr drive the PIR uses to switch the lighting on the cheap  or even use the PIR as an additional sensor into the PI.

     

    Only other thing I can think of is that the heat from the Halogen may cook the PI even behind the reflector

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to Problemchild

    Thinking about it I'm not sure most  lights are as sealed as they could be they often have spiders and all sorts making home in there .. might be best to house the PI inside an inner case or at least keep it stood off the outer shell of the lamp.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<>