Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Cirrus Logic - RPI 2 FFT on streaming audio
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 2 answers
  • Subscribers 707 subscribers
  • Views 2366 views
  • Users 0 members are here
  • wolfson
  • logic
  • raspberry
  • python
  • audio
  • pi
  • cirrus
  • 2
  • raspberry_pi
  • fft
  • raspeberry_pi_accessories
  • card
Related

Cirrus Logic - RPI 2 FFT on streaming audio

e14 Contributor
e14 Contributor over 10 years ago

Hi everyone,

My current project is to run constant FFT on an audio stream and output the data to a 3D LED Array. Google 3D LED cubes if you don't know what they are. My cube is more of a rectangular prism, 24x8x8=1536 LED's. I am new to the world of PI and have found the support for the cirrus logic card to be vague, if it wasn't for ppl like ragnar.jensen I'd probably still be stuck (thanks for all the information you've shared).

 

Anyway, currently I am recording 1 second of audio after a 1 second delay. So it takes 2 seconds to get the data / audio.

 

I then perform the FFT on 16384 samples. But this is only 1/3 of the 44000 raw audio samples recorded in the 1 second interval. I then group the frequencies into bands and then scale the amplitudes of those bands into a single byte which represents the bands power. The result of each FFT is 24 bytes, one byte for each band. All this takes 0.1 second.@@@@@

 

It then takes 0.004 seconds to send that data to my PIC, which I had to bit bang through the GPIO's since I couldn't get I2C or UART working.

 

The LED array takes the data and displays the 24x8 bits on the front row, when it receives the next group of data the front row shifts back one row. The LED array displays 3 dimensions, time (each group of data), frequencies and amplitude.

 

Question:

In the arecord command, I would like to erase the delay or change it to 0 seconds and change the minimum record length so I can stream the data at a faster rate to the LED array. Does anybody know how????

 

Answering this would result in a real time graphics equalizer on live audio and a more fluent transition between groups of data (more like a wave travelling away from you).

 

If anybody has an idea on how to achieve this please reply, or share your thoughts.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    import numpy as np

    import wave

    import struct

    import os

    from struct import unpack

    import time

    import RPi.GPIO as GPIO

    GPIO.setmode(GPIO.BCM)

    GPIO.setwarnings(False)

    import smbus

    import time

     

    bus = smbus.SMBus(1)

    address = 0x40

    mode = 0x00

     

     

     

    def sendbyte(txbyte):

        CLK = 5

        OUT = 6

        NEXT = 25

        GPIO.setup(CLK,GPIO.OUT)

        GPIO.setup(OUT,GPIO.OUT)

        GPIO.setup(NEXT,GPIO.IN)

     

     

        number = 1

        for i in range (1,9):                   #for bits 1 to 8, send bit values

           

            if txbyte &number != 0:             #if txbyte bit = 1, data line = 1

                GPIO.output(OUT, 1)

                #print "1 %s" %(number)

            else:                               #else data line = 0

                GPIO.output(OUT, 0)

                #print "0 %s" %(number)

               

            while GPIO.input(NEXT) == 0:        #wait for pic to say its ready for data

                time.sleep(0.0000005)                #sleep for 0.5 microsecond

               

            GPIO.output(CLK, 1)                #raise the clk edge indicating data is valid

           

            while GPIO.input(NEXT) == 1:        #wait for pic to say it is not ready

                time.sleep(0.0000005)                #sleep for 0.5 usec

            GPIO.output(CLK, 0)

            number = number*2                   #change to the next bit

           

        GPIO.output(OUT, 0)                     #lower the data line as byte tx has ended

       

     

       

     

     

     

     

     

    os.system("bash /home/pi/Desktop/Code/Reset_paths.sh")

    #os.system("bash /home/pi/Desktop/Code/Record_from_DMIC.sh")

    os.system("bash /home/pi/Desktop/Code/Record_from_lineIn.sh")

    audiolr = []

    index = 0

    #frequency bandwidths for display                               

    bw = [7,9,13,19,27,37,51,69,99,139,189,249,319,419,519,699,899,1099,1399,1899,2499,3199,4099,3200]

    #number of values in each band - divisible factor

    band = [7,3,3,6,6,11,14,20,26,37,52,70,193,119,156,193,261,334,409,520,705,929,1186,1528]

    #frequency center of bandwidths

    freq = [10,24,32,45,62,85,118,163,224,310,430,595,815,1100,1470,1940,2550,3350,4350,5600,7250,9500,12300,15950]

     

    subindex = 0

     

    for i in range(0,16384):

        audiolr.append(0)

     

    freqoutput = []

    for i in range(0,24):

        freqoutput.append(0)

     

    while True:

        startt = time.time()

        os.system("aplay -vv /home/pi/Desktop/Code/Song.wav")

        os.system("arecord -f cd -c2 -D hw:sndrpiwsp -d 1 Song.wav")

     

       

        wavfile = wave.open("/home/pi/Desktop/Code/Song.wav",'r')

        paramet = wavfile.getparams()

     

        wavfile.setpos(27100)

        wavedata = wavfile.readframes(16384)

        audio = struct.unpack("<32768h",wavedata)

        i = 0

        index = 0

        for i in range(0,32768,2):

            audiolr[index] = audio[i] +audio[i+1]

            index += 1

     

        complexfreq = np.fft.fft(audiolr[0:16384])

     

        print len(audiolr)

        f = [0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0]

     

     

     

        start = 1

        stop = 8

       

     

     

        for index in range(0,24):

            for subindex in range(start,stop):

                f[index] = f[index] + abs(complexfreq[subindex])

            f[index] = (f[index]/32768)/band[index]

            #print "%s, Fc=%sHz,    BW-%sHz,     power %s" %(index+1, freq[index], bw[index], f[index])

            start = stop+1

            stop = stop + band[index]

     

        for index in range(0,24):

            if f[index]>32:

                freqoutput[index]=255

            elif f[index]>16:

                freqoutput[index]=127

            elif f[index]>8:

                freqoutput[index]=63

            elif f[index]>4:

                freqoutput[index]=31

            elif f[index]>2:

                freqoutput[index]=15

            elif f[index]>1:

                freqoutput[index]=7

            elif f[index]>0.5:

                freqoutput[index]=3

            elif f[index]>0.25:

                freqoutput[index]=1

            else:

                freqoutput[index]=0

            sendbyte(freqoutput[index])

        for index in range(0,24):

            print "%s, Fc=%sHz has a power of %s, Equalizer Level = %s     BW=%sHz" %(index+1, freq[index], f[index],freqoutput[index], bw[index])

        print (time.time()-startt)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Bit wobbly after I moved it between home and work a few times, I've given up straightening everything,,,, that is until everything works as planned.image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    image

    The output of the FFT is grouped into 24 bands, the FC denotes the center frequency. On the far right is the BW. The power level is the average power of the individual frequencies in that band. The final output that is sent to the PIC is a scaled value shown by the equalizer level, note: an Equalizer level of 63 in binary is 0011 1111 which will show an amplitude of 6 LEDs being illuminated on the array.

     

    I ran the python program in the previous post with a 3.5mm audio cable plugged in between my phone and the cirrus logic cards line in. I used an app called "PA tone"  (which is free) to generate a 5000Hz Sine wave tone out of my phone. The results show the tone in the 20th band, with an FC of 4350Hz and a BW of 1899Hz (which is 3400Hz to 5300Hz). I found some noise present in unused bands no matter what frequency I generated. I put that down to noise in the phones output or on the line, poor handling of the FFT output (my fault) and digital noise in single precision numbers which can become collectively significant when summed. But clearly the frequency amplitude of the 5000Hz wave is the most significant.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago

    Hi Daniel,

     

    Looks like a fun project : )

    I'm not knowledgeable in Python but you might be pushing the limits of it to be honest. It could be better to code this in C, because there is a C API to the ALSA framework, which

    should allow you to read bytes from the audio device (hw:0 or whatever). Maybe there is an API for Python too, I just don't know it.

    I've not used the C API, but it is described on the ALSA site. Then you should be able to read exactly what you need (e.g. a fraction of a second instead of having to read a whole seconds-worth),

    and using C would also allow you to maybe do your FFT faster (just a guess).

    If you really want to speed the calculation up, then there is a feature called 'NEON' on some of the ARM processors (not on the older RPI models, but is available on the RPI 2 and BeagleBone Black)

    but it takes some learning to use. Fortunately you don't need to learn it, there are libraries out there that are already coded to take advantage of NEON.

    Also, you may wish to migrate to the BeagleBone Black since there is a Music Tech design challenge for it out there, if you (say) want to convert your device into a tool for creating and visualising

    sounds : ) Just an idea! Less than two days left to apply for it though.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • scitechindian
    0 scitechindian over 10 years ago in reply to e14 Contributor

    OMG ! image Awesome ! how much time it took to build image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to scitechindian

    Hi SYED. It took 5 days with 2 people soldering to build the LED array (approximately 80 Man hours). It took me 3 days to design,route and solder the PCB. It took one full day to join the wires to the board and It took about 2 days to program the PIC.

    But it has taken me about 2-3 weeks to research and develop the code on the raspberry pi, since I have never touched one before this.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to shabaz

    Thanks for your reply shabaz, I appreciate your comments. I found this on a different forum but I don't know how to use it.

    http://stackoverflow.com/questions/29839082/capture-record-audio-in-linux-for-milliseconds

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to e14 Contributor

    Eh eh ... Coding is always the hard part image

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago

    Hello Daniel,

     

    I found this on a different forum but I don't know how to use it.

     

    I took a look to the mentioned library available on GitHub: http://stackoverflow.com/questions/29839082/capture-record-audio-in-linux-for-milliseconds

    Despite the excessive simplification I am sadly used reading by the experts of stackoverflow, these piece of code are almost interesting as released under source so you can eventually change and adapt to your needs without big difficulties interfacing them. You should consider it as a simplifying interface between Alsa - that is, a library - and your program. The point IMHO is not the math but the fact that in a multithreaded environment without a real time kernel you risk to have unpredictable delays due the other common processes Linux is running by itself (at least). If you are using Cirrus Logic audio on Raspberry PI2 I suppose you have installed a real time version of Raspbian, is correct? I have done so and despite the limitations in the update / upgrade possibilities (that are not available after this version of kernel is running) I have experienced that solved a lot of problems.

     

    There is another factor that I suggest you to consider; the audio source should be also played or should just only managed by a mathematical point of view? In this second case I think that the Alsa library should be sight by a different point of view as what you need in this case is a robust data acquisition system and probably real-time processing of the data generating the visual audio you will provide.

     

    Let me know. Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>