Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Cirrus Logic - RPI 2 FFT on streaming audio
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 2 answers
  • Subscribers 707 subscribers
  • Views 2360 views
  • Users 0 members are here
  • wolfson
  • logic
  • raspberry
  • python
  • audio
  • pi
  • cirrus
  • 2
  • raspberry_pi
  • fft
  • raspeberry_pi_accessories
  • card
Related

Cirrus Logic - RPI 2 FFT on streaming audio

e14 Contributor
e14 Contributor over 10 years ago

Hi everyone,

My current project is to run constant FFT on an audio stream and output the data to a 3D LED Array. Google 3D LED cubes if you don't know what they are. My cube is more of a rectangular prism, 24x8x8=1536 LED's. I am new to the world of PI and have found the support for the cirrus logic card to be vague, if it wasn't for ppl like ragnar.jensen I'd probably still be stuck (thanks for all the information you've shared).

 

Anyway, currently I am recording 1 second of audio after a 1 second delay. So it takes 2 seconds to get the data / audio.

 

I then perform the FFT on 16384 samples. But this is only 1/3 of the 44000 raw audio samples recorded in the 1 second interval. I then group the frequencies into bands and then scale the amplitudes of those bands into a single byte which represents the bands power. The result of each FFT is 24 bytes, one byte for each band. All this takes 0.1 second.@@@@@

 

It then takes 0.004 seconds to send that data to my PIC, which I had to bit bang through the GPIO's since I couldn't get I2C or UART working.

 

The LED array takes the data and displays the 24x8 bits on the front row, when it receives the next group of data the front row shifts back one row. The LED array displays 3 dimensions, time (each group of data), frequencies and amplitude.

 

Question:

In the arecord command, I would like to erase the delay or change it to 0 seconds and change the minimum record length so I can stream the data at a faster rate to the LED array. Does anybody know how????

 

Answering this would result in a real time graphics equalizer on live audio and a more fluent transition between groups of data (more like a wave travelling away from you).

 

If anybody has an idea on how to achieve this please reply, or share your thoughts.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to balearicdynamics

    Hi Enrico,

                   Thank you very much for sharing your thoughts I agree with you on many things, such as- all I require is a robust data acquisition system. It just needs to capture live data, perform math and output the result. I do not need a GUI, applications and sub processes that I don't even realize are running. On a side note: I originally chose the raspberry Pi for this project for 3 reasons, its cheap, its fast enough to perform the calculation, there appeared to be lots of support/resources for me to learn from and achieve my goal.

    Currently I am using a standard kernel, but I intend on attempting to use a real time kernel once I can capture audio in frames determined by milliseconds or number of samples. Like you said, once you change to real time kernel there are limitations on updates. So I wanted to achieve my goals in the most common environment that the community uses. I am taking tiny little baby steps!

     

    I tried to compile main.cc (from Waxo's library on GitHub), using geany, but this failed. I am not sure why, perhaps geany needs to be configured to compile c++ instead of c? Could you point me in the right direction about things I should learn or do?

     

    After that attempt, I tried to edit the source file "aplay.c" as mentioned in that forum. So I downloaded all the ALSA utils and libraries I could find as compiling aplay.c includes files which include other files.

    Within aplay.c, the start_delay was easy enough to find, I simply changed it to 0 on lines 119,505 and 651

                          the record duration was a bit more difficult to find. I believe it is in the sub routine, static void capture(char *orig_name) under the variable count,, could be wrong. (around line 2926)

    In any case I could not compile aplay.c either

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to e14 Contributor

    Hi Daniel,

     

    I have already experienced a similar problem using the CL for data processing in the Meditech project. One of the difficulties is to download the RT Linux for PI. I have a copy and if you need I can send you it by private email just because I have searched it again recently and I have not found image

     

    About the issues on the RT Kernel specific for the CL and some details I have published some articles in past that I will link below. More details I can find in my local archives.

     

    Meditech: Microphonic stethoscope

    Cirrus Logic Audio Card: audio monitor while recording

    Meditech: Text-To-Speech user support

     

    Here and there in these posts there are some useful information, links and also good comments from the other valuable guys. For more detailed information let me know because to have the stuff working I had to do a lot of research and tests and I have saved almost all the documentation.

     

    Hope this can help.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • scitechindian
    0 scitechindian over 10 years ago in reply to balearicdynamics

    awesome reply image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 10 years ago in reply to e14 Contributor

    It may be far to late but you might just possibly want to consider moving away from the Pi - you can buy as ST Nucleo board with a 180MHz Arm CortexM4 for under £10 and it can easily do 12 bit ADC at any rate you like (and has interfaces to use external converters if you really need them) , FFT and get data out to your display. The good thing is that it is easy (simple enough and documented) to code without any OS in the way. The PI can probably out perform it on the FFT but not in the IO.

    If you think you might go this way I can give some more pointers about how to make the best of the ADC/DMA features to get what you need.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<