RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum ROADTEST POLL: Would You Be Interested in Roadtesting an Open Source Single Board Computer?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 2747 subscribers
  • Views 4422 views
  • Users 0 members are here
  • roadtest survey
  • beaglebone play
Related

ROADTEST POLL: Would You Be Interested in Roadtesting an Open Source Single Board Computer?

rscasny
rscasny over 3 years ago

imageI have a couple of new BeagleBone SBCs that I'd like the community to roadtest.

This poll is to gauge the level of interest.

About the product:

BeaglePlay is an open-source single board computer designed to simplify the process of adding sensors, actuators, indicators, human interfaces, and connectivity to a reliable embedded system. It features a powerful 64-bit, quad-core processor and innovative connectivity options, including Wi-Fi, Gigabit Ethernet, sub-GHz wireless, and single-pair Ethernet with power-over-data-line. With compatibility with 1,000s of off-the-shelf add-ons and a customized Debian Linux image, BeaglePlay makes expansion and customization easy. It also includes ribbon-cable connections for cameras and touch-screen displays, and a socket for a battery-backed real-time-clock, making it ideal for human-machine interface designs. With its competitive price and user-friendly design, BeaglePlay provides a positive development experience for users.

Features

  • Multicore A53s with R5, M4s and PRUs processor, TI AM6254
  • WiFi/2.4G, MIMO/5G, SISO M2 1216, TI WL1807 Wi-Fi module, U.FL x2
  • TI BLE/SubG CC1352P7 M4+M0 with BeagleConnect firmware
  • 2GB(1Gb x 16)-1600MHz 3200Mbps DDR
  • Kingston 16GB eMMC
  • Gigabit Ethernet with RJ45 x1, single pair Ethernet and power over with RJ11
  • Power input with USB Type-C
  • HDMI Type-A supports up to Full-HD/1080P with 24-bit RGB
  • Support FPC 22pin CSI and FPC 40pin OLDI
  • 1x MikroBus connector, 1x USB Type-A, 1x micro SD socket, 1x QWIIC, 1x grove connector, 1x RTC

Documentation

Datasheet 
Getting Started 
For More Information

Polls

  • Sign in to reply
  • Cancel
  • Amethyst
    Amethyst over 3 years ago

    Some of these are tough to answer.

    I'm currently working on  a Samus costume with many bells and whistles. For some applications such as mine, you may want to give an estimated battery draw for portable applications.

    I'm considering that this board may be overkill for my project, but I'm still testing many ideas to add, and having more resources available is a nice thing, battery depending. If you wanted me to try and it's not heavy power consumption, I'm interested.

    How I describe myself is vague for how I should answer. I'm IPC certified and do make props for people using electronics, but probably not enough for anything but "hobbyist"?

    But if you update with battery life, please lmk. I'm off to make another forum post for ideas for my project lol.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • misaz
    misaz over 3 years ago in reply to RobPaige

    Feel free to apply here: /products/roadtest/rt/roadtests/624/sign_up_to_review_th#pifragment-4106=9&pifragment-4100=4

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • RobPaige
    RobPaige over 3 years ago

    I'd be interested, if you'd have me. Would likely be testing integration with 3d printers

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 3 years ago in reply to Fred27

    There are some expensive Ethernet Development Tools out there for 10Base-T1L single-pair Ethernet PHY.

    For example, the DP83TD510E-EVM (price circa $180).

    I think this would make for an interesting design challenge as suitable single pair Ethernet PHY chips are around $8. E.g. https://www.ti.com/lit/ds/symlink/dp83td510e.pdf

    There is also this new PHY+MAC chip from onsemi at a similar price: https://www.onsemi.com/download/data-sheet/pdf/ncn26010-d.pdf

    EV boards for that chip are rather expensive.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Fred27
    Fred27 over 3 years ago in reply to mp2100

    I've been searching and I don't think you can buy any SPE devices - apart from a few impractically expensive specialist bits of kit. Also, it doesn't seem that RJ11 is a standard connector for SPE so it would also probably involve making up your own cables.

    I'd also like to play with SPE, but I don't think it's practical as part of a road test - unless it's between 2 BeaglePlays.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 3 years ago in reply to rscasny

    A matching power supply would be nice. I was myself thinking a usb-c to terminal board adapter to be included ,  most any power supply could be used and the tester could try different variations of current limit/voltage sag. Some Grove connector pigtails would also be really helpful, I have a nice collection of sensors , most don't have Grove connectors. The sensors that do have Grove connectors have lost their provided cables in the micro-black hole that randomly moves about in my man-cave.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 3 years ago in reply to colporteur

    I don't think it comes with a power supply when I opened up the package we received them in. Adding in a power supply is not really a problem. Often times roadtesters have a power supply or power cords and we ask them what they need. The power supply shouldn't be a deal breaker. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 3 years ago in reply to charlieo21

    I would challenge the assumption it requires a 5V 3A power supply.

    I think if the RoadTest requires the candidate to provide the power supply it needs to state that or provide the supply. It has been suggested in another post an escrow be established for a candidate to participate. The participant having to purchase a PS can be a burden just like an escrow. I have struggled with cables used in RoadTests to discover I'm using the wrong one. Great teaching moment but hey was the RoadTest about the correct cable.

    If you want to test a Raspberry Pi you better have knowledge of power requirements or your frustration will mount. Clearly tell me what I am getting and what I would need to purchase. If I have to purchase, what is recommended not leave me guessing. Try any old 5V 3A PS on a Pi and let me know of the success.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • skruglewicz
    skruglewicz over 3 years ago

    I will apply for this roadtest. My experience with Development kits will qualify me to do the roadtest. Very interested.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • charlieo21
    charlieo21 over 3 years ago in reply to DAB

    It requires a 5V 3A power supply.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
>