Browse By Tags

  • LabVIEW Test Automation - Part 1: Hardware Setup

    I have this plan to script an automated test setup. I want to check the behaviour of GaN power FETs. I'll need to control the input signals that drive the FETs, the load that the FETs see, and the measurement instruments. To make this possible, I bought…
  • LabVIEW Baby Steps

    I have this plan to script an automated test setup. I want to check the behaviour of GaN power FETs. I'll need to control the input signals that drive the FETs, the load that the FETs see, and the measurement instruments. To make this possible, I bought…
  • Repairing my Rigol DS1052E Oscilloscope

    Unfortunately my trusty old Rigol DS1052e oscilloscope suffered from damage on the way to the calibration laboratory. The control knob for the trigger level had been broken off and the calibration lab advised that they could not repair the device, so…
  • SimpleLink™︎ Sub-1 GHz Wireless Microcontroller - Side Note : Measure Power Use of Sensor Controller Engine

    Complexity: medium What do you need: a CC1310 LaunchPad Code Composer Studio Wirelsess Sensor Network Node example loaded An instrument to log low currents This blog digs into the sub-module that manages communication with sensors. A dedicated part of…
  • TI Ultrasonic Sensor - Show 3 Signals on a 2 Channel Oscilloscope (RIGOL DS1052E)

    The TDC1000-TDC7200EVM TDC1000-TDC7200EVM evaluation module has 4 main parts The TDC1000 analog front-end and a pre-programmed MSP430 microcontroller on the board, a 1MHz Piezo Ceramic sensor that plugs into the board and a GUI client for on your PC.…