Browse By Tags

  • Pads and Nets both red, so I'm a little confused.

    I made a simple PCB that involves surface mounting large components (.15x.076 pads), and noticed that both the pads and net connections are all red in the Board Editor. I just wanted to make sure that this is ok, and that the pads are actually above the…
  • Connect two different NETs

    This isn't that simple as it first sounds. Assume the following scenario. Fullscreen contentimage_30700.html Download <html><head><title>Jive SBS</title></head> <body><font face="arial,helvetica,sans-serif"> <b>Error</b><br><font size…
  • How do I sync removal of pin from a net between schematic capture and PCB layout

    I have two nets: LED_3 and CHARGE_DISABLE . They are connected to pins 14 and 19 of my microcontroller, respectively. I would like to swap the pinout such that now net LED_3 is connected to pin 19 and net CHARGE_DISABLE is connected to pin 14 . To be…
  • BUSSES, MODULES and NETS

    Hi everone, maybe someone can help me. I'm pretty familiar with but it seems like I cant solve the following problem: (I'm working with EAGLE 7.7) I've created a MODULE named DAC_CHANNEL and added a "bus" PORT called DB[0..13] to it. I've added 16 DAC_CHANNEL…
  • Can you interconnect nets with different names?

    Hi! I'm wondering if it's possible to inter-connect busses (nets) with different names? This is what I'm trying to do: I have a large uC that has different pins for analog, I/O and logic power. Each is connected to VCC, but with specific and different…
  • Other supply nets (not sure if it's a net)

    I'm making an Eagle version of an old paper schematic. The drawing has many places that look like nets to me, named ending of lines that have another named partner elsewhere on the drawing. For example, V+ is one and I understand how to use the V+ in…
  • How to rename routed nets without having them disconnect.

    I have multiple nets named 5V. Now I want to rename them all to 3V. I have to click each net anc rename it to 3v. Is there any way to rename all 5V nets to 3V?
  • Clearance from Ground Plane on certain nets?

    Is there a way to specify that you want more clearance between the ground plane and certain nets (wires) etc? If I set the clearance in the Defaults I get good clearance on most nets but there are a few higher current nets I would like to increase the…