The board uses the default AC-coupling capacitor values on the PCIe edge connector. This probably comes from the GTH transceiver user guide and doesnt take into account requirements comming from the PCIe standard. As such, the board might have difficulties…
I think I just ran into an early-stage bug on the Arduino Uno R4 WiFi.
My previous 2 blog posts separately covered displaying frames on the LED Matrix and Receiving BLE commands. Combining the 2 sketches, however, caused it to break.
When I first…
Hi,
I'm trying to work with some mechanical layers on my PCB, but I can't find where to enable or disable them.
I've read that the "View Configurations" > "Board Layers and Colors" is supposed to look like this:
Where you can enable and disable…
Hi All,
I have a weird problem on Circuit Studio that makes me a bit confused, if I'm missing something here or it's a software bug!
I set my design rules, and everything works well as per the rules until I update the design rule again for making…
Although I'm documenting which recent quizzes (since the new site's been up) didn't award me points, there are at least two that showed all correct answers in that there were no answers marked in red and I logged all my answers to these two. Though no…
I read that CS is slow for any updates and bug fixes, but this bug MUST be fixed asap.
CS loses focus and drop me to any other windows on my Win10 after I select an item to edit from popup. I didn't found a specific pattern when this behavior begins…
Video showing the net parameter of a via gets overidden even when you explicitly set it during placement when adding a via over top of a polygon pour. The via automatically changes its net parameter to the "highest priority" polygon (probably the ...
I think I've run into a bug in 7.2.0 Standard that defeats the Export Libraries feature much of the time. The main symptom is that during the export process a dialog pops up with "[Somefile.scr], Line [n] The Standard edition of EAGLE can't perform the…
From a current project Version 7.2.0, Eagle Hobbyist. In schematic module (say "AB-CDEF-1") net name is "SW1". This is is visible and can be manipulated routed, changed, etc. as normal. in a PCB layout. It is always showing up as AB-CDEF-1:SW1 I want…
Often (but not every time) when placing a part from a library, the display stops showing the part outline being dragged. Blindly clicking to drop causes the part to magically appear (usually in the wrong place...), and (sometimes) changing the zoom level…