Browse By Tags

  • When and in Which Regions will the Raspberry Pi 5 be Available to Purchase?

    When can I get my hands on one, and which countries or regions will it be available to pre-order or purchase in?
  • order Raspberry Pi to Rwanda

    I want to order raspberry Pi 3 Model B +. I want to know if it is available and price of 10 Items
  • DRV 102 (TO220)

    Hi,in order to vary the duty cycle at same time for example from 20% to 50 to 70 to 90% ,can i program an arduino to do such control since i want actually to control a soilenoid to control the air fluid to suspension car model ?
  • Episodes Play In Reverse Order Using Continuous Play on Embedded Player

    I recently sat down to catch up on some episodes and tried the "continuous play" feature of the embedded player while streaming the videos to my AppleTV via AirParrot, but the episodes played in reverse order instead of forward as expected. For example…
  • Pre-order with virtual credit card

    Hello, I've pre-ordered Raspi with my virtual credit card and my order ref. number is ORP009210. It's said that my order will be shipped at July 2'nd. I thought that I'll be notified when my credit card will be charged and because of that I didn't transfer…
  • Order Related! #17226505

    Hi, Recently I ordered 2 Pi cameras order # 17226505 by following simple steps as registering and placing the order. There is no problem with the order in fact everything went smooth but the thing is I wish to have these items delivered to me as soon…
  • Question about your Order Status?

    Q: I have a question about my order status. A: Please contact Customer Service on the commercial site where you purchased the part by clicking here . If you are having trouble finding help with your problem or have some feedback. Please visit…
  • Getting a Quote for Parts

    Q: I need a quote on products. A: element14 Community does not provide quotes - please contact one of our global quotations teams for assistance . If you are having trouble finding help with your problem or have some feedback. Please visit our…
  • Tenma 72-7730A & 72-7732A user manual , data sheet ,Farnell order code: 2100035 , web link to for driver and software for window 8

    TENMA - 72-7730A - MULTIMETER, DIGITAL,HANDHELD, TRMS, USB Image is for illustrative purposes only. Please refer to product description Manufacturer: TENMA Order Code: 2100035 Manufacturer Part No: 72-7730A Web link to rotate to view 360 degree 72-7730A…
  • For Newark element14 customers – we are fixing the shipping fee error on Raspberry Pi

    Hello to all of you! Thanks for letting us know about the $20 shipping fee you were charged at check-out at Newark element14. We investigated what happened, and it was completely our mistake! We're really sorry for the confusion and frustration this has…
  • Tenma 72-8720  DMM, BENCH, order code 1836062, data sheet & calibration procedures

    Tenma 72-8720 DMM, BENCH, 39999 COUNTS TRMS , order code 1836062 Product Information DMM, BENCH, 39999 COUNTS TRMS DMM Type: Bench Voltage Measuring Range DC: 400mV to 1kV Voltage Measuring Range AC: 4V to 1kV Current Measuring Range DC: 400mA, 4000mA…
  • Tektronix MSO/DPO4000B series oscilloscopes,Farnell order code 1856690  to 1856711

    Tektronix MSO/DPO4000B series oscilloscopes Offering up to 1 GHz bandwidth and 5 GS/s sample rate, the MSO/DPO4000B Mixed Signal Oscilloscope Series delivers the performance you need to see fast-changing signal details. With as many as 20 channels, you…
  • I need to cancel a order.

    I ordered a RPI but the date says it wont arrive until 12/01/14..
  • Order System Glitchy for Raspberry Pi

    Before I begin I would like to thank you all who took the time to listen to my rant. I have finally joined the Element 14 community and decided I needed to get back into the fun of programming. I have placed my order for the Raspberry Pi and a Power Cable…
  • piFace Add-on

    Does anybody know where I can buy the piFace or perhaps when it's likely to become available ? Alternatively, has anybody acquired the other Interface Board and is it very comparible to the piFace ? Regards Andy
  • délai réappro Raspberry PI (512Mo) pour la france

    Bonjour, Savez-vous d'ici combien de temps il sera de nouveau possible de commander des raspberry pi à destination de la france? Merci d'avance. Cordialement.
  • ¡Nuevo equipo multilingüe para dudas sobre pedidos Raspberry Pi!

    Debido a la gran afluencia de pedidos de consumidores, Farnell element14 ha decidido crear un equipo multilingüe de agentes que os podrán ayudar a solventar las dudas sobre los pedidos de Raspberry Pi realizados en el microsite. Por ello, podéis contactarles…
  • Cancelar orden Raspberry PI

    Hola, hace una semana compré una Raspberry PI , he visto que ya se ha hecho el cargo en la cuenta bancaria y al ver que no me han contestado he decidido cancelar la orden!, he enviado un correo para cancelar la orden y no me dan opción.... Me he puesto…
  • Cancel one order?

    Hi there, I received a reminder that I was able to preorder a Raspberry Pi. I thought "damn I forgot to do it". I did a search in my emails and I did not find any trace of a order. A couple of minute later I finished my order. I received an email confirmation…
  • Registered, got the invite, but can't order

    I registered a while back, and a couple days ago I got an email: Thank you for registering your interest in Raspberry Pi . We are very pleased to tell you that you can now place your Pi order. So I clicked the "Buy Now" link in the mail, and here's what…
  • Accidentally ordered two Raspberry Pis

    I didn't notice there was 2 Raspberry Pis in the cart when the order was placed. Is there someway I can revise the order and remove one? I read that you can only buy one. Will the second one be removed and will the other $35.00 be refunded?
  • Got my Raspberry Pi, mixed feelings about Farnell

    Hi all, I just received my Raspberry Pi. I think about one month before scheduled delivery. I'm really happy about it. Anyway I ordered it for my company,I specified my EU tax id and added as comment to the order that it should be VAT free as b2b. I received…
  • How can I cancel my order?

    I would like to cancel my order (I have a reference number ORP ) with the fact that there has been a new chinese PC released these days which is smaller than raspberry Pi (it's a bit bigger than a USB flash drive) it comes with a case, it has conrtex…
  • hardware differences between batches

    the latest batch just starting to arrive reportedly has a date on the front of week 1215, compared to week 1213 and 1208 for the prior two batches. It also reportedly has Samsung memory rather than Hynix. I think Samsung has offered 512MB PoP ram for…
  • Newark knows "Diddly"!

    I just got off the phone with Newark, US/Canada, same place. They know nothing, diddly squat, rien, zip, zilch...did I say nothing! You would think after almost three months that the sales support team would have some thing new. I got some guy saying…