3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum Building a 3D printer out of Hp G85 Office jet printers
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 341 subscribers
  • Views 2790 views
  • Users 0 members are here
Related

Building a 3D printer out of Hp G85 Office jet printers

e14 Contributor
e14 Contributor over 12 years ago

Hello there my friends... so i saw these 3D printer things... and i thought it would be cool to try to make one... now i have no background with Arduino at all... but i do have a little bit of knowlege when it comes to CNC's... see my father purchased 6 of these Hp G85 office jets this was a loooong time ago at least 12 years ago recently the last of them died and was replaced with a newer inkjet...

and so with the permission of my father i started disassembling one of these printers to see if they could be of use...

 

parts of notable significance

 

steppers 2 steppers per printer... both have encoders not sure if they are useful to me though

rails there are 2 rails per printer aswell

belts two belts per printer and gears/ sprockets to go with the belts...

cold cathode light (from the scanner) useful for other projects and possibly for built in lighting on the 3d printer...

Glass plate from the scanner

various springs and stuff

 

that seems to be it

 

so my question is could i use 2-3 of these printers to build a 3d printer

will the steppers be adequate?

if not what steppers are recommended?

where can i find a mc-mega dev board and a RAMPS Sheild?

 

my goal design is to build one similar to the portable one ben heck built... although mine wont be portable...

 

any information you have to share with me would be greatly appreciated!

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    That sounds like a Cartesian-format layout (take a look at the Mendel or Prusa i3) and definitely the Arduino MEGA + RAMPS is a good way to go. Most of the other common boards (RAMBO, etc) are just combined…
  • hawkeyethehacker
    hawkeyethehacker over 12 years ago

    Springs could be used on the bed for tension, the steppers can be used to drive the axis' and the belt could be used in conjunction to move them.

    Very nice idea on the subject of recycling electronics, good luck!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to hawkeyethehacker

    thats what i was thinking with the steppers... although one is larger than the other as one was use to move the print head and ink carts... while the other was only used to move the scan bar....im not sure about using springs on the bed because im going to have the bed move along the x axis and let the hot end take care of y and z

     

    Thanks for the reply Josh i appreciate the advice!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    Ink-jet printers are great source material for 3D printers. With the parts you list, I might also look at a Delta-format printer (Rostock, Kossel, 3DR, etc). That way, you only need four steppers (three for the composite axis traverse, one for the extruder). So long as you match the three, control should be fairly simple and you can use the rails and belts together with a framework support of any type (many parts of printers can be used here). They are also fun to watch print, since they are so "busy" with all three steppers moving for any planar traverse, and have the advantage of much higher speed Z-axis traverse than Cartesian format printers. Good luck with this, though!

     

    Kirk

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    thank you Kalani!

    i have access to a plastics fabrication shop and lots of plastic so i will most likely be building the entire thing out of pvc or Centra material...

     

    as for other information what could i use to drive the steppers?

     

    i was thinking about using a arduino dev board and a Ramps Sheild poped on top

     

    like here:

    http://youtu.be/z0h2Uf6XGLs?t=3m15s

     

    other than that i still need to find out about the hot end and the Z axis... (the screw mostly)

     

    i want to use 2 steppers to drive the Z axis... just to keep things clean

    one for the y one for the x

    X axis moves the hot end

    y axis moves the print bed...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    That sounds like a Cartesian-format layout (take a look at the Mendel or Prusa i3) and definitely the Arduino MEGA + RAMPS is a good way to go. Most of the other common boards (RAMBO, etc) are just combined variations of the Arduino+RAMPS functionality. You should be about to source the Arduino MEGA for around $35-40 USD and the RAMPS as a kit around $35 USD on EBay, You would also need the stepper motor drivers (I like the Pololu A4988 or something like it, due to the ability to handle higher current than some off-brands), 1 controller per stepper or a higher current-carrying version if you want to slave dual Z-steppers from the same controller. That will require some interesting management to split off the drivers (split the driver output before the controller, you just need +1 controller and careful balancing of both motors pushing the screw). There are a wide range of options in terms of extruders and hot ends (I have never had a J-head fail at the start, but many like to fabricate their own).

     

    Make sure to let others follow your path through the various challenges you will encounter in this build!

     

    Kirk

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Nate1616
    Nate1616 over 12 years ago in reply to e14 Contributor

    Like Kirk stated, the arduino + ramps combo just can't be beat.  I use that combo on all my printers and have purchased them on ebay or through http://www.lulzbot.com/.  The j-head is a great hotend but I have also used the budaschnozzle from lulzbot with great success.

     

    Nate

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to Nate1616

    So which arduino and RAMPS combo should I use... Like I said in my original post I have no experience with arduinos... So I know Nothing about which I should use

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    Here is a extremely basic 2d drawing of what i plan to build

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hawkeyethehacker
    hawkeyethehacker over 12 years ago in reply to e14 Contributor

    A comment is that the two steppers on one belt was listed as a major design fault in the Prusa Mendel.

    It may be easier to use a single stepper with a tension belt system to avoid the pains in alignment, maintenance and the case of where you need to manually move the Z axis (for example, if it jams)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hawkeyethehacker
    hawkeyethehacker over 12 years ago in reply to e14 Contributor

    I would say just from looking at the RepRap wiki you will probably want to get your hands on an Arduino Mega and a RAMPS board. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>