Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog MSPM0 project with VS Code, CMake and GCC - part 2: build a real project
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 2 Sep 2026 8:23 PM Date Created
  • Views 143 views
  • Likes 4 likes
  • Comments 2 comments
  • MSPM0L1105
  • ccs
  • MSPM0
  • easyL1105
  • VS Code
  • MSPM0L1306
  • vscode
  • code_composer_studio
Related
Recommended

MSPM0 project with VS Code, CMake and GCC - part 2: build a real project

Jan Cumps
Jan Cumps
2 Sep 2026

In this blog series, I build a Texas Instruments MSPM0 example with VS Code as IDE, and CMake as build infrastructure.
Post 1 covered the software setup. In this post: build firmware,

image

Configure Environment Variables

SDK_ROOT and SYSCONFIG_CLI:

image

In the next post, where I use the debugger, there are a few more settings to do.

    Build Project

    We 'll need 3 files to build firmware for the MSPM0:

    • system configuration (SysConfig)
    • C source
    • CMake script

    The first two can be taken from any Resource Explorer project. Or one of your own designs. I reused one of the projects of TI's DMA training course:  DMA move a table in memory with MSPM0 

    The CMake file takes more work. I started from TI's example for CLang. Then made changes so that it works for the GCC ARM cross-compiler. I used AI to resolve errors and gaps.

    Before the traditional C build can run, the CMake file invokes SysConfig twice:

    • to turn your device configuration settings into C code, and get linker the right command file and library list. That part is 100% based on TI's CMake script.
    • to tell what startup_xxxx.c file to use for our device. I added that part.

    The remainder is more traditional: gather sources, includes, libs. Compile and Link.

    I added the command to also create a bootloader compatible binary (for Shabaz' Python programmer).

    Here is the result:

    cmake_minimum_required(VERSION 3.29)
    
    set(CMAKE_VERBOSE_MAKEFILE ON)
    
    set(CMAKE_C_STANDARD 11)
    set(CMAKE_CXX_STANDARD 26)
    set(CMAKE_EXPORT_COMPILE_COMMANDS ON)
    set(CMAKE_CXX_FLAGS "${CMAKE_CXX_FLAGS} -fmodules-ts")
    set(CMAKE_CXX_FLAGS "${CMAKE_CXX_FLAGS} -fcommon -fno-rtti -fno-exceptions")
    set(CMAKE_CXX_FLAGS "${CMAKE_CXX_FLAGS} -ffunction-sections -fdata-sections -g -gstrict-dwarf -Wall")
    set(CMAKE_CXX_STANDARD_REQUIRED ON)
    
    # Cross compiling for a target system that is an embedded device
    set(CMAKE_SYSTEM_NAME Generic)
    set(CMAKE_EXE_LINKER_FLAGS "${CMAKE_EXE_LINKER_FLAGS} --specs=nosys.specs --specs=nano.specs -static -Wl,--gc-sections")
    set(CMAKE_EXE_LINKER_FLAGS "${CMAKE_EXE_LINKER_FLAGS} -nostartfiles -mthumb")
    
    # Create the project
    project(
        mspm0_cmake
        LANGUAGES C  CXX     # Uses the programming language C
    )
    
    # Directory to the SDK used
    # SDK_ROOT set externally
    set(SDK_ROOT $ENV{SDK_ROOT})
    
    #---------------------------------------------------------------------
    # Configuration related to SysConfig
    #---------------------------------------------------------------------
    # Find the SysConfig command line interface (CLI) command in the system path
    # SYSCONFIG_CLI set externally
    set(SYSCONFIG_CLI $ENV{SYSCONFIG_CLI})
    
    # Directory to the generated SysConfig files
    set(SYSCONFIG_GENDIR ${CMAKE_BINARY_DIR}/sysconfig_generated)
    
    # SysConfig Input Script
    set(SYSCONFIG_INPUT_FILE_NAME ${CMAKE_PROJECT_NAME}.syscfg)
    set(SYSCONFIG_INPUT ${CMAKE_SOURCE_DIR}/${SYSCONFIG_INPUT_FILE_NAME})
    message(STATUS "SYSCONFIG_INPUT_FILE_NAME: ${SYSCONFIG_INPUT_FILE_NAME}")
    
    # SysConfig stamp file.  Described in the block comment at the end.
    set(SYSCONFIG_STAMP_FILE ${SYSCONFIG_GENDIR}/${SYSCONFIG_INPUT_FILE_NAME}.stamp)
    
    # SysConfig invocation command line
    set(SYSCONFIG_CLI_CMD
        ${SYSCONFIG_CLI}
            --script ${SYSCONFIG_INPUT}
            -o ${SYSCONFIG_GENDIR}
            --compiler gcc
            -s ${SDK_ROOT}/.metadata/product.json
    )
    
    # Ask SysConfig what files it generates.  Then categorize them.  This occurs
    # when CMake configures the project.
    execute_process(
        COMMAND ${SYSCONFIG_CLI_CMD} --listGeneratedFiles
        OUTPUT_VARIABLE SYSCONFIG_GEN_FILES_STR
    )
    string(REPLACE "\n" ";" SYSCONFIG_GEN_FILES ${SYSCONFIG_GEN_FILES_STR})
    
    set(SYSCONFIG_GEN_CFILES        ${SYSCONFIG_GEN_FILES})
    set(SYSCONFIG_GEN_HFILES        ${SYSCONFIG_GEN_FILES})
    set(SYSCONFIG_GEN_LNKCMD        ${SYSCONFIG_GEN_FILES})
    set(SYSCONFIG_GEN_COMPILER_OPTS ${SYSCONFIG_GEN_FILES})
    set(SYSCONFIG_GEN_LNKFILE       "${SYSCONFIG_GENDIR}/device_linker.lds")
    
    list(FILTER SYSCONFIG_GEN_CFILES        INCLUDE REGEX ".*\\.c$")
    list(FILTER SYSCONFIG_GEN_HFILES        INCLUDE REGEX ".*\\.h$")
    list(FILTER SYSCONFIG_GEN_LNKCMD        INCLUDE REGEX ".*\\.lds\\.")
    list(FILTER SYSCONFIG_GEN_COMPILER_OPTS INCLUDE REGEX ".*\\.opt$")
    
    # Ask SysConfig what file it references.  Then categorize it.  This occurs
    # when CMake configures the project.
    # Returns the fully qualified startup_mspm0xxxxx_gcc.c file for the selected device
    execute_process(
        COMMAND ${SYSCONFIG_CLI_CMD} --listReferencedFiles
        OUTPUT_VARIABLE SYSCONFIG_REF_FILES_STR
    )
    string(REPLACE "\n" ";" SYSCONFIG_REF_FILES ${SYSCONFIG_REF_FILES_STR})
    
    set(SYSCONFIG_REF_CFILES        ${SYSCONFIG_REF_FILES})
    list(FILTER SYSCONFIG_REF_CFILES        INCLUDE REGEX ".*\\.c$")
    message(STATUS "SYSCONFIG_REF_CFILES: ${SYSCONFIG_REF_CFILES}")
    
    # Cause CMake to run when the SysConfig input is modified, because that may
    # change the list of generated files
    set_property(
        DIRECTORY
        APPEND
        PROPERTY CMAKE_CONFIGURE_DEPENDS ${SYSCONFIG_INPUT}
    )
    
    # Run SysConfig over the input script.  Described further in a block comment
    # at the end.
    add_custom_command(
        DEPENDS    ${SYSCONFIG_INPUT}
        OUTPUT     ${SYSCONFIG_STAMP_FILE}
        BYPRODUCTS ${SYSCONFIG_GEN_FILES}
        COMMAND    ${SYSCONFIG_CLI_CMD}
        COMMAND    ${CMAKE_COMMAND} -E touch ${SYSCONFIG_STAMP_FILE}
        COMMENT    "Running SysConfig on ${SYSCONFIG_INPUT}"
        VERBATIM
    )
    add_custom_target(SysConfig_build ALL DEPENDS ${SYSCONFIG_STAMP_FILE})
    
    #---------------------------------------------------------------------
    # Configuration related to compiling
    #---------------------------------------------------------------------
    set(PROCESSOR_OPTIONS
        -march=armv6s-m
        -mcpu=cortex-m0plus
        -mfloat-abi=soft
        -mlittle-endian
        -mthumb
    )
    
    # These compiler options typically change as the project evolves.  Because
    # CMake replaces an undefined variable with an empty string, one way to
    # disable an option is to comment out that line.
    set(OPTIMIZATION_OPTION -O0)
    set(LTO_OPTION          -flto)
    set(DEBUG_OPTION        -gdwarf-3)
    
    message(STATUS "SYSCONFIG_GEN_COMPILER_OPTS: ${SYSCONFIG_GEN_COMPILER_OPTS}")
    
    # Compiler options
    add_compile_options(
        ${PROCESSOR_OPTIONS}
        ${OPTIMIZATION_OPTION}
        ${LTO_OPTION}
        ${DEBUG_OPTION}
        @${SYSCONFIG_GEN_COMPILER_OPTS}
    )
    
    message(STATUS "SYSCONFIG_GEN_CFILES: ${SYSCONFIG_GEN_CFILES}")
    
    # C files
    set(SOURCES
        ${CMAKE_SOURCE_DIR}/mspm0_cmake.cpp
        ${SYSCONFIG_GEN_CFILES}
        ${SYSCONFIG_REF_CFILES} # startup_mspm0xxxxx_gcc.c file for the selected device
    #    ${SDK_ROOT}/source/ti/devices/msp/m0p/startup_system_files/gcc/startup_mspm0l130x_gcc.c
    )
    
    # Cause C files to depend on the SysConfig generated compiler options file
    set_source_files_properties(
        ${SOURCES}
        PROPERTIES OBJECT_DEPENDS
        ${SYSCONFIG_GEN_COMPILER_OPTS}
    )
    
    message(STATUS "SYSCONFIG_GENDIR: ${SYSCONFIG_GENDIR}")
    
    # Directories searched for header files
    include_directories(
        ${SDK_ROOT}/source
        ${SDK_ROOT}/source/third_party/CMSIS/Core/Include
        ${SYSCONFIG_GENDIR}
    )
    
    #---------------------------------------------------------------------
    # Configuration related to linking
    #---------------------------------------------------------------------
    # Linker Options
    add_link_options(
        ${LTO_OPTION}            # Required when compiling AND linking
    )
    
    # Directories searched for libraries
    link_directories(
        ${SDK_ROOT}/source
    )
    
    message(STATUS "SYSCONFIG_GEN_LNKFILE: ${SYSCONFIG_GEN_LNKFILE}")
    message(STATUS "SYSCONFIG_GEN_LNKCMD: ${SYSCONFIG_GEN_LNKCMD}")
    
    set(CMAKE_EXE_LINKER_FLAGS "${CMAKE_EXE_LINKER_FLAGS} -Wl,-T ${SYSCONFIG_GEN_LNKFILE}")
    
    message(STATUS "SOURCES: ${SOURCES}")
    # Build the executable from source files in the project
    add_executable( ${CMAKE_PROJECT_NAME}
        ${SOURCES}
    )
    add_dependencies(${CMAKE_PROJECT_NAME} SysConfig_build)
    
    target_link_directories(${CMAKE_PROJECT_NAME} PRIVATE 
    )
    
    # Libraries and linker command files
    target_link_libraries( ${CMAKE_PROJECT_NAME} PRIVATE
        ${SYSCONFIG_GEN_LNKCMD}
    )
    
    get_target_property(TARGET_LIBS ${CMAKE_PROJECT_NAME} LINK_LIBRARIES)
    message(STATUS "Libraries linked to ${CMAKE_PROJECT_NAME}: ${TARGET_LIBS}")
    
    message(STATUS "SDK uses value of assignment with 'volatile'-qualified left operand ")
    target_compile_options(${CMAKE_PROJECT_NAME} PRIVATE $<$<COMPILE_LANGUAGE:CXX>:-Wno-volatile>)
    message(STATUS "SDK uses bitwise operation between different enumeration types ")
    target_compile_options(${CMAKE_PROJECT_NAME} PRIVATE $<$<COMPILE_LANGUAGE:CXX>:-Wno-deprecated-enum-enum-conversion>)
    
    # objcopy for bootloader compatible firmware
    set(HEX_FILE ${PROJECT_BINARY_DIR}/${CMAKE_PROJECT_NAME}.hex)
    
    # POST_BUILD 
    message(STATUS "ObjCopy utility: ${CMAKE_OBJCOPY}")
    message(STATUS "firmware: ${PROJECT_BINARY_DIR}/${CMAKE_PROJECT_NAME}")
    add_custom_command(TARGET ${CMAKE_PROJECT_NAME} POST_BUILD
        COMMAND ${CMAKE_OBJCOPY} -O ihex  --gap-fill 0xFF ${PROJECT_BINARY_DIR}/${CMAKE_PROJECT_NAME} ${HEX_FILE}
        COMMENT "creating .hex file ..."
        VERBATIM
    )

    The TI pages that I linked to above, go in detail over each section.

    Use the VS Code CMake plugin to select the GCC compiler, and then config and build the project:

    image

    If all is well, you should get this message after config:

    [cmake] -- Configuring done (4.2s)
    [cmake] -- Generating done (0.1s)
    [cmake] -- Build files have been written to: C:/Users/jancu/workspace_vscode_mspm0/msmp0_cmake/build

    And this after build:

    [build] [4/4 100% :: 1.279] Linking C executable mspm0_cmake
    [driver] Build completed: 00:00:01.337
    [build] Build finished with exit code 0

    You can now load this firmware to your MSPM0. Either with Uniflash, or with Shabaz' Python loader.
    Or wait for the next post, where I'll build a VS Code launch script. That 'll allow you to step through your code, just like with TI's Code Composer Studio.

    Thank you for reading.

    post 1:  MSPM0 project with VS Code, CMake and GCC - part 1: infrastructure 

    post 3:  MSPM0 project with VS Code, CMake and GCC - part 3: debug 

    part of the EasyL1105 series. all posts

    • Sign in to reply
    Parents
    • Qbit
      Qbit 19 days ago

      Great see you using VS code in the build.

      • Cancel
      • Vote Up 0 Vote Down
      • Sign in to reply
      • More
      • Cancel
    Comment
    • Qbit
      Qbit 19 days ago

      Great see you using VS code in the build.