Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog PID temperature controller for the EasyL1105 MSPM0 board - Pt. 1: framework
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 25 Sep 2025 6:01 PM Date Created
  • Views 1547 views
  • Likes 7 likes
  • Comments 5 comments
  • MSPM0L1105
  • MSPM0
  • easyL1105
  • texas instruments
Related
Recommended

PID temperature controller for the EasyL1105 MSPM0 board - Pt. 1: framework

Jan Cumps
Jan Cumps
25 Sep 2025
PID temperature controller for the EasyL1105 MSPM0 board - Pt. 1: framework

 shabaz designed a development kit for the recent Texas Instruments MSPM0 microcontroller series. 
This 4 part blog series documents the steps to design a PID temperature controller. Part 1: the framework.

image
(post that introduces the kit)

Goal of this 1st post

  • select a PID algorithm that's fit for an MSPM0, without floating point
  • set up a timer that makes the code execute on precise intervals
  • have a heartbeat pulse to monitor time health (via green LED, counter or scope)
  • make it build and execute

Not a goal in post 1:  ADC, PWM. Conversion to PID savvy UOM of both. Tuning the PID algorithm.

Most of this stage of the design is borrowed from examples and previous posts.

resources used

  •  MSP432 and TI-RTOS: PID Library Part 1 - Intro 
  •  MSP432 and TI-RTOS: PID Library Part 2 - Real World Example 
  •  PID algo for ARM M0: Nuvoton PID Control Operation in Fixed-point Format
  • Timer: TI timx_timer_mode_periodic_sleep
  • PID guidelines:  PID Control in Flowcode 

Framework: PID algorithm

The ARM M0 doesn't have floating point hardware. I found a PID example that is written by Nuvoton for that family (see resources used). I'm using both the PID algorithm and the timer approach.

  • wait for a timer tick, 5 times per second
  • call the PID algorithm to keep the circuit controlled

int32_t PID(PIDC_T* C, int32_t i32_Cmd, int32_t i32_Feedback)
{
    int32_t output;
    
    /* Calculate error */
    C->i32_Err = i32_Cmd - i32_Feedback;
    
    /* Integral calculation */
    C->i32_I += C->i32_Ki * C->i32_Err;	
    
    /* PID calculation */
    output = C->i32_Kp * C->i32_Err + C->i32_I + C->i32_Kd * (C->i32_Err - C->i32_Last_Err);	
    
    /* Set output in Q15.0 format */
    output = output >> 15;	
    
    if(output > C->i32_Out_Limit)
        output = C->i32_Out_Limit;
    else if(output < -C->i32_Out_Limit)
        output = -C->i32_Out_Limit;	
        
    /* Update last error */
    C->i32_Last_Err = C->i32_Err;
        
    /* Return the output of PID Controller */
    return output;													
}

What I changed: I don't do the PID (or any other logic) in the timer handler. The handler just sets a flag, and the loop() executes the logic if that flag is set. This is an architectural choice. We 'll have to do ADC, PID and PWM. I prefer not to have all of that executed in an interrupt handler. For low power designs, I'd leave it in the interrupt.

void perform_pid() {

            
    /* Execute PID control in every TM0 interrupt. */
    i32_Output_PID = PID(&PID_Var, i32_Target_Command, i32_Plant_Signal);
		
    /* Following is for test only */
    /* Simulate it is unit gain feedback */
    i32_Plant_Signal = i32_Output_PID;	// TODO: this is test code. need to define correct feedback based on sensor hw

    // TODO: add PWM
    cnt++; // TODO: remove test

}

int main(void) {
    // ...

	/* Initialize the parameters of PID */
	Initialize_PID_Parameter();

    // ...   

    while (1) {
        if (perform) {
            perform = false;
            // ...
            
            perform_pid();

            // ...
        }
    }
}


The PID algorithm uses Q15 format, to represent - and calculate with - floating points as integers.

What does AI say about  Q15 format?

The Q15 format, also known as the 1.15 format, is a fixed-point number representation that uses 16 bits to store a two's complement signed fractional number, with one bit for the sign, zero bits for the integer part, and 15 bits for the fractional part. It is commonly used in Digital Signal Processing (DSP) for representing numbers in the range of -1.0 to +0.999969482, where the value is the stored integer divided by 2^15. 
How it Works
  • Signed Representation: The most significant bit (MSB) is the sign bit. 
  • Radix Point: The binary point (radix point) is implied to be just after the sign bit. 
  • Value Calculation: A number stored in Q15 format is calculated by dividing the integer value by 2^15 (32768). For example, the integer 24576 represents the value 0.75 in Q15 format (24576 / 32768). 
  • Range: The representable range for a Q15 number is from -1.0 to (1 - 2^-15), which is approximately -1.0 to 0.999969482. 
  • Storage: A Q15 value is stored as a 16-bit signed integer. 
Example 
  • 0x7FFF (0111 1111 1111 1111 in binary): This represents the maximum positive value, which is close to 1.0 (specifically 0.999969482).
  • 0x8000 (1000 0000 0000 0000 in binary): This represents the most negative value, which is -1.0.
Why Use Q15?
  • Efficiency: 
    Using fixed-point formats like Q15 allows for faster arithmetic operations (multiplication and division) compared to floating-point numbers because it uses integer hardware. 
  • DSP Applications: 
    It is frequently used in DSP applications where integer math is preferred for its speed and efficiency, especially on embedded systems. 

Framework: Timer

The timer logic is based on a TI example for this controller (see resources used). It fires an interrupt 5 times per second.

image

There's a little bit of setup in main():

int main(void) {
    SYSCFG_DL_init();

    // /* timer 5 interrupt ticks per second */ 
    // /* Enable Timer0 NVIC */
    NVIC_EnableIRQ(TIMER_0_INST_INT_IRQN);

	// ...

    // /* Start Timer counting */
    DL_TimerG_startCounter(TIMER_0_INST);    

    while (1) {
        if (perform) {
            perform = false;
            
            // ...
            
            perform_pid();

            // ...
        }
    }
}

Our handler checks if it's the right interrupt. Then sets a flag and moves on.

volatile bool perform = false;

void TIMER_0_INST_IRQHandler(void) {
    switch (DL_TimerG_getPendingInterrupt(TIMER_0_INST)) {
        case DL_TIMER_IIDX_ZERO:
            perform = true;
            break;
        default:
            break;
    }
}

Framework: heartbeat and placeholders for ADC and PWM

With the timer in place, and the PID executed after each tick, we're ready to put in some hooks for the next parts:

an empty implementation for the ADC and PWM logic. These will be implemented in the next posts.

void perform_adc() {
    // TODO: implement
}

void perform_pwm() {
    // TODO: implement    
}

Add a heartbeat, and ADC + PWM calls to the loop()

image

The heartbeat gives an option to externally monitor if we're staying within timer limits. A pin is pulled high when an end-to-end cycle starts, and switched off when finished. I've used the EasyL1105 pin that has the green LED attached. Although it 'll be barely visible, you can use it to check that the code runs every 200 ms. For better control, add an oscilloscope or counter.

    DL_TimerG_startCounter(TIMER_0_INST);    

    while (1) {
        if (perform) {
            perform = false;
            DL_GPIO_setPins(GPIO_GRP_LEDS_PORT,
                GPIO_GRP_LEDS_PIN_LED_GREEN_PIN);

            perform_adc();
            
            perform_pid();

            perform_pwm();

            DL_GPIO_clearPins(GPIO_GRP_LEDS_PORT,
                GPIO_GRP_LEDS_PIN_LED_GREEN_PIN);
        }
    }
}

Thanks for reading. Next, get ADC working.

ccs project for EasyL1105: pid_EasyL1105_20250925.zip

This post contains AI generated info. This info is put in a table with pink coloured background.

Related posts

  • Sign in to reply
Parents
  • Jan Cumps
    Jan Cumps over 1 year ago

    Note to self:  PID Control in Flowcode 

    A reactive PID system should aim for a little overshoot before settling down. Rule of thumb values are that P is roughly equal to I and D is roughly one quarter the value of I.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 1 year ago

    Note to self:  PID Control in Flowcode 

    A reactive PID system should aim for a little overshoot before settling down. Rule of thumb values are that P is roughly equal to I and D is roughly one quarter the value of I.