Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog PSoC 6 and ModusToolbox: FreeRTOS to AWS MQTT
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 28 Mar 2021 7:10 PM Date Created
  • Views 8877 views
  • Likes 2 likes
  • Comments 33 comments
  • mqtt
  • aws
  • psoc_6
  • freertos
  • aws_iot
  • cypress
Related
Recommended

PSoC 6 and ModusToolbox: FreeRTOS to AWS MQTT

Jan Cumps
Jan Cumps
28 Mar 2021

In this post we react on a message on the RTOS queue and publish its payload on Amazon's AWS IoT MQTT service.

image

 

Together with the two previous posts, this one describes a hardware component in the NanoDrone II project of balearicdynamics

Scenario: receive 16 bytes of payload from an Arduino over serial, and forward it to AWS cloud.

The summary of the flow:

  • 2 main tasks, one for the UART with Arduino, one for MQTT with AWS.
  • all tasks sleep.
  • when Arduino sends 16 bytes, a trigger fires, and it wakes up the UART task.
  • UART task copies payload from UART buffer, and puts it on a RTOS queue as a message.
  • UART task back to sleep.
  • When a message is on the queue, the MQTT task wakes up
  • gets the message data from the queue and publishes a new message on AWS MQTT service with that data as payload.
  • MQTT task back to sleep
  • repeat

The two tasks run and sleep independently. The queue has 10 positions and can act as a UART data buffer if there's a slowness in publishing the message on AWS cloud.

 

Instead of showing the whole exercise, I'm going to point you to the AnyCloud MQTT Client example that this firmware borrowed from.

What have we changed:

  • the MQTT topic. It was "ledstatus". we use "nanodrone"
  • the trigger: a button press in the PSoC example. We use a message on the queue as trigger
  • subscribe: the original example subscribes to the same message as posted, then toggles the user led. We don't subscribe. One way traffic.
  • We introduced a queue to interact between the UART and MQTT client.
  • Changed power modes in the RTOS config. To keep the UART reactive.

 

The firmware is available on github: https://github.com/alicemirror/Nanodrone-II_PSoC6 .

Before cloning the project, check out the original AnyCloud MQTT Client example in ModusToolbox.

It serves two purposes: you have an example, and it takes care that the dependencies are all available in your workspace.

Follow its instructions to connect you to AWS MQTT. You'll need to do the exact same steps with our project. If you know it works with the standard example, it makes the next steps easier.

 

After cloning and importing the project into your workspace, perform these activities in the Quick Panel:

  • open the Library Manager and click Update. Close when finished.
  • click Refresh Quick Panel.
  • update mqtt_client.h with your Amazon certificates, and wifi_config.h with your WiFI settings, as you'd do for the AnyCloud MQTT Client example.
  • click Build Nanodrone-II_PSoC Application

 

Then connect  a 3.3 V Arduino. GND to PSoC 6 GND, TX with PSoC 6 pin 10.0.

Program this example on the Arduino: a simple program that will send 16 bytes once every time the Arduino resets.

 

void setup() {
  // start serial port at 9600 bps and wait for port to open:
  Serial1.begin(9600);
  establishContact();
}


void loop() {
    delay(100000);
}

void establishContact() {
    Serial1.print("{\"a\":-122,\"b\":3}");   // send a fixed lenght string
}

 

If all is well, you should get a message on your MQTT Cloud account each time you press the Arduino reset button.

 

image

 

PSoC 6 series
PSoC 6 and ModusToolbox: Create a Project with its own Board- and Module configurations
PSoC 6: Low Power Management - Power consumption without WiFi or Bluetooth
PSoC 6 and ModusToolbox: Create a FreeRTOS 10.3 Project
PSoC 6 and ModusToolbox: UART receiver with FreeRTOS
PSoC 6 and ModusToolbox: FreeRTOS message queue
PSoC 6 and ModusToolbox: FreeRTOS to AWS MQTT
PSoC 6 and ModusToolbox: Break the Debugger from the Proto Board
  • Sign in to reply
Parents
  • skruglewicz
    skruglewicz over 4 years ago

    Hello Jan Cumps

     

    I hope this comment finds you well.

    I've been reviewing your code on the PSoC6 kit for the NanoDrone_II project, which this blog is a part of.

    I'm still trying to get the AnyCloud example to work but in the meantime I cloned

    "The firmware is available on GitHub: https://github.com/alicemirror/Nanodrone-II_PSoC6 "

    I'm using a different kit, the CY8CKIT-062S2-43012 given to me for an element14 design challenge.

    In theory (and you state in your GitHub repo) that this should be compatible.

    I getting build error?

     

    I have imported the project into ModusToolbox with the "Open Project from File System".

    I changed the target= in the makefile and changed the

    Library Manager to my kit which is CY8CKIT-062S2-43012

    it was CY8CPROTO-062-4343W

     

     

    I try to build and I get 6 Errors as follows:

    -----------------------------------------------------------------------

    Description Resource Path Location Type

     

    #error "MBEDTLS_PSA_ITS_FILE_C defined, but not all prerequisites" check_config.h /mtb_shared_2/mbedtls/mbedtls-2.22.0/include/mbedtls line 580 C/C++ Problem

     

    make: *** [../mtb_shared/core-make/release-v1.9.0/make/core/main.mk:434: secondstage_build] Error 2 Nanodrone_II C/C++ Problem

     

    make[1]: *** [../mtb_shared/core-make/release-v1.9.0/make/core/build.mk:387: C:/PSoC6/Nanodrone-II_PSoC6-main/build/CY8CKIT-062S2-43012/Custom/ext/mtb_shared/mbedtls/mbedtls-2.22.0/library/aes.o] Error 1 Nanodrone_II C/C++ Problem

     

    make[1]: *** [../mtb_shared/core-make/release-v1.9.0/make/core/build.mk:387: C:/PSoC6/Nanodrone-II_PSoC6-main/build/CY8CKIT-062S2-43012/Custom/ext/mtb_shared/mbedtls/mbedtls-2.22.0/library/aesni.o] Error 1 Nanodrone_II C/C++ Problem

     

    make[1]: *** [../mtb_shared/core-make/release-v1.9.0/make/core/build.mk:387: C:/PSoC6/Nanodrone-II_PSoC6-main/build/CY8CKIT-062S2-43012/Custom/ext/mtb_shared/mbedtls/mbedtls-2.22.0/library/arc4.o] Error 1 Nanodrone_II C/C++ Problem

     

    make[1]: *** Waiting for unfinished jobs.... Nanodrone_II C/C++ Problem

    -----------------------------------------------------------------------

    not sure what the errors mean?

    Is "MBEDTLS_PSA_ITS_FILE_C needed?

    can I change the makefile in some way to support the CY8CKIT-062S2-43012 kit.

    the challenge page on element14 is -----

     

     

    Thanks in advance

    Steve K

     

    PS.. you can send a message directly to me if you would like to communicate in this way.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to skruglewicz

    Did it build before you changed the target?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • skruglewicz
    skruglewicz over 4 years ago in reply to Jan Cumps

    No ,same error I recall. Haven't been able to build. I have a question into the cypress forum as well.

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to skruglewicz

    What happens if you try and load the original AnyCloud AWS MQTT example? Does that build?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • skruglewicz
    skruglewicz over 4 years ago in reply to Jan Cumps

    Yes that builds fine. I'm connected over WiFi and I about to connect the the AWS MQTT broker.

     

    So when I get your project to build, I plan on using your design and code for the design challenge. I have a long way to go and it turns out your FreeRTOS design is just what I can use for my idea.

     

    There are some mention of the MBEDTLS library in the Makefile. I'm new to ModusToolbox and don't know what that Library does.

     

    Regards

    SteveK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • skruglewicz
    skruglewicz over 4 years ago in reply to Jan Cumps

    Yes that builds fine. I'm connected over WiFi and I about to connect the the AWS MQTT broker.

     

    So when I get your project to build, I plan on using your design and code for the design challenge. I have a long way to go and it turns out your FreeRTOS design is just what I can use for my idea.

     

    There are some mention of the MBEDTLS library in the Makefile. I'm new to ModusToolbox and don't know what that Library does.

     

    Regards

    SteveK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to skruglewicz

    balearicdynamics,  you have imported the Nanodrone2 project in ModusToolbox before.

    Did you have to do something to make it compile?