Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Damage detection of roads using piezo sensors
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 335 subscribers
  • Views 4036 views
  • Users 0 members are here
  • research
  • piezoelectric
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Damage detection of roads using piezo sensors

AniketVis
AniketVis over 3 years ago

I'm working on a project called damage detection in roads using piezoelectric sensor....i need some help and guidance regarding this....

  • Sign in to reply
  • Cancel

Top Replies

  • scottiebabe
    scottiebabe over 3 years ago +3
    I'm not sure of your location but the search term "smartphone pothole detection" should lead to lots of research papers that might be helpful
  • Gough Lui
    Gough Lui over 3 years ago +3
    There's a mob here that uses accelerometers and cameras mounted to our bus fleet to scan the roads on a nearly continuous basis: https://www.arrb.com.au/news/using-the-sydney-bus-network-to-find-potholes…
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to michaelkellett +2
    AniketVis , I can point you to some of the posts that Michael discusses above. They will help you with 3 things: turn the piezo signal into a safe signal, and condition / buffer it (front end) : Piezo…
Parents
  • michaelkellett
    michaelkellett over 3 years ago

    You'll need to tell us a bit more.

    What sort of piezo electric sensor ?

    I know of force, displacement, acceleration, pressure, microphones, acoustic emitters and more.

    Why don't you explain what your project is, what you have done so dar and where you are stuck ?

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • AniketVis
    AniketVis over 3 years ago in reply to michaelkellett

    We have taken some readings and waveforms with this piezo sensor on a road using digital oscilloscope....but we don't know how to interpret those readings....our target is to detect how damaged the road is from inside by using these readings we received....we need basically all guidance about instrument, sensor, method....or if we get any good research paper it will be a great help....thank youimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago in reply to AniketVis

    Interesting project. There are lots of causes of road damage, but the result is usually a bumpier road. When vehicles go over a bump, their suspension and tires oscillate. You may be able to detect this oscillation and its amplitude with this sensor. It will take some experimentation to get the sensor coupled to the road properly without damaging the road and more experimentation to make sense of the data. You may find some frequencies correlate better to road damage. This is a good application for machine learning, but you probably need multiple installations.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 3 years ago in reply to AniketVis

    I'm guessing that this is a college project.

    You would help yourself a lot if you write down in advance exactly what you are trying to do - this would help you start to work out how you might do it.

    From what you've said so far, I think you are attempting to measure the quality of the surface of the road by making acceleration measurements inside a vehicle driving along the road.

    This is a staggeringly difficult problem to solve analytically.

    Let's assume the vehicle has 4 wheels and the input displacement from the road surface is filtered by the suspension system which will include tyres, springs, dampers etc. The vehicle body, and your accelerometer will experience pitch, roll,yaw  and vertical acceleration accordng to the sum of these inputs. The input from a given road feature will often stimulate the system twice (as front then rear wheels pass over it).

    The classical way to solve this problem is to make a mathematcial whole vehicle model and use this as a tool to help relate road surface to accelerometer signal. Frequently at this point the conclusion is that the motion analysis is so complex that it isn't possible to do it in real time, often more measurment data like multiple accelerometers and gyros is required.

    Of course you are attempting this with a piezo electric sounder disk which will make a not very good accelerometer.

    Jan Cumps has blogged on E14 about doing this - it will help you unbderstand the lmitations of the sounder disk accelerometer if you read his blogs.

    Long experience tells me that you will not be able to make a good model of the vehicle (such projects require several skilled PHD+ level engineers with adequate resources in terms of computing and software tools).

    You could still do something.

    I would avoid the machine learing approach - it will eat up a lot of time and you will have enormous dificulty in gathering training data.

    What might work for you is recording the acceleration data over time (simplest is to record peak acceleration seen in each second but better to sample faster if you can) and the position of the vehicle (from GPS I expect). Then survey the road and see how the potholes correlate with the data you have collected. My guess is that you'll be able to see at least the worst potholes from the data. This might be good enough.

    Your accelerometer will need a bandwidth from about 0.5Hz to 25Hz  - so you'll need a buffer amplifier (see Jan's blogs) and  a filter.

    AN oscilloscope is the wrong instrument for this work. You need to be able to record raw data at maybe 100samples per second and correlate it with GPS data. This isn't too hard - well within Arduino capability.

    You don't say what your team's skills are so I can't be more specific.

    Once more, I urge you, write a plan, think about what might go wrong and how you can deal with it. Limit the scope of the project to stuff you can actually do.

    People on E14 can do much more to help if they have  a bit more to work on.

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago in reply to dougw

    If you are instrumenting the vehicle instead of the road, there are papers on this. I was a reviewer of a Master's thesis on a similar topic a decade ago. It was aimed more at determining when the vehicle would need maintenance, but the instrumentation would be similar.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to michaelkellett

     AniketVis , I can point you to some of the posts that Michael discusses above. They will help you with 3 things:

    • turn the piezo signal into a safe signal, and condition / buffer it (front end) :  Piezo disk as Vibration Sensor: input buffer and filter 
    • a possible data acquisition system that allows you to sample the signal fast and for a long time
    • the calculations to turn the samples into acceleration info and frequency info (fft)
    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to michaelkellett

     AniketVis , I can point you to some of the posts that Michael discusses above. They will help you with 3 things:

    • turn the piezo signal into a safe signal, and condition / buffer it (front end) :  Piezo disk as Vibration Sensor: input buffer and filter 
    • a possible data acquisition system that allows you to sample the signal fast and for a long time
    • the calculations to turn the samples into acceleration info and frequency info (fft)